Pro Micro & Fio v3 Hookup Guide Datasheet by SparkFun Electronics

View All Related Products | Download PDF Datasheet
Page 1 of 27 '.
PM A
Pro Micro & Fio v3 Hookup Guide
CONTRIBUTORS: JIMB0
Introduction
Welcome to the new frontier of Arduino-compatible boards, made possible
by the ATmega32U4. No longer does your Arduino need to be harnessed
by an FTDI Cable, or an ATmega8U2, or any chip who’s sole purpose is
acting as an intermediary between your Arduino and your computer.
The SparkFun Pro Micro is a really cool, little development board. It’s an
Arduino-compatible microcontroller, micro-sized, and it accomplishes with
one single chip what old Arduino Unos, Duemilanoves, and Diecimeillas
could never dream of: true USB functionality.
This tutorial also covers the Fio v3, which works a lot like the Pro Micro but
adds features like easy XBee interfacing and LiPo charging.
Page 1 of 2
7
Page 2 of 27
Covered In This Tutorial
This tutorial aims to introduce you to both the hardware and firmware sides
of the Pro Micro (and Fio v3). We’ll also dedicate a few pages to helping
install the boards on Windows and Mac. Here’s a summary of what will be
covered:
Hardware Overview: Pro Micro – An overview of the pinout and
hardware features of the Pro Micro.
Hardware Overview: Fio v3 – An overview of the pinout and
hardware features of the Fio v3.
Installing on Windows – How to install the drivers and Arduino addon
on Windows.
Installing on Mac/Linux – How to install the drivers and Arduino
addon on Mac.
Example 1: Blinkies – A simple “Hello, world” sketch specifically
suited to the Pro Micro and Fio v3.
Example 2: HID Mouse and Keyboard – An introduction to the HID
USB capability of the Pro Micro. How to emulate USB keyboards and
mice!
Troubleshooting and FAQ – Helpful troubleshooting tips and tricks for
getting the most out of the Pro Micro.
Suggested Reading
Before delving into this tutorial, here are some concepts you should be
familiar with. If you’re not, consider checking out the related tutorial first.
What is Arduino? – An introduction to the Arduino platform and IDE.
How to Install Arduino – A general installation guide for Arduino.
Serial Communication – Serial is a great, easy-to-use communication
protocol.
Hardware Overview: Pro Micro
Page 2 of 2
7
Page 3 of 27 --.I1C--
Before we get into installing and using the Pro Micro, let’s quickly look at
the board – examine its inputs, outputs, and other hardware quirks.
The Pinout
All of the Pro Micro’s I/O and power pins are broken out to two, parallel
headers. Some pins are for power input or output, other pins are dedicated
I/O pins. Further, the I/O pins can have special abilities, like analog input.
Here’s a map of which pin is where, and what special hardware functions it
may have:
Delving a little further into which pins do what…
Power Pins
There are a variety of power and power-related nets broken out:
RAW is the unregulated voltage input for the Pro Micro. If the board
is powered via USB, the voltage at this pin will be about 4.8V (USB’s
5V minus a schottkey diode drop). On the other hand, if the board is
powered externally, through this pin, the applied voltage can be up to
12V.
VCC is the voltage supplied to the on-board ATmega32U4. This
voltage will depend on whether you’re using a 3.3V/8MHz Pro Micro
or a 5V/16MHz version, it’ll be either 3.3V or 5V respectively. This
voltage is regulated by the voltage applied to the RAW pin. If the
board is powered through the ‘RAW’ pin (or USB), this pin can be
used as an output to supply other devices.
RST can be used to restart the Pro Micro. This pin is pulled high by
a 10k&Ohm; resistor on the board, and is active-low, so it must be
connected to ground to initiate a reset. The Pro Micro will remain “off”
until the reset line is pulled back to high.
GND, of course, is the common, ground voltage (0V reference) for
the system.
Page 3 of 2
7
Page 4 of 27
I/O Pins
The Pro Micro’s I/O pins – 18 in all – are multi-talented. Every pin can be
used as a digital input or output, for blinking LEDs or reading button
presses. These pins are referenced in the Arduino IDE via an integer value
between 0 and 21. (The A0-A3 pins can be referenced digitally using either
their analog or digital pin number).
Nine pins feature analog to digital converters (ADCs) and can be used as
analog inputs. These are useful for reading potentiometers or other analog
devices using the analogRead([pin]) function.
There are five pins with pulse width modulation (PWM) functionality, which
allows for a form of analog output using the
analogWrite([pin], [value]) function. These pins are indicated on-board
with a faint, white circle around them.
There are hardware UART (serial), I C, and SPI pins available as well.
These can be used to interface with digital devices like serial LCDs, XBees,
IMUs, and other serial sensors.
The Pro Micro has five external interrupts, which allow you to instantly
trigger a function when a pin goes either high or low (or both). If you attach
an interrupt to an interrupt-enabled pin, you’ll need to know the specific
interrupt that pin triggers: pin 3 maps to interrupt 0, pin 2 is interrupt 1, pin 0
is interrupt 2, pin 1 is interrupt 3, and pin 7 is interrupt 4.
On-Board LEDs
There are three LEDs on the Pro Micro. One red LED indicates whether
power is present.
The other two LEDs help indicate when data is transferring over USB. A
yellow LED represents USB data coming into (RX) the the Pro Micro, and a
green LED indicates USB data going out (TX).
3.3V or 5V? 8MHz or 16MHz?
Pro Micros come in two flavors, which vary by system voltage and
operating frequency. The standard 5V Pro Micro runs at 16MHz, and is
very comparable to an Arduino Leonardo, while the 3.3V version of the Pro
Micro runs at half the speed (to remain in the safe operating zone at the
lower voltage) – 8MHz.
The operating voltage of your Pro Micro determines the maximum allowable
voltage on any of the I/O pins. For example, if you have a 3.3V Pro Micro,
don’t interface it with something that outputs 5V.
2
Page 4 of 2
7
Page 5 of 27
Don’t forget which version you have! We’ll need to differentiate between the
two when we get to uploading code in Arduino. If you’re not sure which
version you have, check the back corner of the board. One of two boxes
should be checked to indicate the operating voltage.
How to Power the Pro Micro
As the Pro Micro’s main feature is its innate USB functionality, the most
common way to power it is via USB. In this setup, a 5V Pro Micro will be
powered directly from the USB bus and a 3.3V Pro Micro will regulate the
5V supply coming in from USB down. The other end of the USB cable can
be connected to either a computer, USB hub, or a USB wall adapter, which
can (in most cases) provide more power.
Alternatively, if your Pro Micro is living out in the wild, out of reach of USB
cables, it can be powered through either the ‘RAW’ or ‘VCC’ pins. A supply
going into the ‘RAW’ pin will be regulated down to the correct operating
voltage (5V or 3.3V). To be safe, it shouldn’t be any higher than 12V, and it
should be at least 1V more than the Pro Micro’s operating voltage (e.g. >6V
for a 5V Pro Micro).
Pro Micro powered through the RAW pin by a set of four, series AA
batteries.
If you power the Pro Micro through the ‘VCC’ pin, keep in mind that this
signal is unregulated. Only use this if you have a clean, regulated 3.3V or
5V supply to connect to it.
Page 5 of 2
7
Page 6 of 27 2 9qu —sm@e)w J sq. Jaw oJm . 9105M
How, exactly, you power your project is up to you and the demands of your
project. If you’re making something battery powered, you may want to opt
for the 3.3V Pro Micro, which could be powered by a LiPo battery or a
couple alkalines.
Hardware Overview: Fio v3
On this page we’ll examine the hardware half of the Fio v3, looking at the
pinout, layout, and schematic of the board.
The Fio v3 is like an elongated Pro Micro. On one end, it’s shape and
pinouts are similar to it’s ATmega32U4 sibling. The other end of the Fio v3
is what makes it unique: a footprint for an XBee on the bottom, and a LiPo
charging circuit on the top.
The Pinout
All of the Fio v3’s pins are broken out to either side of the board. Some pins
are for power input or output, other pins are dedicated I/O pins. Further, the
I/O pins can have special abilities, like analog input, or serial input/output.
Here’s a map of which pin is where, and what special capabilities it may
have:
Power Pins
The pins labeled ‘3.3V’ break out the operating voltage source of the
ATmega32U4. As long as the board is powered through the white JST
connector or USB, this voltage is regulated down to 3.3V. These pins can
be used as outputs to supply 3.3V to other devices.
Page 6 of 2
7
Page 7 of 27
The ‘RST’ pin can be used to restart the Fio. This pin is pulled high by a
10kΩ resistor on the board, and is active-low, so it must be connected to
ground to initiate a reset. The Fio will remain off until the reset line is pulled
back to high.
I/O Pins
Many of the Fio’s I/O pins are multi-talented. Every pin can be used as a
digital input or output, for blinking LEDs or reading button presses. These
pins are referenced in the Arduino IDE via an integer value between 0 and
23. (The A0-A10 pins can be referenced digitally via either their analog pin
number or digital pin number).
Eleven pins feature analog to digital converters (ADCs) and can be used as
analog inputs. These are useful for reading potentiometers or other analog
devices using the analogRead([pin]) function.
There are six pins with pulse width modulation (PWM) functionality, which
allows for a form of analog output using the
analogWrite([pin], [value]) function. These pins are indicated on-board
with a faint white circle around the pin.
There are also hardware UART (serial), I C, and SPI pins available. These
can be used to interface with digital devices like serial LCDs, IMUs, and
other serial sensors.
The Fio v3 has five external interrupts, which allow you to instantly trigger a
function when a pin goes either high or low (or both). If you attach an
interrupt to an interrupt-enabled pin, you’ll need to know the specific
interrupt that pin triggers: pin 3 maps to interrupt 0, pin 2 is interrupt 1, pin 0
is interrupt 2, pin 1 is interrupt 3, and pin 7 is interrupt 4.
On-Board LEDs
There are a variety of LEDs on the Fio, the simplest of which is the red
power indicator. Two LEDs towards the bottom – labeled RX and TX – help
indicate when data is transferring to and from the Fio through USB. A blue
LED represents USB data coming into (‘RX’) the the Pro Micro, and a
yellow LED indicates USB data going out (‘TX’).
There are three LEDs tied to the XBee interface in particular: stat, RSSI,
and associate. The red LED labeled ‘ON’ is connected to the XBee’s pin 13
– DIO9 – which is, by default, set to indicate the XBee module’s ON/OFF
status. An ‘RSSI’ LED connects to XBee pin 6 (PWM0) which defaults to
indicate RSSI (received signal strength) – a brighter LED means a stronger
received signal. Lastly, the ‘ASO’ LED connects to XBee pin 15, which will
blink if the module is associated.
2
Page 7 of 2
7
Page 8 of 27
Finally, there’s a yellow LED labeled ‘CHG’ which indicates if an attached
lithium polymer battery is charging. If a battery is not connected to the Fio,
the LED will be in an undefined state, and most likely be illuminated.
How to Power the Fio v3
The suggested power supply for the Fio v3 is any single-cell lithium
polymer (LiPo) battery. These batteries have a nominal voltage of 3.7V,
which is perfect for supplying power to the 3.3V-operating Fio. LiPos are
awesome, because they’re rechargeable and still pack a lot of power into a
tiny space. Any of our single cell LiPos with JST terminators can connect
directly to the Fio’s onboard JST connector.
As an (immobile) alternative to batteries, the Fio can be powered directly
through the USB connector.
Using the LiPo Charger
The Fio v3 has a LiPo charge management circuit (based around the
MCP73831) built onto it, which handles the signal conditioning required to
safely charge a single-cell LiPo battery.
To use the charge circuit, you’ll obviously need a single-cell LiPo battery
plugged into the Fio. Then connect the board up via USB, so the charge
circuit has a primary voltage source to supply charge to the battery.
The ‘CHG’ LED will indicate the status of the battery charge. If it’s on, the
battery is still charging. Once the ‘CHG’ LED goes off, the battery is fully
charged.
The charge circuit is programmed to charge the battery at 500mA, so, to be
safe, the battery should be no smaller than 500mAH in capacity.
Connecting An XBee
The XBee-footprint connectors on the bottom of the Fio v3 are what make it
so unique. This product is designed to provide a simple interface between
Arduino and XBee, as such a few of the XBee pins come wired up to the
Page 8 of 2
7
Page 9 of 27
ATmega32U4. Most significantly, the serial interfaces of both devices are
wired – the XBee’s ‘DOUT’ pin is connected to the ATmega32U4’s ‘RX’,
and ‘DIN’ is connected to ‘TX’.
XBee’s are controlled and configured over a serial interface. To learn more
about using XBee’s check out their datasheet and various tutorials for help
getting started with these awesomely simple wireless transceivers.
Installing: Windows
Getting the Pro Micro or Fio v3 set up on your computer and in your
Arduino environment can be difficult. Follow along on this page for a step-
by-step guide through the driver installation and Arduino-enabling process.
Windows Driver Installation
A note to Windows 8 users: Before you can install these drivers, you’ll
need to disable driver signature enforcement. Please check out our quick
Disabling Driver Signature Enforcement tutorial for help with that.
Step 1: Download the Driver
Before plugging your board in, get a head start by downloading the
drivers (check the GitHub Repository for the latest files). The same driver
file works for both the Pro Micro and the Fio v3.
Unzip that zip file, and don’t forget where you’ve left its contents. In that zip
file, you should find an INF file, which contains all the information Windows
needs to install the Pro Micro’s driver.
Step 2: Plug in the Pro Micro / Fio v3
When you initially plug the board in, an “Installing device driver software”
bubble notification should pop up in the lower-right corner of your taskbar.
After the green dot circles the grey box a number of times, you’ll probably
get a sad bubble like this:
Page 9 of 2
7
J3 Dcvlcc dnvu softwav: was not sumessmny mstzlled * X (m mlundmk. E mm: "mm . pwognm, lama, dot-mum nvlnlems 15mm: and \Mndms w." up!" an. ynu. 9.x.“ ammm’ —. "us [ask w." n awed wflh mmmmmm pnvllegn rm um Page 10 of 27
Never fear! Windows just doesn’t know where to find our driver.
Note: Some users have experienced issues when plugging the Pro Micro
into a USB 3.0 port. If you experience issues on USB 3.0 ports, try
switching to use a USB 2.0 port.
Step 3: Open the Device Manager
From here, the most straightforward way to install the driver is through the
Device Manager. To get to the Device Manager, click the Start button, then
open the Control Panel. In the Control Panel, click System and
Maintenance, and then open the Device Manager.
Alternatively, you can open the Run prompt (Windows key+R) and type
‘devmgmt.msc’ and click OK.
In the Device Manager, expand the ‘Other devices’ tree, where you should
find a ‘USB IO Board’ with a yellow warning sign over its icon. Right-click
the ‘USB IO Board’ and select Update Driver Software….
Page 10 of 2
7
4 fl SFHQEGJJ‘IML o a (Mum ,, a Duk am. u q. D'splay adapters p ova/comm drivu » a Happy arm mrdlers p h Humminwvm Dar-cs .7 Q 1.“. a a Keyboards u 71] Nice and any painting tin/its b g Munilnu o i Network “my: . 5 o»... deviz= ‘ , {1i “mow a 6 9mm: om: \ s- '1 Fans (COM 51 m 9 I 9mm“; 9 ‘ Scund via» “a o c- Shrlge (mum n a System flakes n 0 umusai SeliaIHu Page 11 of 27
This should spawn an ‘Update Driver Software - USB IO Board’ window.
Step 4: Finding the Driver
In the first window that pops up, click ‘Browse my computer for driver
software’. On the next window, click ‘Browse…’ to search for the driver
you just downloaded. It should be a folder named ‘SFE32U4_Drivers’. After
you’ve selected the ‘driver’ folder, click OK, then select Next.
Windows will attempt to do its driver install thing, but not before complaining
about the driver being unsigned. It’s safe to select ‘Install this driver
software anyway’ on the warning dialog.
After watching the progress bar beam by a few times, you should get a
happy ‘Windows has successfully updated your driver software’ window.
And the ‘Device Manager’ should have a new entry for the ‘SparkFun Pro
Micro (COM ##)’ (or ‘SparkFun Fio V3 (COM##)’ if you have one of those)
under the ‘Ports’ tree.
Page 11 of 2
7
lmmmmm @kammmmntflé.“ @Wnummhmm mvdummheafikdaed'ynkfi mus-mmwvmumwmumm (ultmiv mm Mmm‘mknn'lg) I..- m..." -—-- s- u a . . ._ a...“ M m i.,_ a... 'wmmu-I w... h... .— mm“. W... up... ... mm”... mm I...“ 5......— mm..- M. u... ._ mm..- W. n... __.. “m...“ u. a... J... “m“... u. Page 12 of 27
Take note of which COM port your Pro Micro was assigned. We’ll need it
soon.
Installing the Arduino Addon
We’re still not completely ready for Arduino, but this is the final stretch.
Before you can use the ProMicro in the Arduino IDE, you need to enable it
and activate some super-secret Arduino files.
To begin, download this zip folder, and unzip its contents into a
‘hardware’ directory within your Arduino sketchbook.
Note: These Arduino addon files only work with Arduino 1.5 and up. If
you're using an earlier version of Arduino, either update (and get some
cool new features), or download the older version of the Addon.
Where’s your Arduino sketchbook? Well, by default, it should an ‘Arduino’
folder in your home directory, but to double check you can go to ‘File’ >
‘Preferences’ within Arduino and check the ‘Sketchbook location’ text box.
Just make sure you close all Arduino windows once you’re done.
Once you’ve unzipped that folder into the ‘hardware’ folder within your
Arduino sketchbook (you may actually have to create a hardware folder),
your directory structure should look something like this:
Page 1
2
of 2
7
fit: mm :memm smmm fla ma “Mn 1 and 1mm < m="" m...="" avdmeimd‘="" a="" 5mm="" lab)!="" 5(th="" manny="" (mm-pm="" am="" fan="" mm...="" a..."="" inmhadu="" srquun="" .w="" ,="" (m)="" wm.="" pm="" man="" swmm="" 5pm..="" pm="" man="" 33mm.="" spam.="" mam/m,="" sir-mun="" mm="" wry="" page="" 13="" of="" 27="">
The structure of this directory is critical – it should look something like
“Arduino/hardware/[manufacturer]/[architecture]”, in this case
[manufacturer] is “sparkfun”, and [architecture] is “avr.”
There’s a lot going on in that addon, but one of the most important files is
‘boards.txt’, which will add a few new entries to your ‘Tools > Board’ menu.
To double-check that the board definitions have been added to Arduino,
open up Arduino, and check under the ‘Tools > Board’ menu. There
should be some new entires for ‘SparkFun Pro Micro 8MHz/3.3V’,
‘SparkFun Pro Micro 16MHz/5V’, and other 32U4 boards.
Notice there are two options for Pro Micro - 8MHz and 16MHz. It’s very
important that you select the Pro Micro option that matches your
board’s voltage and speed. Don’t know which board you have? Check the
bottom of the board, where you should find either a ‘5V’ or ‘3.3V’ box
checked.
You should also see your Pro Micro’s COM port under the ‘Tools > Serial
Port’ menu. Select it, and head over to the Example 1 page where we’ll
upload our first piece of code.
Installing: Mac & Linux
If you’re using Mac or Linux, follow the steps below to get your Pro Micro
(or Fio v3) ready to go on your computer. We’re not going to name names
here, but installing the Pro Micro on Mac OS X and Linux is a lot easier
than on other OS’s…
Following these directions is critical to getting your Pro Micro supported
within your Arduino environment!
Board Installation
When you initially plug your Pro Micro into a Mac, it’ll pop up a “Keyboard
Setup Assistant” window. This stems from the Pro Micro’s ability to emulate
an HID USB device (e.g. keyboards and mice) – the Mac thinks your Pro
Micro is a human input device (which it could be! but isn’t yet).
Page 1
3
of 2
7
Page 14 of 27
There’s nothing to configure in this window, so just click the big, red, ‘X’ to
close it.
That’s all there is to it! The CDC (communication device class) portion of
your Pro Micro (the part that handles USB to Serial conversion) should
automatically install on your computer.
Installing the Arduino Addon
In order to use the Pro Micro or Fio v3 in your Arduino IDE, you need to add
a few board definition files to it. That’s what we’ll do in this section. Begin by
downloading the Pro Micro addon files.
Note: These Arduino addon files only work with Arduino 1.5 and up. If
you're using an earlier version of Arduino, either update (and get some
cool new features), or download the older version of the Addon.
With that downloaded, follow these steps to enable the Pro Micro in your
Arduino environment:
1. The addon files are supplied in a zip folder, so you’ll need to extract
the files within first.
2. Find your Arduino sketchbook folder. If you don’t know where it is,
you can locate your sketchbook by looking at the preferences dialog
in your Arduino IDE.
3. If there isn’t already one, create a folder in your sketchbook called
hardware’.
4. Copy the ‘sparkfun’ folder that was unzipped in the first step into the
‘hardware’ folder.
Your directory structure should look something like
“Arduino/hardware/sparkfun/avr.”
5. Restart Arduino, and look under the Tools > Board menu. You should
see a few new options, including ‘SparkFun Pro Micro 5V/16MHz’,
‘SparkFun Pro Micro 3.3V/8MHz’, and ‘'SparkFun Fio V3 3.3V/8MHz’.
Page 1
4
of 2
7
Page 15 of 27
If the boards are visible, select the option that matches your board. If you
have a Pro Micro, make sure you select the correct operating speed and
voltage! Then head over to the next page where we’ll upload our first
sketch!
Example 1: Blinkies!
The Arduino-standard Blink sketch won’t have any visible effect on the Pro
Micro – there’s no LED on pin 13. In fact, the only LEDs on the board are
the power indicator, and RX/TX blinkies. Unlike other Arduino boards,
though, we can control the RX/TX LEDs in our sketch. So let’s get blinking!
Upload the RX/TX Blinky Sketch
Copy and paste the code below, and upload* it to your Pro Micro.
Page 1
5
of 2
7
Page 16 of 27
/*ProMicroTestCode
by:NathanSeidle
modifiedby:JimLindblom
SparkFunElectronics
date:September16,2013
license:PublicDomainpleaseusethiscodehoweveryo
u'dlike.
It'sprovidedasalearningtool.
ThiscodeisprovidedtoshowhowtocontroltheSparkFun
ProMicro'sTXandRXLEDswithinasketch.Italsoserves
toexplainthedifferencebetweenSerial.print()and
Serial1.print().
*/
int RXLED=17;//TheRXLEDhasadefinedArduinopin
//TheTXLEDwasnotsolucky,we'llneedtousepredefined
//macros(TXLED1,TXLED0)tocontrolthat.
//(WecouldusethesamemacrosfortheRXLEDtooRXLED1,
//andRXLED0.)
void setup()
{
pinMode(RXLED,OUTPUT);//SetRXLEDasanoutput
//TXLEDissetasanoutputbehindthescenes
Serial.begin(9600);//Thispipestotheserialmonitor
Serial1.begin(9600);//ThisistheUART,pipestosensorsatt
achedtoboard
}
void loop()
{
Serial.println("Helloworld");//Print"HelloWorld"toth
eSerialMonitor
Serial1.println("Hello!");//Print"Hello!"overhardwareU
ART
digitalWrite(RXLED,LOW);//settheLEDon
TXLED0;//TXLEDisnottiedtoanormallycontrolledpin
delay(1000);//waitforasecond
digitalWrite(RXLED,HIGH);//settheLEDoff
TXLED1;
delay(1000);//waitforasecond
}
Page 1
6
of 2
7
Page 17 of 27
With the code uploaded you should see the RX and TX LEDs take turns
blinking on and off every second. You can also open up the serial monitor
(set to 9600 bps) and see every programmer’s favorite two-word phrase.
Understanding the Sketch
The RX LED is tied to Arduino’s pin 17. You can control it just as you would
any other digital pin. Set it as an OUTPUT , and
digitalWrite([pin],[level]) it HIGH or LOW . The TX LED was not
provided as an Arduino-defined pin, unfortunately, so you’ll have to use a
pair of macros to control it. TXLED1 turns the LED on, and TXLED0 turns
the LED off.
In that sketch, you’ll also notice a pair of Serial initialization statements:
Serial.begin(9600) , Serial1.begin(9600) . That ‘1’ makes a huge
difference. Think of the Pro Micro having two separate serial ports. The one
without the ‘1’ is for communication to and from the computer over USB;
this is what is visible in the Serial Monitor. The Serial1 port is a bonafide,
hardware UART, where your Pro Micro can talk to any serial-enabled piece
of hardware.
If you open up the Serial Monitor, you should only see ‘Hello world’
printed. ‘Hello!’ is being sent out over the hardware UART, where,
presumably, nothing is listening. This begs the age-old question: “if a Pro
Micro is saying ‘Hello!’ over the hardware serial port, and nothing is there to
hear it, does the Pro Micro really say anything at all?.”
Why Does My Board Re-Enumerate Every
Upload?
In order to communicate serially, the Pro Micro emulates a virtual serial
port. Actually, it emulates two different serial ports – one for the bootloader,
and one for the sketch. Since the bootloader and sketch run individually.
Only one of these serial ports is visible at any one time.
When you click ‘Upload’ in the Arduino IDE, the Pro Micro resets itself and
starts its bootloader program. (The bootloader is a low-level program on
the Pro Micro which enables self-programming via serial.) To our operating
system, the bootloader looks like a completely different device, so it gets its
own serial port number. While the Pro Micro is being programmed, the
bootloader serial port will be open. When the sketch upload is finished, the
bootloader will exit, that serial port will be closed, and the regular Pro Micro
serial port will open up.
What this all boils down to is the fact that you have to be patient with Pro
Micros. Every time you upload a new sketch, your OS will need to work its
driver magic before you can open up the COM port. This can take a few
seconds after the code has finished uploading.
Page 1
7
of 2
7
Page 18 of 27
* Note for Windows users: The first time you upload a sketch, it may fail
and give you an error. On top of that Windows will pop up that familiar
‘Device driver software was not successfully installed’ notification. Don’t let
this worry you too much. If you get the error, wait about a minute, and try
uploading again.
Hopefully the upload will succeed the second time, but if it continues to fail,
check out the how to enter the bootloader section of the FAQ. Windows
needs to install the same driver we’ve already installed for the Pro Micro’s
bootloader, but it’s unable to get everything set up before the bootloader
exits.
Example 2: HID Mouse and Keyboard
By far, the Pro Micro’s most revolutionary feature (as far as Arduinos go) is
its true USB functionality. The Pro Micro can be programmed to emulate
any USB device you could imagine. You can even program it to act just like
a mouse, keyboard, or other HID-class USB device.
What is HID? It’s one of the many defined USB device classes. Every USB
device is assigned a class, which defines what its general purpose is. There
are loads of classes – printers, hubs, speakers, and webcams to mention a
few, but in this example we’ll be emulating HID – Human Interface Device.
The ATmega32U4 takes care of the USB-hardware hurdle, but we’ve still
got to clear the firmware one. Time for some example code!
USB Keyboards Made Simple
To emulate a USB keyboard, we’ll be making use of the Keyboard class.
Here are some of the functions made available to us by this class:
Keyboard.write(char) - This function will send a single character
over USB. The character passed can be any standard, printable,
ASCII-defined character: 0-9, a-z, A-Z, space, symbols, etc. Here’s
an example line of code:
Keyboard.write('z')//Thiswillsendasingle'z'charactertoyourcomputer.
Keyboard.print(string) - If you need to perform a series a
Keyboard.write() ’s, consider using just a single
Keyboard.print() . This works similar to Serial.print() – give it a
string of characters and it’ll send that stream of characters over USB.
Keyboard.println(string) is also defined, if you want a
newline/linefeed to close out your string. An example:
Keyboard.print("Hello,world");//This'llsendyourcomputeran'H',followedby'e',followedby...
Page 18 of 2
7
Page 19 of 27
Keyboard.press(byte) and Keyboard.release(byte) give you more
precise control over key presses. They do exactly what you’d expect.
One presses a button down, the other releases a button. Make sure
you release any buttons you press, otherwise you’ll encounter some
wiggyness on your computer.
That’s it. You don’t need to include any libraries or anything, just invoke any
of those functions. Here’s an example sketch to try it out:
int buttonPin=9;//Setabuttontoanypin
void setup()
{
pinMode(buttonPin,INPUT);//Setthebuttonasaninput
digitalWrite(buttonPin,HIGH);//Pullthebuttonhigh
}
void loop()
{
if (digitalRead(buttonPin)== 0)//ifthebuttongoeslow
{
Keyboard.write('z');//senda'z'tothecomputerviaKe
yboardHID
delay(1000);//delaysotherearen'takajillionz's
}
}
In this sketch, connecting pin 9 to ground will make the Pro Micro spit out
a ‘z’ character. If you have a simple, momentary button handy, tie one end
to pin 9 and the other to ground. Otherwise, just use a wire to short 9 to
GND.
After a Keyboard.write() or Keyboard.print() function has been
performed by the Pro Micro, your computer will have to decide what to do
with it. What your computer does with that character, or string of characters,
is entirely dependent on what program it’s running at the time. If you have a
text editor open and active, it’ll print it out there.
USB Mouse Functionality
That covers about half of USB HID library. How about we add a mouse to
the mix now? Implementing a USB HID mouse requires a few more
functions, but it’s still crazy simple. There are five functions provided by
Arduino’s HID class that can be used to implement a mouse:
Page 1
9
of 2
7
Page 20 of 27
Mouse.move(x, y, wheel) tells the computer to move the mouse a
certain number of pixels along either the x, y and/or wheel axis. Each
variable can be any value between -128 and +127, with negative
numbers moving the cursor down/left, positive numbers move the
right/up.
Mouse.press(b) sends a down-click on a button or buttons. The
button(s) will remain “pressed” until you call Mouse.release(b) . The
bvariable is a single byte, each bit of which represents a different
button. You can set it equal to any of the following, or OR (|) them
together to click multiple buttons at once:
MOUSE_LEFT - Left Mouse button
MOUSE_RIGHT - Right Mouse button
MOUSE_MIDDLE - Middle mouse button
MOUSE_ALL - All three mouse buttons
Mouse.click(b) sends a down-click (press) followed immediately by
an up-click (release) on button(s) b. For example, to click the left
and right buttons simultaneously, try this:
Mouse.click(MOUSE_LEFT|MOUSE_RIGHT);//Pressandreleasetheleftandrightmousebuttons
Here’s some example code to show off these functions:
Page 20 of 2
7
Page 21 of 27
/*HIDJoystickMouseExample
by:JimLindblom
date:1/12/2012
license:MITLicenseFeelfreetousethiscodeforanyp
urpose.
Norestrictions.Justkeepthislicenseifyougoontous
ethis
codeinyourfutureendeavors!Reuseandshare.
Thisisverysimplisticcodethatallowsyoutoturnthe
SparkFunThumbJoystick(http://www.sparkfun.com/products/9
032)
intoanHIDMouse.Theselectbuttononthejoystickisse
tup
asthemouseleftclick.
*/
int horzPin= A0;//Analogoutputofhorizontaljoystickpin
int vertPin= A1;//Analogoutputofverticaljoystickpin
int selPin=9;//selectbuttonpinofjoystick
int vertZero,horzZero;//Storestheinitialvalueofeacha
xis,usuallyaround512
int vertValue,horzValue;//Storescurrentanalogoutputof
eachaxis
const int sensitivity= 200;//Highersensitivityvalue=sl
owermouse,shouldbe<=about500
int mouseClickFlag=0;
void setup()
{
pinMode(horzPin,INPUT);//Setbothanalogpinsasinputs
pinMode(vertPin,INPUT);
pinMode(selPin,INPUT);//setbuttonselectpinasinput
digitalWrite(selPin,HIGH);//Pullbuttonselectpinhigh
delay(1000);//shortdelaytoletoutputssettle
vertZero= analogRead(vertPin);//gettheinitialvalues
horzZero= analogRead(horzPin);//Joystickshouldbeinne
utralpositionwhenreadingthese
}
void loop()
{
vertValue= analogRead(vertPin) vertZero;//readvertica
loffset
horzValue= analogRead(horzPin) horzZero;//readhorizon
taloffset
Page 21 of 2
7
Page 22 of 27
if (vertValue!= 0)
Mouse.move(0,vertValue/sensitivity,0);//movemouseo
nyaxis
if (horzValue!= 0)
Mouse.move(horzValue/sensitivity,0,0);//movemouseo
nxaxis
if ((digitalRead(selPin)== 0)&& (!mouseClickFlag))//if
thejoystickbuttonispressed
{
mouseClickFlag=1;
Mouse.press(MOUSE_LEFT);//clicktheleftbuttondown
}
else if ((digitalRead(selPin))&&(mouseClickFlag))//ifthe
joystickbuttonisnotpressed
{
mouseClickFlag=0;
Mouse.release(MOUSE_LEFT);//releasetheleftbutton
}
}
This sketch is set up so that an analog joystick connected to analog pins A0
and A1 can be used to move your mouse cursor.
The loop() of this code continuously monitors the horizontal and vertical
analog values of the joystick and sends the Mouse.move() command based
on what it reads. It’ll move the mouse in steps, depending on what the
sensitivity variable is set to. With sensitivity set to 2, the cursor will move in
either 1 or 2 pixel steps.
The select switch on the joystick is used to control the mouse left click.
Notice this code is using Mouse.press() and Mouse.release() , rather
than just calling a single Mouse.click() . This requires a bit more coding,
but it allows you to do things like drag-and-drop, double click, etc.
For more HID example code, check out the Arduino-supplied examples
under the ‘File’ > ‘Examples’ > ‘09.USB’ menu.
Troubleshooting and FAQ
On this page you’ll find troubleshooting tips and FAQs. Here’s a directory of
the subjects covered:
Troubleshooting
Serial Port Not Showing Up in “Tools > Board” menu
How to Reset to Bootloader
How to Revive a “Bricked” Pro Micro
Page 2
2
of 2
7
h ‘Pvess noomanev mud! comma” mode am code user code Page 23 of 27
Frequently Asked Questions
What are VIDs and PIDs?
How Can I Change the VID and PID on an ATmega32U4?
Why Does my ATmega32U4 Board Show up Twice in the
Device Manager?
How Does the IDE Know Which COM Port to Use?
How Do I Reinstall the Bootloader?
Serial Port Not Showing Up in ‘Tools > Board’
Menu
The Pro Micro can be a finicky little thing. There are a few series of events
that can lead to its serial port being removed from the Arduino IDE’s Serial
Port selection menu. If you can’t see your Pro Micro’s serial port, give these
steps a try:
1. Close all Arduino windows. (Don’t forget to save!)
2. Unplug Pro Micro from your computer.
3. Wait a few seconds for the device to be detached.
4. Plug Pro Micro back in.
5. Open Arduino back up, check the Serial Ports menu again.
Reset to Bootloader
We ship the Pro Micro with a modified version of the Arduino Leonardo
bootloader, with one major enhancement. When a Leonardo (or any device
using the “stock” bootloader) is externally reset, it goes back into the
bootloader…and waits there eight seconds before it starts running the
sketch. For some embedded projects, waiting eight seconds before a
program runs isn’t acceptable, so we modified the bootloader run time.
Leonardo bootloader on reset functionality.
When a Pro Micro is externally reset (by pulling the RST pin low), it’ll only
briefly (<750ms) start the bootloader before continuing on to the sketch. If
you need the bootloader to run longer, resetting twice quickly will get the
Pro Micro to enter bootloader mode for eight seconds.
Pro Micro and Fio v3 reset functionality. Press reset twice, quickly to enter
bootloader mode.
Page 2
3
of 2
7
Page 24 of 27 A USB Device Nok Recognized “ X one am: use dmts ll'uhed n. rimming-nah” mum-mm um mam am run recognize n Fm .mm. 'm whiny INS pmlm mun"; msugL
Resetting the Pro Micro’s, in particular, can be tricky, because there’s no
reset button. The ‘RST’ pins needs to be connected to ground to initiate a
reset. This can be done with a small piece of wire, or an externally
connected button.
Why would you need to enter bootloader mode in the first place. Glad you
asked…
How to Revive a “Bricked” Pro Micro
Incorporating all of the USB tasks on a single chip is an awesome feature
that makes the Pro Micro and boards like it truly unique. But it also places
more stress on a single chip, and if anything goes wrong with that chip, the
board becomes nearly unusable. It’s not uncommon for Pro Micro’s to
become “bricked” and unprogrammable. But, in most cases, the bricking is
reversible!
The most common source of Pro Micro “bricking” is uploading code to it
with an incorrectly set board (e.g. programming a 16MHz/5V Pro Micro
with the board set to 8MHz/3.3V). Also, make sure your sketch doesn’t
mess with the ATmega32U4’s PLLCSR register, or any other register that
sets up USB functionality on the ATmega32U4. The Pro Micro will actually
take code compiled for the wrong operating speed, but when it tries to re-
enumerate, you’ll be greeted with a notification like this:
To revive the Pro Micro, you’ll need to find a way to upload a sketch to it
with the board option correctly set. We can do this with a little help from the
bootloader.
Page 2
4
of 2
7
Page 25 of 27
First, you’ll need to set the serial port to the bootloader. But that port is
only visible when the board is in bootloader mode, so pull the reset line low
twice quickly to invoke the bootloader reset feature discussed above. On
Pro Micro’s, or other devices which don’t have a reset button, you can
either use a wire to quickly short ‘RST’ to ‘GND’ twice, or wire up a
temporary reset button. While the Pro Micro is in the bootloader change
the ‘Tools > Serial Port’ menu to the bootloader COM port. Quick! You’ve
only got eight seconds. On Windows, the bootloader’s COM port number is
usually one number higher than the Pro Micro’s regular port number.
With the serial port set, we’re just about ready to re-upload our sketch. But
first, double check that the board is correctly set. Then reset to
bootloader again, and quickly upload your sketch. Again, you’ll have to be
quick…you’ve only got eight seconds. It may help to press the Upload
keybind – CTRL+U / CMD+U – immediately after resetting.
It can take a few tries to get the timing right. Since the code has to compile
first, it may help to hit upload first and then reset.
Frequently Asked Questions
If you’re having technical difficulties with your Pro Micro or Fio v3, see if any
of the answers to these FAQs help. If not, please get in touch with our tech
support team.
What are VID and PIDs?
VID is short for ‘Vender Identification’ and PID is short for ‘Part
Identification’. In other words, this pair of IDs defines the device. This is
how your computer knows what you’ve plugged in, what drivers to use with
it, what COM port is assigned to it, etc. All native USB devices have a
VID/PID.
All SparkFun ATmega32U4 boards share the same VID – 0x1B4F, and
they all have unique PIDs. 5V Pro Micros lay claim to PIDs 0x9205 and
0x9206 (one for the bootloader, one for the sketch). 3.3V Pro Micros will
show up as 0x9203 and 0x9204 for bootloader and sketch, respectively.
And the Fio v3 has 0xF100 and 0xF101.
How Can I Change the VID and PID on an ATMega32U4
Board?
Every time you upload code the VID and PID are uploaded to the device.
These values are located in the ‘boards.txt’ file and will therefore be
determined by the board you have selected. Keep in mind that if you select
the wrong board you will get the wrong VID/PID uploaded which means the
Page 2
5
of 2
7
Page 26 of 27
computer can’t recognize, and program the board. The VID/PID for the
bootloader is part of the bootloader file. To change this you will need to
recompile the bootloader with the new VID/PID, and upload it.
Why Does my ATMega32U4 Board Show up Twice in Device
Manager?
Both the bootloader and the sketch have their own VID/PIDs. When you
plug in a board the bootloader starts running for a few seconds, and you will
see the board show up in Device Manager based on those VID/PIDs. After
a few seconds, the sketch will start running, and you will see Device
Manager disconnect from the bootloader and connect to the sketch.
How Does the IDE Know Which COM Port to Use?
When the IDE resets the board, the COM port is disconnected from the
computer. The IDE then looks for a new COM port. This is the port it uses.
This is one of those weird things Arduino did to get things to work on this
chip.
How Do I Reinstall the Bootloader?
Check out or reinstalling the bootloader tutorial, which should work for both
ATMega32U4 and ATMega328 boards. If you have the tools to do so,
reinstalling the bootloader is often easier then trying to stay in the
bootloader. Since reinstalling the bootloader puts the board back in factory
settings this will reset the VID/PID numbers allowing your board to work
again.
Resources & Going Further
Thanks for checking out our Pro Micro and Fio v3 Hookup Guide! If you’re
looking for more resources related to these boards, here are some links:
Pro Micro Schematic
Pro Micro EAGLE Files
Fio v3 Schematic
Fio v3 EAGLE Files
ATmega32U4 Datasheet
ATmega32U4 Arduino Addon GitHub Repository
Going Further
Thanks for reading along with our Pro Micro hookup guide! Hopefully now
you’re fully prepared to begin using the Pro Micro in a project of your own.
Here are some tutorials that might be worth checking out as you continue
down the rabbit hole:
Exploring XBees and XCTU
Arduino Programming 101
Page 2
6
of 2
7
Page 27 of 27 htrps://lcam.sparkfun.cKym/tutorials/pro-micro--fio—v3—hookup—guidc 2/12/2015
Arduino Comparison Guide
Connecting Arduino to Processing
Using the Arduino Pro Mini 3.3V
Page 2
7
of 2
7
2
/
12
201
5
htt
p
s://learn.s
p
arkfun.com/tutorials/
p
r
o
-micr
o
--fi
o
-v
3
-hooku
p
-
g
uid
e

Products related to this Datasheet

PRO MICRO ATMEGA32U4 5V/16MHZ
PRO MICRO ATMEGA32U4 3.3V/8MHZ
FIO V3 ATMEGA32U4 EVAL BRD