User Guide
Digi One IAP Family
Digi One IAP
Digi One IAP Haz

Digi One IAP 2
Revision history—90000263
Trademarks and copyright
Digi, Digi International, and the Digi logo are trademarks or registered trademarks in the United States and other
countries worldwide. All other trademarks mentioned in this document are the property of their respective
owners.
© 2019 Digi International. All rights reserved.
Disclaimers
Information in this document is subject to change without notice and does not represent a commitment on the
part of Digi International. Digi provides this document “as is,” without warranty of any kind, expressed or implied,
including, but not limited to, the implied warranties of fitness or merchantability for a particular purpose. Digi
may make improvements and/or changes in this manual or in the product(s) and/or the program(s) described in
this manual at any time.
Warranty
To view product warranties online, visit www.digi.com/howtobuy/terms.
Send comments
Documentation feedback: To provide feedback on this document, send your comments to
techcomm@digi.com.
Customer support
Digi Technical Support: Digi offers multiple technical support plans and service packages to help our customers
get the most out of their Digi product. For information on Technical Support plans and pricing, please contact us
at +1 952.912.3456 or visit www.digi.com/support.
Support portal login: www.digi.com/support/eservice.
Revision Date Description
A 7/19/2002 First revision.
B 5/27/2003 Add pass-through port.
C 2/12/2004 Update Declaration of Conformity.
D November 2016 Updated document to remove outdated references as well as
formatting and editing changes.
EJanuary 2019 Added warning statement for explosive hazard.

Digi One IAP 3
Contents
About the Digi One IAP
Key features . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5
Flexible Industrial Automation support . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 5
Serial port and network protocol support . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6
Package contents . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7
About the Digi One IAP documentation . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7
Other guides and references . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7
Additional software, utilities, and other resources on Digi website . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7
Configure the Digi One IAP using IA profiles
About IA configuration profiles . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 9
Key terms in IA configuration profiles . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 9
Serial bridge profile: master and slave connected to Digi ports . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 10
Modbus profile: serial-connected slave . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 11
Modbus profile: serial-connected master . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 11
DF1 profile: serial-connected slave . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 12
DF1 Profile: serial-connected master . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 12
Omron family profile: serial-connected slave . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 12
Omron family profile: serial-connected master . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 13
Other serial port protocol profile: serial-connected slave . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 13
Other serial port protocol profile: serial-connected master . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 14
Configure a serial-connected slave: generic procedure . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 14
Configure a serial-connected master: generic procedure . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 15
Configure a serial-connected master: TCP/UDP sockets . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 15
Configure a serial-connected slave: other IA protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 15
Configure a serial-connected master: other IA protocol . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 16
Set up COM port redirection . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 16
Administration tasks
Log in as the Administrator . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 18
Update firmware . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 18
Update POST code . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 19
Reset the Digi One IAP configuration to factory defaults . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 19
Reset the Digi One IAP from the web interface . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 19
Reset the Digi One IAP from the command line . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 20
Reset the Digi One IAP using the reset button . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 20
Digi One IAP 4
Enable pass-through port . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 20
Enable the pass-through port . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 20
Run diagnostics . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 20
Interpreting the status LEDs . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 22
Hardware information
Hardware specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 24
Regulatory information . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25
FCC Part 15 Class A . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25
International EMC (Electromagnetic Emissions/Immunity/Safety) standards . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 25
Safety considerations and warnings . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 26
Other considerations . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 26
Environmental considerations and cautions . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 26
Log in as the Administrator . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 26
Reset the Digi One IAP configuration to factory defaults . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 26
Reset the Digi One IAP from the web interface . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 27
Reset the Digi One IAP from the command line . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 27
Reset the Digi One IAP using the reset button . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 27

Digi One IAP 5
About the Digi One IAP
Key features
The Digi One IAP is high-performance, flexible device server that meets the specific requirements of
the industrial automation (IA) market. It delivers simple, reliable and cost effective network
connectivity for serial devices common in industrial automation applications, such as
Programmable Logic Controllers (PLC), CNC/DNC (Computerized Numerical Control/Direct
Numerical Control) equipment, process and quality control equipment, bar-code readers, operator
displays, scales and weighing stations, printers, vision systems, and many other types of
manufacturing equipment.
Features include:
An industrial-strength, ergonomic enclosure designed to mount on a standard DIN rail
EIA-232/422/485 switch select ability for use with virtually any device with a serial port, and
expanded supply voltage range of 9-30 VDC with screw terminal connections or the industry’s
first powered Ethernet option (802.3af) that eliminates the need for an external power supply.
RealPort® COM Port redirection technology
Easy web-based configuration
Multi-master capability
Easy management through SNMP.
Flexible Industrial Automation support
The Digi One IAP support for IA protocols is exceedingly flexible, providing connectivity solutions in a
wide variety of industrial automation environments. It supports the following:
Multi-mastering, which means that a slave using any supported serial port protocol can be
managed by multiple masters; the masters need not use the same network protocol to access
the device server.
A variety of serial-port protocols, including Modbus ASCII, Modbus RTU, DF1 Full-Duplex,
Compoway/F, FINS, and Hostlink. Support extends to what Digi calls the “user-defined” protocol,
which is any serial protocol that has fixed header and trailer strings that bound all message
packets and where each protocol request is followed by a single response.
Almost any other IA serial device, master or slave, as long as the device on the other side of the
network can communicate using TCP sockets, UDP sockets, or COM Port redirection (using
RealPort).
Several methods to encapsulate serial data across a network, including Modbus/TCP, Ethernet/
IP, Allen-Bradley Ethernet, TCP sockets, UDP sockets, and COM Port redirection (using RealPort).

About the Digi One IAP Flexible Industrial Automation support
Digi One IAP 6
Serial port and network protocol support
The following figure depicts serial port and network protocol support.
The following table provides a list of serial-port protocols and compatible network protocols. The
table also lists which protocols support multi-mastering, a feature that allows multiple masters,
each of which may use a different network protocol, to manage a slave simultaneously.
Serial port protocol Network protocols
Multi-master
support
Modbus ASCII and Modbus RTU Modbus/TCP
TCP Sockets
UDP Sockets
RealPort COM Port redirection
Yes
DF1 Full-Duplex Allen-Bradley Ethernet
Ethernet/IP
TCP Sockets
UDP Sockets
RealPort COM Port redirection
Yes
FINS, CompoWay/F, and
Hostlink
TCP Sockets
UDP Sockets
RealPort COM Port redirection
Yes

About the Digi One IAP Package contents
Digi One IAP 7
Package contents
In addition to this manual, the package includes the following items:
A Digi One IAP
A single loopback plug, used to test the port in EIA-232 and EIA-422/485 4-wire full-duplex mode
testing only. The loopback does not work for EIA-422/485 half-duplex connections except when
running diagnostics. If you have trouble running your application in EIA-422/485 2-wire half-
duplex mode, contact Digi Technical Support for additional testing or diagnostic procedures.
A DB9-to-DB9 cable to connect a PC or laptop to the serial port, enabling you to access the Digi
One IAP command line to configure the device.
About the Digi One IAP documentation
This guide provides all the information most users need to set up the device server for industrial
automation applications.
Other guides and references
In addition to this guide, the device server library consists of the following documents:
Digi One IAP Quick Start Guide, included in the Digi One IAP package.
Context-sensitive online help, accessible from the Digi One IAP web interface.
Digi One/PortServer TS Command Reference, available from the Digi One IAP product page on the
Digi website, provides complete descriptions of all commands.
Additional software, utilities, and other resources on Digi website
In addition to the user documentation, the following utilities and software for working with your Digi
One IAP are available on the Digi website (www.digi.com):
Digi Device Discovery Utility, a utility that enables you to discover all Digi devices on our
network and configure an IP address.
DPA-Remote software, a utility that enables you to configure the device server with an IP
address and monitor the serial port.
RealPort software, which installs on your PC and enables you to use the device server’s serial
port as though it were a local serial port on your server.
Simple Network Management Protocol (SNMP) and Management Information Management
Information Bases (MIBs).
Firmware release notes
User-defined TCP Sockets
• UDP Sockets
• RealPort COM Port redirection
Yes
Other serial-port protocols TCP Sockets
• UDP Sockets
• RealPort COM Port redirection
No
Serial port protocol Network protocols
Multi-master
support

Digi One IAP 8
Configure the Digi One IAP using IA profiles
This chapter describes the IA configuration profiles available for the Digi One IAP, and describes how
to configure the Digi One IAP for use in an IA environment. It covers the following topics:
IA configuration profiles:
•About IA configuration profiles on page 9
•Key terms in IA configuration profiles on page 9
•Serial bridge profile: master and slave connected to Digi ports on page 10
•Modbus profile: serial-connected slave on page 11
•Modbus profile: serial-connected master on page 11
•DF1 profile: serial-connected slave on page 12
•DF1 Profile: serial-connected master on page 12
•Omron family profile: serial-connected slave on page 12
•Omron family profile: serial-connected master on page 13
•Other serial port protocol profile: serial-connected slave on page 13
•Other serial port protocol profile: serial-connected master on page 14
Configuration tasks:
•Configure a serial-connected slave: generic procedure on page 14
•Configure a serial-connected master: generic procedure on page 15
•Configure a serial-connected master: TCP/UDP sockets on page 15
•Configure a serial-connected slave: other IA protocol on page 15
•Configure a serial-connected master: other IA protocol on page 16
•Set up COM port redirection on page 16
Configure the Digi One IAP using IA profiles About IA configuration profiles
Digi One IAP 9
About IA configuration profiles
Port profiles simplify serial port configuration by displaying only those items that are relevant to the
currently selected profile.
There are several port profile choices for the Digi One IAP, on the Serial Port Configuration page of
the web interface. If a port profile has already been selected, it appears at the top of the Serial Port
Configuration page in the web interface. Everything displayed on the Serial Port Configuration page
between Port Profile Settings and the links to the Basic Serial Settings and Advanced Serial
Settings depends on the port profile selected.
You can change the selected profile or modify individual settings of a selected profile.
Key terms in IA configuration profiles
IA configuration profiles involve the following key terms and concepts:
Com port redirection
A method of redirecting the serial data generated by a PC-based master to a slave connected to a
port on a network-based device server. In this scheme, the master “thinks” it is communicating with
a device connected to a serial port on the PC system when, in fact, the data is encapsulated in
network packets and transported across the network to a device connected to a serial port on the
Digi One IAP. Many applications, written to support serial communication only, require this service
in order to communicate over the Ethernet.
IA
Abbreviation for industrial automation.
master (or protocol master)
The host or IA device that initiates all communication with a protocol slave.
multi-master
Any configuration in which more than one master simultaneously communicates with a slave.
protocol request
A message generated by the master and sent to the slave that requests information or issues a
command protocol response a message generated by the slave in response to a protocol request
from the master.
slave (or protocol slave)
The device that responds to requests from the master.
TCP socket (or TCP socket service)
A type of network service that uses TCP to ensure reliability. When this guide discusses TCP sockets,
it means that IA protocol messages are encapsulated in network packets and transported across the
network using a standard network service. Many applications support connections to devices using
TCP socket.
TCP tunnel
A TCP socket connection in which a master is connected to the serial port of one device and a slave
to the serial port of another device.
RealPort

Configure the Digi One IAP using IA profiles Serial bridge profile: master and slave connected to Digi ports
Digi One IAP 10
UDP sockets (or UDP socket service) similar to TCP socket service (discussed above) except that the
UDP protocol is used instead of TCP, which means that the reliability service TCP performs is not
provided. Advantages of UDP socket service are slightly less protocol overhead and support for
multicasting. Some applications support connections to devices using TCP socket.
UDP tunnel
A UDP socket configuration in which a master is connected to the serial port of one device and a
slave to the serial port of another device.
Serial bridge profile: master and slave connected to Digi ports
Use the Serial Bridge profile to connect a protocol master to the serial port of one device server and
the protocol slave (or slaves) to the serial port of another device server. This profile, which is often
called a serial bridge, is applicable to environments that use most IA serial port protocols and to
multi-master environments as well. The network is completely transparent to the serial devices,
which means they do not have to be reconfigured.
Configuration requirements
The serial port connections must be configured to meet the requirements of the attached device,
which can be one of the following:
Modbus ASCII
Modbus RTU
DF1 Full-Duplex
Omron Hostlink
Omron FINS
Omron CompoWay/F
A serial port protocol that meets Digi’s definition of a “user defined” protocol, that is, one that
has fixed header and trailer strings that bound all message packets and where each protocol
request is followed by a single response.
For the network connection, Digi recommends TCP sockets, which works regardless of the serial port
protocol specified and provides an efficient and reliable network service. Another option is UDP
sockets, which also works with all the serial port protocols, although it lacks TCP socket reliability.
For Modbus devices, Modbus/TCP is an option, and for DF1 Full-Duplex devices, Allen Bradley
Ethernet and Ethernet/IP are options.
Setup information for slave side
See Configure a serial-connected slave: generic procedure on page 14.
Locate setup information for master side
To configure TCP socket or UDP socket communication, see Configure a serial-connected master:
TCP/UDP sockets on page 15.
To configure any of the other network communication protocols, see Configure a serial-
connected master: generic procedure on page 15.

Configure the Digi One IAP using IA profiles Modbus profile: serial-connected slave
Digi One IAP 11
Modbus profile: serial-connected slave
Use the Modbus profile to connect a slave device (or devices) using Modbus RTU or Modbus ASCII.
This profile is applicable to environments in which multiple masters control the slave or slaves.
Configuration requirements
The serial port connection must be configured for the protocol required by the slave, in this case
Modbus RTU or Modbus ASCII.
The network connection usually does not require configuration. The only exception is if the master
requires COM port redirection. In that case, the master is an application that resides on a PC, such as
a Microsoft Windows system, and communicates only with devices on COM ports.
Setup information
To configure the serial port for Modbus ASCII or Modbus RTU, see Configure a serial-connected
slave: generic procedure on page 14.
To set up a PC and the device server for COM port redirection using RealPort, see Set up COM port
redirection on page 16.
Modbus profile: serial-connected master
Use the Serial Connected Master profile to connect a master device using Modbus RTU or Modbus
ASCII to the serial port of the device server.
Configuration requirements
The serial port connection must be configured for the protocol required by the master, in this case
Modbus RTU or Modbus ASCII. If the remote slave supports TCP socket communication, which is the
case if the remote slave is connected to another device server, Digi recommends this option.
Modbus/TCP is the other supported network option. This master can be configured to control up to
8 slaves.
Setup information
To configure the port for Modbus ASCII or Modbus RTU and the network for TCP socket
communication, see Configure a serial-connected master: TCP/UDP sockets on page 15.
To configure the port for Modbus ASCII or Modbus RTU and the network for Modbus/TCP, see
Configure a serial-connected master: generic procedure on page 15.

Configure the Digi One IAP using IA profiles DF1 profile: serial-connected slave
Digi One IAP 12
DF1 profile: serial-connected slave
Use DF1 Serial-Connected Slave Profile to connect a slave device (or devices if multiple slaves are
connected) using the DF1 Full-Duplex protocol.
Configuration requirements
The serial port connection must be configured for the protocol required by the slave, in this case,
DF1 Full-Duplex.
The network connection usually does not require configuration. The only exception is if the master
requires COM port redirection. In that case, the master is an application that resides on a PC, such as
a Microsoft Windows system, and communicates only with devices on COM ports.
Setup information
To configure the serial port of the device server for DF1 Full-Duplex, see Configure a serial-
connected slave: generic procedure on page 14.
To set up a PC and the device server for COM port redirection using RealPort, see Set up COM port
redirection on page 16.
DF1 Profile: serial-connected master
Use the DF1 Serial-Connected Master profile to connect a master device using the DF1 Full-Duplex
and protocols to the serial port.
Configuration requirements
The serial port connection must be configured for the protocol required by the master, in this case,
DF1 Full-Duplex. If the remote slave supports TCP socket communication, which is the case if the
remote slave is connected to another device, Digi recommends this option. For DF1 Full-Duplex
users, Allen Bradley Ethernet and Ethernet/IP are other supported network options.
Setup information
To configure the port for DF1 Full-Duplex and the network for TCP socket communication, see
Configure a serial-connected master: TCP/UDP sockets on page 15.
To configure the port for DF1 Full-Duplex and the network for Allen Bradley Ethernet or Ethernet
IP, see Configure a serial-connected master: generic procedure on page 15.
Omron family profile: serial-connected slave
Use this profile to connect a slave device (or devices) using one of the Omron serial port protocols,
Hostlink, FINS, or CompoWay/F.

Configure the Digi One IAP using IA profiles Omron family profile: serial-connected master
Digi One IAP 13
Configuration requirements
The serial port connection must be configured for the protocol required by the slave, Hostlink, FINS,
or CompoWay/F.
The network connection usually does not require configuration. The only exception is if the master
requires COM port redirection. In that case, the master is an application that resides on a PC, such as
a Microsoft Windows system, and communicates only with devices on COM ports.
Setup information
To configure the serial port of the device server for any of the Omron protocols, see Configure a
serial-connected slave: generic procedure on page 14.
To set up a PC and the device server for COM port redirection using RealPort, see Set up COM port
redirection on page 16.
Omron family profile: serial-connected master
Use the Omron Family serial-connected master profile to connect a master device to the serial port
using one of the Omron serial port protocols, Hostlink, FINS, or CompoWay/F.
Configuration requirements
The serial port connection must be configured for the protocol required by the master, in this case
Hostlink, FINS, or CompoWay/F. If the remote slave supports TCP socket communication, which
includes a slave connected to another device server, Digi recommends this network option. UDP
Sockets is another supported network option.
Setup information
To configure the port for one of the Omron protocols and the network for TCP or UDP socket
communication, see Configure a serial-connected master: TCP/UDP sockets on page 15.
Other serial port protocol profile: serial-connected slave
Use the serial-connected slave profile to connect a slave device to the serial port using any IA serial
port protocol not previously discussed in this guide.

Configure the Digi One IAP using IA profiles Other serial port protocol profile: serial-connected master
Digi One IAP 14
Configuration requirements
In this configuration, you do not set up the port of the device server for an IA protocol; instead:
If you will use RealPort for COM port redirection, you simply set up the port for RealPort.
If you will have the master access the device server using TCP or UDP sockets, configure the
standard serial port parameters required by the attached slave, such as line speed, number of
data bits, and parity scheme.
No special network configuration is required in either case.
Setup information
To set up the device server for RealPort, see Set up COM port redirection on page 16.
To set up the port for an “unsupported” IA protocol, see Configure a serial-connected slave: other
IA protocol on page 15.
Other serial port protocol profile: serial-connected master
Use the serial-connected master profile to connect a master device to the serial port using any IA
serial port protocol not previously described in this section.
Configuration requirements
In this configuration, you do not set up the port of the device server for an IA protocol. Instead, you
configure the standard serial port parameters required by the attached master, such as line speed,
number of data bits, and parity scheme, and then configure the port for autoconnection.
Setup Information
See Configure a serial-connected master: other IA protocol on page 16.
Configure a serial-connected slave: generic procedure
Use this procedure when a protocol slave is connected to the serial port of the device server. If the
associated master requires COM port redirection, see Set up COM port redirection on page 16.
1Access the web interface by entering the device server IP address in a browser’s URL window.
2Log in to the device server as root. The default password is dbps.
3From the main menu, choose Setup Wizards > Industrial Protocols.
4Choose the serial port protocol required by the slave that is connected to the serial port.
Configure the Digi One IAP using IA profiles Configure a serial-connected master: generic procedure
Digi One IAP 15
5For device type, select Slave.
Any number of network masters can communicate with the slave.
Configure a serial-connected master: generic procedure
Use this procedure when a protocol master is connected to the serial port of the device server. If the
master requires TCP socket or UDP socket communication, see Configure a serial-connected master:
TCP/UDP sockets on page 15.
1Access the web interface by entering the device server IP address in a browser’s URL window.
2Log in to the device server as root. The default password is dbps.
3From the main menu, select Setup Wizards > Industrial Protocols.
4Choose the serial port protocol required by the master.
5For Mode, select Master.
6Configure up to 8 network slaves.
Configure a serial-connected master: TCP/UDP sockets
Use this procedure in the following situations:
•When a protocol master using one of the supported serial port protocols (Modbus ASCII,
Modbus RTU, DF1 Full-Duplex, FINS, Hostlink, CompoWay/F or a protocol that meets Digi’s
definition of a “user-defined” protocol) is connected to the serial port.
•When the master requires TCP or UDP sockets for network communication.
1Access the web interface by entering the device server IP address in a browser’s URL window.
2Log in to the device server as root. The default password is dbps.
3From the main menu, choose Setup Wizards > Industrial Protocols.
4Choose the serial port protocol required by the master.
5For Mode, select Master.
6Configure up to 8 network slaves.
7Change the default socket number only if required.
Configure a serial-connected slave: other IA protocol
Use this procedure in the following situations:
•When the device connected to the serial port is a slave that is using a “non-supported” serial-
port protocol, that is, the serial port protocol is not Modbus ASCII, Modbus RTU, DF1 Full-
Duplex, FINS, Hostlink, CompoWay/F, or a protocol that meets the definition of a “user-
defined” protocol.
•When you do not want to set up the device server for RealPort COM Port redirection.
Configure the Digi One IAP using IA profiles Configure a serial-connected master: other IA protocol
Digi One IAP 16
•When multiple masters will not be communicating with this slave.
1Access the web interface by entering the device server IP address in a browser’s URL window.
2From the main menu, select Configure > Port.
3From the Port configuration screen, set the Device type to Printer, adjust other serial port
communication parameters as required by the connected slave, and click Submit.
4Click Advanced, check Binary Mode, and click Submit.
Configure a serial-connected master: other IA protocol
Use this procedure when the device connected to the serial port is a master that is using a “non-
supported” serial-port protocol. That is, the serial port protocol is not Modbus ASCII, Modbus RTU,
DF1 Full-Duplex, FINS, Hostlink, CompoWay/F, or a protocol that meets the definition of a “user-
defined” protocol.
1Access the web interface by entering the device server IP address in a browser’s URL window.
2Log in to the device server as root. The default password is dbps.
3From the main menu, select Configure > Port.
4From the Port configuration screen, set the Device type to Modem In, adjust other serial port
communication parameters as required by the connected master, then click Submit. The
Terminal type field does not matter.
5To configure the port to launch an automatic connection to the slave, click Advanced.
6Select Enable Autoconnect.
7Specify the IP address of the slave.
8Specify a TCP port to use for this connection. If this is a connection to another device server, use
2101 as the TCP port number.
9To have the autoconnection to launch immediately, choose Force DCD.
10 Choose Binary Mode.
11 To enable UDP sockets (instead of TCP sockets), choose UDP Serial, use the online help for
information on completing configuration task.
12 When you complete configuration, click Submit.
Set up COM port redirection
Use these procedures when a slave is connected to the serial port of the device server and the
master, which must be an application residing on a Microsoft Windows system, requires COM port
redirection.

Configure the Digi One IAP using IA profiles Set up COM port redirection
Digi One IAP 17
Steps for configuring COM port redirection
To enable Com port redirection--which requires that RealPort software be running on the same PC
as the master application--complete the following tasks:
1Configure the serial port for RealPort (See Configure the serial port for RealPort on page 17.).
2Install RealPort software on a host system. See Install RealPort software on page 17.
3Configure the port on the RealPort PC.
See the PC’s documentation for information on configuring serial ports.
Configure the serial port for RealPort
Use this topic for information on configuring the Digi One IAP serial port.
1Access the Digi One IAP configuration from a web browser by entering IP address for the device in
the browser’s URL window.
2Log on to the Digi One IAP as the root user. The default password is dbps.
3Do one of the following:
Install RealPort software
Use this topic for information on installing RealPort software on a Microsoft Windows.
1Go to https://www.digi.com/support/productdetail/drivers.
2From the OPERATING SYSTEM SPECIFIC DRIVERS: drop-down list, select your operating system. A
list of drivers appears.
3Click the link for your operating system, and save the .zip file to your hard drive.
4Navigate to the location of the .zip file, and double-click the file to unzip the files.
5Select the appropriate setup file for your system, and follow the on-screen prompts.
If the slave is using a supported serial port
protocol
If the slave is not using a supported serial
port protocol
1Choose Port from the main menu.
2. Set the Device type to IA.
3. Click Submit.
1 Choose Setup Wizards > RealPort.
2. Use the wizard to complete
configuration.

Digi One IAP 18
Administration tasks
This topic discusses the administration tasks that need to be performed on Digi devices periodically.
Log in as the Administrator
The administrator or root user, is required to perform most administrative tasks. To log in as the
administrator:
1At the Login prompt, enter the user name for the administrator: root.
2At the password prompt, enter the root password. The default password is dbps, which will work
unless the root password has been changed.
Update firmware
You can upgrade the firmware for Digi One IAP from the web interface using the HTTP or TFTP
protocol.
Upgrade firmware from the web Interface using HTTP
1Download a copy of the firmware.
2Access the web interface by entering the Digi One IAP IP address in a browser’s address bar.
3A login prompt is displayed. For the username, enter root. For the password, enter dbps.
4From the web interface’s main menu, select Administration > HTTP Upgrade.
5Navigate to the firmware and then click Submit.
When the Digi One IAP determines that the firmware image is valid, it prompts you to reboot.
6Reboot the device.
Upgrade firmware from the web Interface using TFTP
1Download a copy of the firmware to a server running TFTP.
2Access the web interface by entering the Digi One IAP IP address in a browser’s address bar.
3A login prompt is displayed. For the username, enter root. For the password, enter dbps.
4From the web interface main menu, select Administration > TFTP Upgrade.
5Enter the firmware image name and the IP address of the TFTP server.

Administration tasks Update POST code
Digi One IAP 19
6Click Submit.
7When the device server determines that the firmware image is valid, it prompts you to reboot.
Reboot the device by selecting Reboot > Continue.
Upgrade firmware from the command line
To upgrade firmware from the command line to use the boot command. See the Digi One and
PortServer TS Family Command Reference (Digi part number 90001535) for the boot command
description.
Update POST code
You can upgrade POST code from a file or TFTP. Typically, POST upgrades are not required and
should only be done if the firmware release notes indicate that this step is required.
The preferred method is to use your web browser and download the file onto your PC. TFTP is often
used in UNIX environments and is supported as well.
This procedure assumes that:
You have already downloaded the firmware file from the Digi web site
TFTP is running (if you are using the TFTP option)
1Open a web browser and enter the device server’s IP address in the URL window.
2When the device server prompts you to log in, enter the following:
•Username is root
•The root default password is dbps
3From the main menu, select Administration > Update Firmware.
4From the dropdown menu, select Boot/POST.
5Click Browse to select the Boot/Post image.
6Click Update.
Reset the Digi One IAP configuration to factory defaults
You can reset the Digi One IAP configuration to factory defaults from the web interface or command
line, or by pressing the reset button on the Digi One IAP hardware.
Note When you reset the device to factory defaults, all previous configuration changes will be lost.
Reset the Digi One IAP from the web interface
1Access the web interface by entering the device server IP address in a browser’s URL window.
2Log in to the device server as root. The default password is dbps.
3From the main menu, choose Administration > Factory Default Settings.
4Enable or disable Keep IP address settings and administrator password as desired.
5Click Restore to reset the configuration.

Administration tasks Enable pass-through port
Digi One IAP 20
Reset the Digi One IAP from the command line
To reset the Digi One IAP from the command line, use the revert and boot commands. See the Digi
One and PortServer TS Family Command Reference (Digi part number 90001535) for command
descriptions.
Reset the Digi One IAP using the reset button
1Use a pen or other object that is pointed but not sharp to press and hold the recessed button
(located on the side with the Ethernet connection).
2While holding down the button, power on the device server.
3When a 1-5-1 LED pattern appears, release the button.
The device boots up and restores to the default configuration.
Enable pass-through port
The Digi One IAP has a second DIP switch on the top of the device for enabling the pass-through
port. When the pass-through port DIP switch is enabled (ON), the DIP switch bank for EIA-232/422/
485 operates for the screw terminal port only. The screw terminal port is port 1. The DB-9 serial port
operates as the second port supporting only EIA-232.
The following are the procedures to enable the pass-through port as well as diagnostic and
troubleshooting tips for using the pass-through port.
Enable the pass-through port
1While the unit is off, slide the pass-through switch to ON.
2Power up the unit.
3Install RealPort from the Access Resource CD under Software.
Note If the unit has already been configured and you are adding the pass-through port, reboot the
unit after enabling the pass-through port. If RealPort is installed before the pass-through
port is enabled, the driver must be reinstalled. Configure the pass-through port as the
Master port. See Configure a serial-connected slave: other IA protocol.
Run diagnostics
The following diagrams are for the screw terminal loopback used when testing two port
functionality with the user diagnostics. When running diagnostics, connect to the DB-9. When
running user diagnostics in single port mode, remove the TS-9 loopback.

Administration tasks Run diagnostics
Digi One IAP 21
Screw
terminal
connector
Signal
RS232 RS485
Pin 1 RTS RTS+
Pin 2 DTR RTS-
Pin 3 Tx TX+
Pin 4 RI TX-
Pin 5 GND GND
Pin 6 Rx RX+
Pin 7 DSR RX-
Pin 8 CTS CTS+
Pin 9 DCD CTS-
232 loopback for screw
terminal
Connect Pin 1 to 8
Connect Pins 2, 4, 7, 9
Connect Pin 3 to 6

Administration tasks Interpreting the status LEDs
Digi One IAP 22
Interpreting the status LEDs
Use the following table to interpret LED activity.
485 Loopback for screw
terminal
Connect Pin 1 to 8
Connect Pin 2 to 9
Connect Pin 3 to 6
Connect Pin 4 to 7
LED label Color State Indicates
Power Green On Power detected.
Off No power detected.
Link Red On No network detected.
Off Network detected.
Tx/Rx Green On Network traffic.
Off No network traffic.
Diag Red Blinking 1-1-1 Starting the device’s operating system.
Blinking 1-3-1 Starting the TFTP process.
Blinking 1-5-1 Configuration set to factory defaults.
Steady blinking Device seeking an IP address from a DHCP
server.
Blinking 4-1-1 Problems with the operating system. Contact
Customer support.
Blinking 9-1-1
Tx/Rx Green On Serial port activity.
Off No serial port activity.
RTS Green On RTS is on.
Off RTS is off.
CTS Green On CTS is on.
Off CTS is off.
DTR Green On DTR is on.
Off DTR is off.

Administration tasks Interpreting the status LEDs
Digi One IAP 23
DSR Green On DSR is on.
Off DSR is off.
DCD Green On DCD is on.
Off DCD is off.
LED label Color State Indicates

Digi One IAP 24
Hardware information
This topic provides hardware specifications, regulatory and safety statements, and certifications for
the Digi One IAP.
Hardware specifications
CAUTION! This unit has two power inputs. For total isolation from electrical shock and energy
hazard, disconnect both power inputs.
WARNING! EXPLOSIVE HAZARD. DO NOT DISCONNECT EQUIPMENT UNLESS POWER HAS BEEN
SWITCHED OFF OR THE AREA IS KNOWN TO BE NON-HAZARDOUS.
Category Specification Value
Power requirements 2-Pin Terminal Connector
(green))
+9 to +30 VDC 500 mA (max) external power
supply
RJ-45 Powered Ethernet +37 to +57 VDC 100 mA (max) (802.3af-
compliant)
Environmental Ambient temperature 0 to 60 degrees C
Relative humidity not to exceed 95% non-
condensing over the temperature range of
from 4C to 45C. Above 45C, constant absolute
humidity shall be maintained.
Relative humidity 5 to 90% non-condensing
Mechanical Width 101 mm
Height 22.5 mm
Depth 120 mm

Hardware information Regulatory information
Digi One IAP 25
Regulatory information
FCC Part 15 Class A
Radio Frequency Interference (RFI) (FCC 15.105)
This equipment has been tested and found to comply with the limits for Class A digital devices
pursuant to Part 15 of the FCC Rules. These limits are designed to provide reasonable protection
against harmful interference in a residential environment. This equipment generates, uses, and can
radiate radio frequency energy, and if not installed and used in accordance with the instruction
manual, may cause harmful interference to radio communications. However, there is no guarantee
that interference will not occur in a particular installation. If this equipment does cause harmful
interference to radio or television reception, which can be determined by turning the equipment off
and on, the user is encouraged to try and correct the interference by one or more of the following
measures:
Reorient or relocate the receiving antenna.
Increase the separation between the equipment and the receiver.
Connect the equipment into an outlet on a circuit different from that to which the receiver is
connected.
Consult the dealer or an experienced radio/TV technician for help.
Labeling Requirements (FCC 15.19)
This device complies with Part 15 of FCC rules. Operation is subject to the following two conditions:
(1) this device may not cause harmful interference, and (2) this device must accept any interference
received, including interference that may cause undesired operation.
Modifications (FCC 15.21)
Changes or modifications to this equipment not expressly approved by Digi may void the user's
authority to operate this equipment.
Cables (FCC 15.27)
Shielded cables must be used to remain within the Class A limitations.
International EMC (Electromagnetic Emissions/Immunity/Safety)
standards
The Digi One IAP complies with the requirements of following Electromagnetic Emissions/Immunity/
Safety standards:
Electromagnetic Emissions
Standards Product Safety Standards
EN55022 Class A
EN61000-6-2
VCCI
AS/NZS 3548
UL 60950
EN60950

Hardware information Safety considerations and warnings
Digi One IAP 26
Safety considerations and warnings
To ensure safe operation of your Digi One IAP, observe theseconsiderations and warni ngs:Do not attempt to service the power supply that comes with the Digi One IAP. This sealed unit
contains no user-serviceable parts or adjustments. Do not open or tamper with the power
supply.
Carefully inspect the work area in which the Digi One IAP will be located to ensure against
hazards such as damp floors, ungrounded power extension cords, and missing ground
connections.
Before operating the Digi One IAP, ensure that external power sources comply with the
requirements listed in the specifications. If you are not sure of the type of power source, contact
your dealer or power company.
Ensure that the ampere rating of all equipment plugged into wall outlets does not exceed the
capacity of the outlet.
Ensure that the cover is secure on completion of installation to reduce safety hazards.
Other considerations
If you require an extension cord, ensure that the ampere rating of all equipment plugged into the
extension cord does not exceed the ampere rating of the cord.
If the Digi One IAP is exposed to moisture or condensation, disconnect it from the power source
immediately and obtain service assistance.
If the Digi One IAP exhibits unexpected behavior, such as smoking or becoming extremely hot,
disconnect it from power sources immediately and then obtain service assistance.
Environmental considerations and cautions
To ensure safe and efficient operation of your Digi device, observe these environmental
recommendations and cautions:
Do not position the Digi device near high-powered radio transmitters or electrical equipment,
such as electrical motors or air conditioners. Interference from electrical equipment can cause
intermittent failures.
Do not install the device in areas where condensation, water, or other liquids may be present.
These may cause safety hazards and equipment failure.
Log in as the Administrator
The administrator or root user, is required to perform most administrative tasks. To log in as the
administrator:
1At the Login prompt, enter the user name for the administrator, which is root.
2At the password prompt, enter the root password. The default password is dbps, which will
work unless the root password has been changed.
Reset the Digi One IAP configuration to factory defaults
You can reset the Digi One IAP configuration to factory defaults from the web interface, command
line, or by pressing the reset button on the Digi One IAP hardware.
Note When you reset the device to factory defaults, all previous configuration changes will be lost.
Hardware information Reset the Digi One IAP configuration to factory defaults
Digi One IAP 27
Reset the Digi One IAP from the web interface
1Access the web interface by entering the device server IP address in a browser’s URL window.
2Log in to the device server as root. The default password is dbps.
3From the main menu, choose Administration > Factory Default Settings.
4Enable or disable Keep IP address settings and administrator password as desired.
5Click Restore to reset the configuration.
Reset the Digi One IAP from the command line
To reset the Digi One IAP from the command line, use the revert and boot commands. See the Digi
One and PortServer TS Family Command Reference (Digi part number 90001535) for command
descriptions.
Reset the Digi One IAP using the reset button
1Use a pen or other object that is pointed but not sharp to press and hold the recessed button
(located on the side with the Ethernet connection).
2While holding down the button, power on the device server.
3When a 1-5-1 LED pattern is displayed, release the button.
The device boots up and the configuration is restored to defaults.
Products related to this Datasheet
ETHERNET TO SER RS-232/422/485