TMS320C2000 DC/DC Kit QS Guide Datasheet by Texas Instruments

View All Related Products | Download PDF Datasheet
I TEXAS INSTRUMENTS
Quick Start GuideSPRUFR7 – July 2008
TMS320C2000 DSC DC/DC Developer’s Kit
Providing a great way to experiment and learn about digital power control, the TMS320C2000™ DC/DCDeveloper’s Kit highlights the TMS320C28x™ digital signal controller (DSC) as a multi-rail controller formulti-phase applications. This kit contains a power motherboard which has eight TI PowerTrain™modules, small and efficient 10 Amp synchronous buck power stages, and can interface with any of the TIplug-in controlCARDs. The board requires a single 9-V DC supply and has a separately switched andfused rail as the input voltage bus to the Buck modules. This allows for safe, convenient softwareexperimentation and debug without the risk of hardware damage. The software package for this kit usesthe TMS320F28x DSC to digitally control the output voltage, ramp rates and sequence timing for each ofthe eight DC/DC voltage rails.
SPRUFR7 – July 2008 TMS320C2000 DSC DC/DC Developer’s Kit 1Submit Documentation Feedback
TEXAS INSTRUMENTS
www.ti.com
Features of the DC/DC Developer’s Kit include:Eight non-isolated 10-Amp SyncBuck DC/DC power stages (no heat-sink required)with built in MOSFET driversClosed loop digital control with voltage feedback using F28x on-chip ePWM andADC
Sequencing and ramp rate parameters in software allow DC/DC rails to becontrolled independently and in an organized mannerVoltage input and output measurements via ADCTemperature measurement for each channel monitored by ADCCurrent measurement for each channel monitored by ADCOver-current protection and fault flag detection via GPIO8 x LED indicators for diagnostics and fault statusUART communications header available for host controlHost GUI, a friendly way to control / demo the application, based on open sourceC# freeware
Hardware Developer’s Package is available and includes schematics, bill ofmaterials, Gerber files, etc
CAUTION
During experimentation the lamp loads (LMP1-LMP8 – seeHardware Overview) may become HOT if output voltagesare left running for an extended time (avoid if possible). DONOT TOUCH until the loads cool down.
2TMS320C2000 DSC DC/DC Developer’s Kit SPRUFR7 – July 2008Submit Documentation Feedback
Tms INSTRUMENTS 3V m Main POWEHSWU DC Bus (SWZp Bock Module Luads Aclive Lo: :1 1 Emuhlm power Juwu DMM Header JTAG / Herder Cm; [ED Alriy BOD. Junpers Buck Modfles Acfive Load 2
1 Hardware Overview
www.ti.com
Hardware Overview
The DC/DC Developer’s Kit consists of eight identical buck power stages. The input bus voltage for allstages is 9 V. Shown below is a diagram of the DC/DC Developer’s Kit board and some key features.
Table 1. Hardware Components
Component Description
9V In DC power supply from plug pack (12V supply may also be used)
Main Pwr SW1 – Master power switch for entire EVM
DC Bus SW2 Power switch for Vin to buck stages only. When off the DIMM controller card will still operate (next tothe DC bus switch is a resettable fuse)
Buck 1-8 Buck power stage modules with temperature/current measurement and over current protection
Load 1-8 Load terminals and/or buck converter output - next to each terminal block is a light bulb or “visual” load (thesedraw approx 300 mA hot)
Active Load 1/2 Switched loads controlled by the ECAP peripheral via software. These loads are connected to the output ofbuck 1 & 5 respectively. PR1, PR2, or PR3 will need to be populated for each active load module to functioncorrectly. (ECAP peripheral not available on F28044)
DMM Header Provides convenient access to the outputs of the eight buck converters
Emulator Pwr Sets the voltage sent to power the emulator. No jumper means no power will be sent to an emulator, a jumperat 5V will power the emulator with 5 V, and a jumper at 3V3 will power the emulator with 3.3 V.
Boot Jumpers Controls how the F280x will boot.If no jumpers are placed the target will boot from flash.If a jumper is placed at 34, the target will boot from the SCI.If a jumper is placed at 29 and 34, the target will boot from RAM.
Comms Serial communications UART (allows connection to the external GUI)
SPRUFR7 – July 2008 TMS320C2000 DSC DC/DC Developer’s Kit 3Submit Documentation Feedback
Tms INSTRUMENTS
2 Hardware Set Up
2.1 Test drive with GUI – (skip if you need only emulation support)
2.2 Code Composer Studio Software Development Platform Emulation - Additional Steps
Hardware Set Up
www.ti.com
All the hardware needed to get started (except the emulator) is included in this package (suggestedemulators are listed near the end of this document). The application-specific motherboard provided in thiskit can be used in one of two ways:
1. Test Drive Using the provided GUI application, the user does not require Code Composer Studio™software or emulation tools. This provides a great way to run or demo the application code quickly andsee what functionality the hardware offers. Note: exactly the same functionality can be achieved byusing the Code Composer Studio Watch Window and slider features during emulation in the secondmode.
2. Code Composer Studio Software Development Platform – With the project code provided, theapplication can be modified, compiled, loaded and run in a development environment. Code ComposerStudio and Emulation HW tools are required for this.
Follow these steps to set up the hardware for either the GUI or Software Development Platform:
Step 1. Unpack the DIMM style controlCARD.
Step 2. Spread open the winged retaining clips on connector J2.
Step 3. Sit the DIMM card loosely in the connector slot. Align the 2 keyed notches carefully andposition the card bottom corners inside the retaining clips (see picture below).
Step 4. Push vertically down using even pressure from both ends of the card until the clips snap andlock. (note: to remove or eject the card simply spread open the retaining clips with thumbs).
Step 5. Be sure switch 1 (SW1) is in the off position and connect the included power supply to thepower jack.
Step 1. Plug in the serial cable provided to connector J4 making sure the red wire aligns with the Rxpin on EVM.
Step 2. Insert a jumper in position 34 on the board’s boot pins.
Step 3. Plug the DB9 connector into your PC using either a serial port or a serial-to-USB converterdongle.
Step 4. Turn on the power once you are done with the TI Software download (see Software Set UpGUI-TestDrive).
Step 1. Depending on your emulator type, place the jumper at J2 to either the 3.3-V or 5-V position.
Step 2. Connect the JTAG emulator cable to connector J1.
Step 3. Turn on power once you are done with the TI Software download, see Software Set Up -Code Composer Studio Development. For full details (schematics, pin-out table, etc) of thehardware see the Hardware Developer’s Package, EightChBuck-HWdevPkg. See SoftwareSet Up for the download location.
TMS320C2000 DSC DC/DC Developer’s Kit4 SPRUFR7 – July 2008Submit Documentation Feedback
TEXAS INSTRUMENTS http://www.ti.com/f28xkits http://www.ti.com/f28xkits
3 Software Set Up
www.ti.com
Software Set Up
The DC/DC Developer’s Kit application software example, GUI, step-by-step lab style documentation, andother useful soft collateral is available on the TI website. If you already have your own software projectand do not require this collateral, skip this section. As explained in the hardware set up section, the targetmother board can be run either with the GUI or Code Composer Studio. The GUI executable file is foundas part of the main software download. Follow the steps below for either case.
To run any of the application-specific software in Code Composer Studio, first you must install thebaseline code, which contains the header files, libraries, etc. If you already have the baseline softwareinstalled, skip the baseline install steps and go to the DC/DC Developer’s Kit section.
To download the free TI soft collateral follow these steps:
Step 1. Baseline soft collateral and hardware documents (skip this if you already have this softwareinstalled)
a. On an Internet browser type: http://www.ti.com/f28xkitsb. At the C2000™ DSP collateral page, choose the Experimenter’s Kit download linkc. When prompted, fill in the TI customer registration details and click okd. Save the .zip file to the directory of your choicee. Unzip the file and run the install program Baseline Software Set Upf. The installer will create the following default directories:
C:\TI_F28xxx_SysSW
~Docs
~GeneralPurposeGUI
~SupportFiles
FlashingLeds
C:\TI_F28xxx_SysHW
CC280xxHWdevPkg
CC2833xHWdevPkg
DockingStnHWdevPkg
Step 2. DC/DC Developer’s Kit soft collateral and hardware documents
a. On an Internet browser type: http://www.ti.com/f28xkitsb. Then choose the DC/DC Developer’s Kit link.c. When prompted, fill in the TI customer registration details and click ok.d. Save the .zip file to the directory of your choice.e. Unzip the file and run the install program Eight Channel Buck Software Set Up.f. The installer will create the following default directories:
C:\TI_F28xxx_SysSW
EightChannelBuck
~Docs
~GUI
C:\TI_F28xxx_SysHW
EightChBuck-HWdevPkg
SPRUFR7 – July 2008 TMS320C2000 DSC DC/DC Developer’s Kit 5Submit Documentation Feedback
TEXAS INSTRUMENTS hug://www.b|ackhawkrdsg.com htlg://www.Sgectrumdigitalcom mtg://www.Ii.com/128>
4 Running the Application
5 Emulators
6 References
Trademarks
Running the Application
www.ti.com
To run the application specific hardware, choose either TestDrive-GUI or CCS-Development options belowand follow the appropriate steps.
Step 1. TestDrive-GUI
a. Open the GUI Quick Start Guide, QSG-EightChannelBuck-GUI.pdf, found in:C:\TI_F28xxx_SysSW\EightChannelBuck\~Docs\
b. Go to directory C:\TI_F28xxx_SysSW\EightChannelBuck\~GUI
c. Open EightChannelBuck-GUI.exe
d. Follow the step-by step instructions found in the Quick Start Guide
Step 2. Code Composer Studio - Development
a. If you have emulation tools and Code Composer Studio already installed and active, loadthe project file EightChannelBuck.pjt found in:C:\TI_F28xxx_SysSW\EightChannelBuck\
b. See the EightChannelBuck.pdf for a step-by-step walk through of how to compile and runthe various labs. This document can be found inC:\TI_F28xxx_SysSW\EightChannelBuck\~Docs\.
The following companies provide low cost, full featured emulators designed specifically for C2000™controllers:
Blackhawk™ USB2000 Controller (part number TMDSEMU2000U)
http://www.blackhawk-dsp.com
$299
Spectrum Digital XDS510LC JTAG Emulator (part number 701902)
http://www.spectrumdigital.com
$249
For more information, see the following guides:EightChannelBuck – provides detailed information on the EightChannelBuck project within an easy touse lab-style format.C:\TI_28xxx_SysSW\EightChannelBuck\~Docs\EightChannelBuck.pdf
QSG-EightChannelBuck-GUI gives an overview on how to demo the EightChannelBuck projectquickly using an intuitive GUI interface.C:\TI_28xxx_SysSW\EightChannelBuck\~Docs\QSG-EightChannelBuck-GUI.pdf
EightChBuck-HWdevPkg – a folder containing various files related to the hardware on the DC/DCDeveloper’s Kit board (schematics, bill of materials, Gerber files, PCB layout, etc). All schematics andPCB files created with the freeware ExpressPCB package.C:\TI_28xxx_SysHW\EightChBuck-HWdevPkg\
F28x User’s Guides http://www.ti.com/f28xuserguides
TMS320C2000, TMS320C28x, PowerTrain, Code Composer Studio, C2000 are trademarks of TexasInstruments.
Blackhawk is a trademark of EWA Technologies, Inc.
All other trademarks are the property of their respective owners.
6TMS320C2000 DSC DC/DC Developer’s Kit SPRUFR7 – July 2008Submit Documentation Feedback
amplifier “Lam dataccnveneui com interlace “Lam logiciw cam gawerJiLom micrcccmmllem cam com www.mtom/Igrl wwwm cam/audio www u cam/automative www fl cam/b adband wwwm cam/dig‘talccnlml wwwm cam/medica‘ wwwm cam/mmtam wwwm cam/oglicalnetwolk wwwm cam/security wwwm cam/(e‘eghcny www fl cam/videa www fl cam/wwre‘ess
IMPORTANT NOTICE
Texas Instruments Incorporated and its subsidiaries (TI) reserve the right to make corrections, modifications, enhancements, improvements,and other changes to its products and services at any time and to discontinue any product or service without notice. Customers shouldobtain the latest relevant information before placing orders and should verify that such information is current and complete. All products aresold subject to TI’s terms and conditions of sale supplied at the time of order acknowledgment.
TI warrants performance of its hardware products to the specifications applicable at the time of sale in accordance with TI’s standardwarranty. Testing and other quality control techniques are used to the extent TI deems necessary to support this warranty. Except wheremandated by government requirements, testing of all parameters of each product is not necessarily performed.
TI assumes no liability for applications assistance or customer product design. Customers are responsible for their products andapplications using TI components. To minimize the risks associated with customer products and applications, customers should provideadequate design and operating safeguards.
TI does not warrant or represent that any license, either express or implied, is granted under any TI patent right, copyright, mask work right,or other TI intellectual property right relating to any combination, machine, or process in which TI products or services are used. Informationpublished by TI regarding third-party products or services does not constitute a license from TI to use such products or services or awarranty or endorsement thereof. Use of such information may require a license from a third party under the patents or other intellectualproperty of the third party, or a license from TI under the patents or other intellectual property of TI.
Reproduction of TI information in TI data books or data sheets is permissible only if reproduction is without alteration and is accompaniedby all associated warranties, conditions, limitations, and notices. Reproduction of this information with alteration is an unfair and deceptivebusiness practice. TI is not responsible or liable for such altered documentation. Information of third parties may be subject to additionalrestrictions.
Resale of TI products or services with statements different from or beyond the parameters stated by TI for that product or service voids allexpress and any implied warranties for the associated TI product or service and is an unfair and deceptive business practice. TI is notresponsible or liable for any such statements.
TI products are not authorized for use in safety-critical applications (such as life support) where a failure of the TI product would reasonablybe expected to cause severe personal injury or death, unless officers of the parties have executed an agreement specifically governingsuch use. Buyers represent that they have all necessary expertise in the safety and regulatory ramifications of their applications, andacknowledge and agree that they are solely responsible for all legal, regulatory and safety-related requirements concerning their productsand any use of TI products in such safety-critical applications, notwithstanding any applications-related information or support that may beprovided by TI. Further, Buyers must fully indemnify TI and its representatives against any damages arising out of the use of TI products insuch safety-critical applications.
TI products are neither designed nor intended for use in military/aerospace applications or environments unless the TI products arespecifically designated by TI as military-grade or "enhanced plastic." Only products designated by TI as military-grade meet militaryspecifications. Buyers acknowledge and agree that any such use of TI products which TI has not designated as military-grade is solely atthe Buyer's risk, and that they are solely responsible for compliance with all legal and regulatory requirements in connection with such use.
TI products are neither designed nor intended for use in automotive applications or environments unless the specific TI products aredesignated by TI as compliant with ISO/TS 16949 requirements. Buyers acknowledge and agree that, if they use any non-designatedproducts in automotive applications, TI will not be responsible for any failure to meet such requirements.
Following are URLs where you can obtain information on other Texas Instruments products and application solutions:
Products ApplicationsAmplifiers amplifier.ti.com Audio www.ti.com/audioData Converters dataconverter.ti.com Automotive www.ti.com/automotiveDSP dsp.ti.com Broadband www.ti.com/broadbandClocks and Timers www.ti.com/clocks Digital Control www.ti.com/digitalcontrolInterface interface.ti.com Medical www.ti.com/medicalLogic logic.ti.com Military www.ti.com/militaryPower Mgmt power.ti.com Optical Networking www.ti.com/opticalnetworkMicrocontrollers microcontroller.ti.com Security www.ti.com/securityRFID www.ti-rfid.com Telephony www.ti.com/telephonyRF/IF and ZigBee® Solutions www.ti.com/lprf Video & Imaging www.ti.com/videoWireless www.ti.com/wireless
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265Copyright © 2008, Texas Instruments Incorporated

Products related to this Datasheet

TMDSDCDC8KIT