Managing Converter In-Rush Current

Par Steven Keeping

Avec la contribution de Electronic Products


The sprinkling of capacitors in modern switching DC/DC converter designs can lead to high in-rush currents as the module starts up. Apart from the risk of component damage and system malfunction, such in-rush current can also cause troublesome problems for engineers trying to maximize battery life in portable products.

This article describes why in-rush current occurs, how it can compromise battery life, and the steps that manufacturers of modern power modules have taken to limit the problem.

What is in-rush current?

Switching DC/DC converters typically feature several capacitors. For example, one device forms part of the electromagnetic interference (EMI) input filter designed to limit interference generated by current flow in the input loop (Figure 1) while another sits on the output side to limit voltage ripple.

Schematic of low pass input EMI filter

Figure 1: Schematic of low pass input EMI filter between primary power source and switching regulator. The capacitors charge up during startup causing high in-rush current (Courtesy of Texas Instruments).

When the converter is first switched on, these uncharged capacitors act as virtual short circuits, allowing the current to rapidly escalate. The current spike lasts only as long as it takes the various capacitors to charge, but it can reach a peak value well in excess of what the converter would otherwise experience, even under full load. The only characteristics that limit the magnitude of the spike are the line impedance and the capacitors’ equivalent series resistance (ESR).

An uncontrolled in-rush spike can cause havoc. In the first instance, there’s a chance that components can be damaged or sensitive silicon disturbed such that system errors occur. But that’s not all; in portable devices with modest power supplies, all the good work that the engineer has done to maximize battery life can be undone by wayward current behavior.¹

Startup failure

A battery’s behavior changes during its discharge cycle. As the cell discharges, its internal resistance rises and the voltage the battery can supply to the load falls. Note that the relationship between capacity and supply voltage isn’t linear. The voltage tends to tail off rapidly as the battery nears the end of its life (Figure 2).

Discharge curves for a 1.5 V AA alkaline battery

Figure 2: Discharge curves for a 1.5 V AA alkaline battery at constant load (Courtesy of Energizer).

The DC/DC converter requires a minimum voltage to operate correctly. To ensure that the power module doesn’t attempt to operate below that limit, manufacturers incorporate undervoltage lockout mechanisms into their products. A partially-depleted battery supplying a large in-rush current will struggle to cope and its supply voltage will likely drop below the undervoltage threshold – with the result that the product fails to start up.

Worse yet, the cell may recover, such that the device’s battery gauge indicates it still has some capacity left, only for the process to repeat itself when the user tries to switch on the product again. The likely conclusion is that the owner will swap out a serviceable battery while questioning the product manufacturer’s battery lifetime claims. All the work the engineer has done to maximize the efficiency of the product to extend battery lifetime will be wasted.¹

Soft-start solution

Silicon vendors promote the high efficiency of a switching power module as one of the key reasons for selecting such a component for a battery-powered product. Accordingly, they are not keen to see the extra battery life promised by high efficiency negated by in-rush currents.

The vendors’ answer is to implement soft-start regimes. In simple terms, soft starts control the rate of current build up and stop it from overshooting a pre-determined value that neither stresses components nor causes system malfunctions.

Step-down (“buck”) converters sometimes use a simple soft-start regime that relies on a maximum current detector. The maximum current limit is released after a fixed time or at a set output voltage. The advantage is that the chip remains in its normal operating mode at all times; however, the drawback is that current can still increase rapidly (even though the peak value is limited) causing the battery voltage to drop and the undervoltage mechanism to activate if the battery has little capacity remaining.

An alternative approach for a buck converter is to limit the rate at which the output voltage increases and prevent it from overshooting a set point (or at least minimize the overshoot). This limits both the rate at which the in-rush current escalates and helps prevents battery voltage dipping so dramatically that the undervoltage mechanism triggers.²

Step-up (“boost”) converters tend to have a more complex startup operation. Texas Instruments’ TPS6107x family of boost converters, for example, has a three-phase soft-start regime.³

During phase 1, the internal synchronous FET operates in its linear region and delivers a fixed DC current to charge the output capacitor to a value that’s almost equal to the input voltage. If at the end of phase 1, the output voltage is still less than 1.8 V, the device then switches to phase 2, where it operates with a 70 percent duty cycle until the output voltage is greater than 1.8 V. (If the output voltage is greater than 1.8 V at the end of phase 1, then phase 2 is skipped.)

During the third phase of the soft start, the error amplifier takes over and switches at the normal duty cycle, based on input and output voltage. During this cycle, the current limit is reduced to 50 percent of the nominal current limit to minimize any in-rush current. The device begins normal operation with the standard current limit when the output capacitor finally charges to the nominal output voltage. Figure 3 illustrates how the soft start prevents the output voltage from climbing too rapidly.

TPS61070 soft starting into a 50 Ω load

Figure 3: TPS61070 soft starting into a 50 Ω load. Note controlled increase in Vout which charges output capacitors slowly, limiting in-rush current (Courtesy of Texas Instruments).

Setting the maximum current threshold

The maximum current threshold and output voltage set point will vary depending on the application. Some manufacturers have made module selection easier by allowing the engineer to select the maximum current such that a single converter can be used in a range of applications.

For example, ams’ AS1326 boost converter allows both the selection of the maximum current during startup and soft-start time constant. Figure 4 shows the soft-start circuitry implemented. The engineer selects two resistors (Rss and Rss2) and a capacitor (Css) to set the current limit (ILIMIT) and time constant (tss).

A current limit and time constant for soft start

Figure 4: A current limit and time constant for soft start can be implemented with a simple application circuit for ams’ AS1326.

Other manufacturers offer switching DC/DC converters with soft starting. Maxim Integrated Products, for example, supplies the MAX5073 among its wide range of soft-start DC/DC converters. This is a 2.2 MHz, dual-output buck or boost converter that includes an internal digital soft start. The company claims the mechanism reduces in-rush current, eliminates output-voltage overshoot, and ensures monotonic rise in output voltage during power-up.

For its part, Linear Technology offers the LTC3609 among its products with soft-start capability. The module is a buck DC/DC converter that can deliver up to 6 A output current from a 4 to 32 V input supply. Soft-start capability is accomplished using an external timing capacitor and the converter’s current limit is user programmable.

In summary, in-rush current is the spike of current drawn by a power supply when it is turned on. There is a natural concern that high spike currents can create electromagnetic interference in adjacent circuitry, or trip an upstream circuit breaker or the overcurrent protection of a solid-state power controller.

As we’ve seen, DC/DC converters can employ a well-controlled internal startup sequence and a precise output voltage soft start feature. The voltage soft start feature ensures the output ramps up in a controlled manner, with limited dv/dt. This article has highlighted several such parts as well as one where the supplier allows both the selection of the maximum current during startup as well as the soft-start time constant. For more information on the products mentioned here, use the links provided to access product pages on the DigiKey website.

References:

  1. Understanding power supplies and inrush current,” Michael Allen, Bear Power Supplies, Electronic Products, January 2006.
  2. Extend Battery Life By Implementing Soft Start,” Emir Serdarevic, ams, March 2012.
  3. Extending Soft Start Time in TPS6107x Family of Boost Converters,” Chris Glaser, Texas Instruments Application Report SLVA307, August 2008.

Avertissement : les opinions, convictions et points de vue exprimés par les divers auteurs et/ou participants au forum sur ce site Web ne reflètent pas nécessairement ceux de DigiKey ni les politiques officielles de la société.

À propos de l'auteur

Image of Steven Keeping

Steven Keeping

Steven Keeping is a contributing author at DigiKey. He obtained an HNC in Applied Physics from Bournemouth University, U.K., and a BEng (Hons.) from Brighton University, U.K., before embarking on a seven-year career as an electronics manufacturing engineer with Eurotherm and BOC. For the last two decades, Steven has worked as a technology journalist, editor and publisher. He moved to Sydney in 2001 so he could road- and mountain-bike all year round, and work as editor of Australian Electronics Engineering. Steven became a freelance journalist in 2006 and his specialities include RF, LEDs and power management.

À propos de l'éditeur

Electronic Products

Le magazine Electronic Products et le site ElectronicProducts.com s'adressent aux ingénieurs et aux directeurs de l'ingénierie responsables de la conception de systèmes et d'équipements électroniques.