Pervasive RF Energy Offers Ready Power Source

Par Stephen Evanczuk

Avec la contribution de Electronic Products

Thanks to a widespread growth of wireless communications, the availability of ambient RF energy offers an increasingly attractive power source for many low-powered designs. RF energy harvesting offers significant advantages for many applications, but it requires careful attention to key components, including receiving coils and power conditioning circuits required for this approach. For engineers, efficient RF energy-harvesting design has become simpler thanks to available components and ICs from a variety of manufacturers, including Intersil, Linear Technology, ROHM Semiconductor, STMicroelectronics, Texas Instruments and Vishay Dale, among others.

RF energy sources abound and promise to expand as consumer and industrial markets cut the cord and rely more heavily on wireless technologies for every type of communications from short to long range. Along with ubiquitous Wi-Fi sources, engineers can find RF energy sources ranging from short-range technologies, such as Bluetooth and ZigBee, to the varied long-range technologies behind cellular services.

Along with its growing availability, RF energy harvesting brings multiple benefits to system design itself. Besides enjoying reduced wiring and cabling requirements, a design powered from ambient RF energy can be completely sealed and protected from environmental conditions and hazardous materials. A reduced maintenance requirement not only offers its own merits, but also allows engineers to place systems in locations that are hard to reach or that suffer from reduced availability of other ambient energy sources such as light, temperature, or vibration. For mesh networks, such as those envisioned in the Internet of Things (IoT), engineers can combine RF energy harvesting with sophisticated device-to-device communications using ambient backscatter modulation of the RF source by each individual device.

Harvesting energy requires at a minimum only a few basic components, including an energy source transducer, rectifier, storage, and output regulator (Figure 1). For RF energy harvesting, a receiving coil serves as the energy source, generating a voltage in response to electromagnetic coupling with the RF transmitter. As with energy harvesting in general, the challenge in RF energy harvesting lies in maximizing the output from the transducer (here, the receiving coil) at a given ambient energy level.

Image of Linear Technology energy-harvester circuit

Figure 1: An energy-harvester circuit typically rectifies voltage output of the ambient energy collected by a transducer. Most applications require a means to store the resulting energy and regulate voltage output delivered to the load (Courtesy of Linear Technology).

With RF energy harvesting, engineers face unique challenges in ensuring maximum energy output. At a fundamental level, engineers must contend with weak ambient RF sources. Although forms of RF energy permeate most enclosed areas, they are often at levels below what engineers might expect to find with alternative ambient sources (Figure 2).

Image of Texas Instruments ambient RF sources such as Wi-Fi and cellular GSM

Figure 2: Although increasingly pervasive, ambient RF sources such as Wi-Fi and cellular GSM typically enjoy higher efficiency than other sources, but generally result in lower harvested power (Courtesy of Texas Instruments).

RF transmitters for communications are typically constrained in the amount of power they can radiate. Furthermore, for a given radio source, the power at the receiving antenna falls off with distance as predicted by the Friis transmission equation:

Image of equation 1

where

PT = transmitted power
PR = received power
GT = transmitter antenna gain
GR = receiver antenna gain
λ = wavelength
d = distance between transmitter and receiver

In this environment, design of the receiving antenna plays a critical role in maximizing efficiency of energy harvesting. Although receiving antennas can be etched into printed circuit boards, engineers can find available receiving coil components specifically designed for the task. As with many such devices in this class, the Vishay Dale 48 mm x 32 mm IWAS-3827EC-50 receiving coil (Figure 3) features low DC resistance (200 mΩ) and inductance (9.7 μH). Optimized for wireless power applications, these receiving coils typically feature high- permeability shielding and are built to block charging flux from other circuit components.

Image of Vishay Dale IWAS-3827EC-50

Figure 3: Receiving coils such as the Vishay Dale IWAS-3827EC-50 are optimized for wireless power applications and feature shielding to protect neighboring electronic devices (Courtesy of Vishay Dale).

To generate maximum voltage drop across the coil, engineers would typically add a capacitor in parallel to form a resonant circuit tuned to the frequency of the highest power RF signal. Properly tuned and matched to the load, the output of this resonant circuit would represent the best possible energy output from the optimal RF source.

Using RF energy to power application circuits typically requires a power stage to drive the load or charge an energy storage device such as a supercapacitor or thin-film battery. In the past, engineers looking to implement RF energy harvesting would need to design a custom power stage comprising at a minimum a rectifier such as the ROHM Semiconductor FMN1 or ROHM FMP1, among many others. In addition, the power stage would typically need to boost the rectified voltage output using a DC/DC boost converter such as the Intersil ISL9111 or Linear Technology LTC3429 prior to use by the load or for charging a storage device.

Rather than build a power stage from scratch, however, engineers can find integrated devices that deliver the functionality required for RF energy harvesting. Although many of these devices are built to target the requirements of specific application areas, they can serve more general design needs. The STMicroelectronics M24LR16E-R is designed for conventional NFC/RFID applications, but the device includes special features for RF energy harvesting.

On the input side, the M24LR16E-R provides two pins for RF input from a receiving coil. Besides supporting NFC/RFID application functionality on the output side, the device provides a dedicated Vout analog pin. When programmatically set into energy-harvesting mode, the device uses Vout to output excess energy captured by the device from the RF field. Power on Vout is limited to ensure that the M24LR16E-R has sufficient internal power, but this residual power can be sufficient to drive various low-power application circuits. Engineers can explore the device's energy-harvesting mode using ST's ROBOT-M24LR16E-A evaluation board, which includes an etched inductive antenna, M24LR16E-R IC, PC connector, and associated components.

Increased interest in wireless power and wireless charging applications has also driven the emergence of ICs able to meet the needs of more general RF energy harvesting. The Texas Instruments BQ51221 is designed to support wireless power protocols, but features a full-power-conditioning path required for more general RF energy-harvesting designs (Figure 4). Featuring 79 percent overall efficiency, the IC integrates a synchronous rectifier with 96 percent efficiency and a regulator operating at 97 percent efficiency.

Image of Texas Instruments BQ51221 wireless power receiver

Figure 4: The Texas Instruments BQ51221 wireless power receiver provides power-conditioning functionality required for more general RF energy-harvesting applications (Courtesy of Texas Instruments).

Conclusion

Fast-growing proliferation of mobile systems and wireless smart sensors continues to drive an explosive growth in all forms of wireless communications, resulting in near-pervasive availability of ambient RF energy. For engineers, RF energy harvesting offers an increasingly favorable alternative for supplying low-power designs such as wireless sensors and other devices built for the IoT. Using available components, engineers can easily build circuits able to harvest RF energy; but the growing availability of wireless power ICs provides a ready solution for incorporating RF energy harvesting in any low-power design.

For more information on the parts discussed in this article, use the links provided to access product information pages on the Digi-Key website.

 

Avertissement : les opinions, convictions et points de vue exprimés par les divers auteurs et/ou participants au forum sur ce site Web ne reflètent pas nécessairement ceux de DigiKey ni les politiques officielles de la société.

À propos de l'auteur

Image of Stephen Evanczuk

Stephen Evanczuk

Stephen Evanczuk affiche plus de 20 ans d'expérience dans la rédaction de contenu pour et sur l'industrie électronique, couvrant un large éventail de sujets, notamment le matériel, les logiciels, les systèmes et les applications, y compris l'IoT. Il a obtenu son doctorat (Ph.D.) en neurosciences sur les réseaux neuronaux et a travaillé dans l'industrie aérospatiale sur les systèmes sécurisés massivement distribués et les méthodes d'accélération par algorithmes. Actuellement, lorsqu'il n'écrit pas d'articles techniques, il travaille sur l'application de l'apprentissage approfondi pour les systèmes de reconnaissance et de recommandation.

À propos de l'éditeur

Electronic Products

Le magazine Electronic Products et le site ElectronicProducts.com s'adressent aux ingénieurs et aux directeurs de l'ingénierie responsables de la conception de systèmes et d'équipements électroniques.