Maxim Eyes Panasonic’s GridEye

Touch is the de facto controller. We have touch screens for everything nowadays. But what if you didn’t have to touch anything to control it? With just a wave of a hand, things would move how you want them to. You enter a room, and all the lights turn on. They are too bright; you wave your hands, and the lights dim. Luke Skywalker would be jealous.

Well, this is possible today. Maxim has an evaluation board for the Panasonic GridEye. It uses the 1-wire interface for easy communication. There are also two different design boards available for use with this evaluation board. Maxim has the MAXREFDES130# which is set up for house lighting control with 8 relays on the board. They also have the MAXREFDES132# which is great for other general microcontroller designs.

Using the Maxim board, an Arduino Uno, and the MAXREFDES132#, we created a gesture controller for DC motors. You can watch it in this Another Geek Moment Video.

You can also read about it on our EEwiki.

À propos de l'auteur

Image of Ben Roloff

Ben Roloff, ingénieur d'application associé chez DigiKey, assiste les clients pour tous leurs besoins en microcontrôleurs depuis 2016. Il est né en 1991, à une époque où l'Internet était inconnu à la maison. Internet s'est lentement imposé tout au long de ses études, donc d'une certaine façon, Ben a grandi avec Internet. C'est son intérêt pour les ordinateurs qui l'a poussé à poursuivre des études en informatique, et il est titulaire d'une licence en sciences informatiques de la South Dakota School of Mines and Technology.

More posts by Ben Roloff
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum