Proper Soldering Techniques

When I was a young college student learning to solder, my connections and overall soldering job needed some fine-tuning. Over the past few years I learned a few tips and tricks that helped me to improve my skill. After using the new American Hakko FX-888D soldering station with a variable temperature selection on a recent project, I decided to demonstrate some of those tips and tricks with a couple fellow engineers here at DigiKey with our new video.

To go along with this blog, I wrote an article on the basics of soldering and some information on solder and flux to help all beginners to hone their skills and take their soldering to the next level.

À propos de l'auteur

Image of Ashley Awalt

Ashley Awalt est technicienne en ingénierie des applications chez DigiKey depuis 2011. Elle a obtenu sa licence en sciences appliquées en technologies électroniques et systèmes automatisés du Northland Community & Technical College dans le cadre du programme de bourses de DigiKey. Son rôle actuel est d'aider à créer des projets techniques uniques, de documenter les processus et de participer à la production de la couverture médiatique vidéo des projets. Durant son temps libre, Ashley aime - oh, attendez, est-ce qu'on a vraiment du temps libre quand on est maman ?

More posts by Ashley Awalt
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum