Webinar: Remotely Monitor Equipment in a Challenging Environment with Single-Pair Ethernet

Join DigiKey on Wednesday, June 08, 2022, at 11 AM CDT to hear from industry-leading companies, including SparkFun Electronics, HARTING Group, Würth Elektronik eiSos GmbH & Co. KG, and Analog Devices. Experts from each of these companies are joining together to teach us about Single-Pair Ethernet (SPE) and the benefits this technology brings.

SPE is a fast, reliable form of data transmission that also provides Power over Data Line (PoDL), reducing the number of cables needed in your application. During this webinar, you will also learn about applications and case studies and see a demonstration using SPE.

If you are unable to attend the webinar, be sure to register so we can send a recording after it is complete.

Register here: https://event.on24.com/wcc/r/3776170/37D863B98269A657D6761D2C56A0BB51?partnerref=blog

À propos de l'auteur

Image of Ashley Awalt

Ashley Awalt est technicienne en ingénierie des applications chez DigiKey depuis 2011. Elle a obtenu sa licence en sciences appliquées en technologies électroniques et systèmes automatisés du Northland Community & Technical College dans le cadre du programme de bourses de DigiKey. Son rôle actuel est d'aider à créer des projets techniques uniques, de documenter les processus et de participer à la production de la couverture médiatique vidéo des projets. Durant son temps libre, Ashley aime - oh, attendez, est-ce qu'on a vraiment du temps libre quand on est maman ?

More posts by Ashley Awalt
 TechForum

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.

Visit TechForum