' ‘CYPRESS'
EMIEDDED m lnmnnuw
 
 
 
M stm
itcr RVS and check for any bfle lim
ttem mismatches. RDY wil
e used by an ege
bypass mode, the BIST in the 53
the encoded mode. M
the receivertc SWl
received
The MODE input pin selects betw
modes. When wired to VCC, the
eccder and go directly from the
lthe output latch. When wired i
ng the 83/103 codes showj
' ‘CYPRESS'
EMIEDDED m lnmnnuw
 
 
 
M stm
itcr RVS and check for any bfle lim
ttem mismatches. RDY wil
e used by an ege
bypass mode, the BIST in the 53
the encoded mode. M
the receivertc SWl
received
The MODE input pin selects betw
modes. When wired to VCC, the
eccder and go directly from the
lthe output latch. When wired i
ng the 83/103 codes showj
Document Number: 38-02017 Rev. *K  Page 18 of 42
Receiver Test Mode Description
The CY7B933 receiver offers two types of test mode operation, 
BIST mode and Test mode. In a normal system application, the 
Built-In Self-Test (BIST) mode can be used to check the function-
ality of the transmitter, the receiver and the link connecting them. 
This mode is available with minimal impact on user system logic, 
and can be used as part of the normal system diagnostics. 
Typical connections and timing are shown in Figure 8 on page 15.
BIST Mode
The BIST mode function is as follows:
1. Set BISTEN LOW to enable self-test generation and await 
RDY LOW indicating that the initialization code has been re-
ceived.
2. Monitor RVS and check for any byte time with the pin HIGH 
to detect pattern mismatches. RDY will pulse HIGH once per 
BIST loop, and can be used by an external counter to monitor 
test pattern progress. Q0–7 and SC/D will show the expected 
pattern and may be useful for debug purposes.
3. When testing is completed, set BISTEN HIGH and resume 
normal function.
Note A specific test of the RVS output may be required to assure 
an adequate test. To perform this test, it is only necessary to have 
the transmitter send violation (SVS = HIGH) for a few bytes 
before beginning the BIST test sequence. Alternatively, the 
receiver could enter BIST mode after the transmitter has begun 
sending BIST loop data, or be removed before the transmitter 
finishes sending BIST loops, each of which contain several delib-
erate violations and should cause RVS to pulse HIGH.
BIST mode is intended to check the entire function of the Trans-
mitter, serial link, and receiver. It augments normal factory ATE 
testing and provides the user system with a rigorous test 
mechanism to check the link transmission system, without 
requiring any significant system overhead.
When in bypass mode, the BIST logic will function in the same 
way as in the encoded mode. MODE = HIGH and BISTEN = 
LOW causes the receiver to switch to encoded mode and begin 
checking the decoded received data of the BIST pattern, as if 
MODE = LOW. When BISTEN returns to HIGH, the receiver 
resumes normal bypass operation. In test mode the BIST 
function works as in the normal mode.
Test Mode
The MODE input pin selects between three receiver functional 
modes. When wired to VCC, the shifter contents bypass the 
decoder and go directly from the decoder latch to the Qa–j inputs 
of the output latch. When wired to GND, the outputs are decoded 
using the 8B/10B codes shown at the end of this datasheet and 
become Q0–7, RVS, and SC/D. The third function is test mode, 
used for factory or incoming device test. This mode can be 
selected by leaving the MODE pin open (internal circuitry forces 
the open pin to VCC/2).
Test mode causes the Receiver to function in its Encoded mode, 
but with INB (INB+) as the bit rate Test clock instead of the 
Internal PLL generated bit clock. In this mode, transfers between 
the Shifter, Decoder register and Output register are controlled 
by their normal logic, but with an external bit rate clock instead 
of the PLL (the recovered bit clock). Internal logic and test pattern 
inputs can be synchronized by sending a SYNC pattern and 
allowing the Framer to align the logic to the bit stream. The flow 
is as follows:
1. Assert Test mode for several test clock cycles to establish 
normal counter sequence. 
2. Assert RF to enable reframing. 
3. Input a repeating sequence of bits representing K28.5 (Sync). 
4. RDY falling shows the byte boundary established by the 
K28.5 input pattern. 
5. Proceed with pattern, voltage and timing tests as is conve-
nient for the test program and tester to be used.
(While in Test mode and in BIST mode with RF HIGH, the Q0–7, 
RVS, and SC/D outputs reflect various internal logic states and 
not the received data.)
Test mode is intended to allow logical, DC, and AC testing of the 
Receiver without requiring that the tester generate input data at 
the bit rate or accommodate the PLL lock, tracking and 
frequency range characteristics that are required when the part 
operates in its normal mode.
X3.230 Codes and Notation Conventions
Information to be transmitted over a serial link is encoded eight 
bits at a time into a 10-bit Transmission Character and then sent 
serially, bit by bit. Information received over a serial link is 
collected ten bits at a time, and those Transmission Characters 
that are used for data (Data Characters) are decoded into the 
correct eight-bit codes. The 10-bit Transmission Code supports 
all 256 8-bit combinations. Some of the remaining Transmission 
Characters (Special Characters) are used for functions other 
than data transmission.
The primary rationale for use of a Transmission Code is to 
improve the transmission characteristics of a serial link. The 
encoding defined by the Transmission Code ensures that suffi-
cient transitions are present in the serial bit stream to make clock 
recovery possible at the Receiver. Such encoding also greatly 
increases the likelihood of detecting any single or multiple bit 
errors that may occur during transmission and reception of infor-
mation. In addition, some Special Characters of the Trans-
mission Code selected by Fibre Channel Standard consist of a 
distinct and easily recognizable bit pattern (the Special Character 
Comma) that assists a Receiver in achieving word alignment on 
the incoming bit stream.
Notation Conventions
The documentation for the 8B/10B Transmission Code uses 
letter notation for the bits in an 8-bit byte. Fibre Channel Standard 
notation uses a bit notation of A, B, C, D, E, F, G, H for the 8-bit 
byte for the raw 8-bit data, and the letters a, b, c, d, e, i, f, g, h, j 
for encoded 10-bit data. There is a correspondence between bit 
A and bit a, B and b, C and c, D and d, E and e, F and f, G and 
g, and H and h. Bits i and j are derived, respectively, from 
(A,B,C,D,E) and (F,G,H).
The bit labeled A in the description of the 8B/10B Transmission 
Code corresponds to bit 0 in the numbering scheme of the FC-2 
specification, B corresponds to bit 1, as shown below.
FC-2 bit designation—76543 21 0
HOTLink D/Q designation—76543210
8B/10B bit designation—HGFEDCBA