Data Sheet ADIS16305
CALIBRATION
Manual Bias Calibration
The bias offset registers in Table 16 and Table 17 provide a manual
adjustment function for the output of each sensor. For example,
if GYRO_OFF = 0x1FF6 (DIN = 0x9B1F, 0x9AF6), the GYRO_OUT
offset shifts by −10 LSBs, or −0.125°/sec.
Table 16. GYRO_OFF Bit Descriptions
Bits Description (Default = 0x0000)
[15:13] Not used.
[12:0] Data bits. Twos complement, 0.0125°/sec per LSB.
Typical adjustment range = ±50°/sec.
Table 17. XACCL_OFF, YACCL_OFF, ZACCL_OFF
Bit Descriptions
Bits Description (Default = 0x0000)
[15:12] Not used.
[11:0] Data bits. Twos complement, 0.6 mg/LSB. Typical
adjustment range = ±1.22 g.
Frame Alignment
The PITCH_OFF and ROLL_OFF registers (see Table 18) provide
the angular orientation difference between the inertial frame
(internal) and the external frame (package). They follow the same
orientation as PITCH_OUT and ROLL_OUT, as shown in Figure 14.
Table 18. PITCH_OFF, ROLL_OFF Bit Descriptions
Bits Description
[15:10] Not used.
[9:0] Data bits. Twos complement, 0.014°/LSB.
Gyroscope Automatic Bias Null Calibration
Set GLOB_CMD[0] = 1 (DIN = 0xBE01) to execute the automatic
bias null calibration function. This function measures the
gyroscope output register and then loads the gyroscope offset
register with the opposite value to provide a quick bias calibration.
All sensor data is then reset to 0, and the flash memory is updated
automatically within 50 ms (see Table 19).
Gyroscope Precision Automatic Bias Null Calibration
Set GLOB_CMD[4] = 1 (DIN = 0xBE10) to execute the precision
automatic bias null calibration function. This function takes the
sensor offline for 30 sec while it collects a set of data and calculates
more accurate bias correction factors for each gyroscope. After
this function is executed, the newly calculated correction factor
is loaded into the gyroscope offset registers, all sensor data is
reset to 0, and the flash memory is updated automatically within
50 ms (see Table 19).
Restoring Factory Calibration
Set GLOB_CMD[1] = 1 (DIN = 0xBE02) to execute the factory
calibration restore function. This function resets each user calibration
register to 0x0000 (see Table 16 and Table 17), resets all sensor
data to 0, and automatically updates the flash memory within
50 ms (see Table 19).
Linear Acceleration Bias Compensation (Gyroscope)
Set MSC_CTRL[7] = 1 (DIN = 0xB486) to enable correction for
low frequency acceleration influences on gyroscope bias. Note
that the DIN sequence also preserves the factory default condition
for the data-ready function (see Table 24).
OPERATIONAL CONTROL
Global Commands
The GLOB_CMD register provides trigger bits for several useful
functions. Setting the assigned bit to 1 starts each operation,
which returns the bit to 0 after completion. For example, set
GLOB_CMD[7] = 1 (DIN = 0xBE80) to execute a software reset,
which stops the sensor operation and runs the device through
its start-up sequence. This sequence includes loading the control
registers with their respective flash memory locations prior to
producing new data. Reading the GLOB_CMD register
(DIN = 0x3E00) starts the burst read sequence.
Table 19. GLOB_CMD Bit Descriptions
Bit(s) Description
[15:8] Not used
[7] Software reset command
[6:5] Not used
Precision autonull command
[3] Flash update command
[2] Auxiliary DAC data latch
[1] Factory calibration restore command
[0] Autonull command
Internal Sample Rate
The SMPL_PRD register provides discrete sample rate settings
using the bit assignments in Table 20 and the following equation:
tS = tB × (NS + 1)
For example, when SMPL_PRD[7:0] = 0x0A, the sample rate is
149 SPS.
Table 20. SMPL_PRD Bit Descriptions
Bit(s) Description (Default = 0x0001)
[7] Time base (tB)
0 = 0.61035 ms, 1 = 18.921 ms
[6:0] Increment setting (NS)
Internal sample period = tS = tB × (NS + 1)
The default sample rate setting of 819.2 SPS provides optimal
performance. For systems that value slower sample rates, keep the
internal sample rate at 819.2 SPS. Use the programmable filter
(SENS_AVG) to reduce the bandwidth, which helps to prevent
aliasing. The data-ready function (MSC_CTRL) can drive an
interrupt routine that uses a counter to help ensure data coherence
at reduced rates.
Rev. A | Page 13 of 20