Maker.io main logo

From Zero to Verilog Hero (Part -1) A Comprehensive Introduction

1 560

2023-12-15 | By DWARAKAN RAMANATHAN

What is Verilog?

Verilog is a hardware description language (HDL) used in the field of digital electronics and integrated circuit (IC) design. It serves as a means to describe the behavior and structure of electronic systems, including digital circuits and systems on a chip (SoCs). Verilog is primarily used for the design, simulation, and verification of digital circuits and is an essential tool in the semiconductor and electronics industry.

Here are some key aspects of Verilog:

  • Hardware Description: Verilog allows engineers to describe the functionality and interconnections of digital circuits and systems using a textual or schematic representation. It is used to specify how digital logic elements (such as gates, flip-flops, and multiplexers) are interconnected to create complex digital systems.
  • Design Entry: Engineers use Verilog to create high-level descriptions of their digital designs. These descriptions can range from simple logic gates to complex processors, memory systems, and custom hardware components.
  • Simulation: Verilog is used for simulating the behavior of digital circuits before they are physically implemented. Engineers can test and debug their designs in a software simulation environment, identifying and fixing issues without the need for physical hardware.
  • Synthesis: Verilog code can be synthesized into a netlist, which is a structural representation of a design suitable for implementation on an FPGA (Field-Programmable Gate Array) or ASIC (Application-Specific Integrated Circuit.)
  • Verification: Verilog plays a crucial role in verifying the correctness of digital designs. Engineers can create test benches and apply various test scenarios to ensure that a design functions as intended.
  • Hierarchy: Verilog supports a hierarchical design approach, allowing complex systems to be broken down into smaller, manageable modules with well-defined interfaces.
  • Timing Constraints: It enables designers to specify timing constraints, ensuring that circuits meet required performance criteria, such as clock frequency and setup/hold times.
  • Industry Standards: Verilog has several standardized versions, including IEEE 1364-2005 (Verilog-2005) and SystemVerilog, which is an extension of Verilog with advanced features for verification and design.

Evolution of Verilog:

The evolution of the Verilog language can be traced through several versions and standards, each introducing new features and improvements. Here is a high-level flow or evolution of the Verilog language:

  • Verilog-XL (Proprietary): Early 1980s: The Verilog language originated as a proprietary simulation and verification tool developed by Gateway Design Automation. It was called "Verilog-XL."
  • Open Verilog International (OVI): 1990: Gateway Design Automation and Cadence Design Systems formed the Open Verilog International (OVI) organization to standardize the Verilog language and make it available to the industry.
  • IEEE Standardization: 1995: The IEEE published the first official standard for Verilog, known as IEEE 1364-1995. This standard marked the beginning of the formal standardization of Verilog.
  • Verilog-2001: 2001: IEEE released IEEE 1364-2001, often referred to as Verilog-2001. This version introduced some enhancements and clarifications to the language.
  • Verilog-2005: 2005: IEEE published IEEE 1364-2005, known as Verilog-2005. This version provided additional features and improvements, making it a more comprehensive and widely used standard.
  • SystemVerilog Emergence: Mid-2000s: SystemVerilog, an extension of Verilog, began to emerge. It aimed to enhance Verilog's capabilities for verification, testbench development, and system-level modeling.
  • Unified Standard (IEEE 1800-2017): 2017: The IEEE released IEEE 1800-2017, which unified SystemVerilog and the original Verilog language under a single standard. This unified standard, known as SystemVerilog, incorporated the best aspects of both languages and provided a comprehensive solution for hardware design and verification.
  • Ongoing Evolution: The evolution of the Verilog language continues with ongoing efforts to improve and standardize it further. Updates and revisions may be introduced to address emerging needs in digital design and verification.

How is Verilog different from other languages?

Verilog is a specialized hardware description language (HDL) used for designing and modeling digital circuits and systems. It is distinct from general-purpose programming languages like C++, Java, or Python. Here are some key differences that set Verilog apart from other languages:

  • Purpose:
    • Verilog: Designed specifically for hardware description and digital circuit design, including specifying the behavior and interconnections of electronic components.
    • General-Purpose Languages: Designed for a wide range of applications, including software development, web development, data analysis, and more.
  • Abstraction Level:
    • Verilog: Works at a lower level of abstraction, focusing on describing the physical hardware behavior and structure, including gates, flip-flops, and wires.
    • General-Purpose Languages: Operate at a higher level of abstraction, dealing with algorithms, data structures, and software logic.
  • Parallelism:
    • Verilog: Emphasizes parallelism, as digital circuits operate concurrently with many components working simultaneously.
    • General-Purpose Languages: Typically follow a sequential execution model, where instructions are executed one after another.
  • Simulation vs. Execution:
    • Verilog: Primarily used for simulation and verification of hardware designs before implementation in hardware.
    • General-Purpose Languages: Designed for direct execution on a computer's central processing unit (CPU).
  • Hardware Description:
    • Verilog: Allows for the description of hardware components, their interconnections, and their behaviors, making it suitable for electronic design.
    • General-Purpose Languages: Focus on software development and are not tailored for hardware description.
  • Concurrent vs. Sequential Logic:
    • Verilog: Enables the description of both sequential logic (e.g., flip-flops, registers) and combinational logic (e.g., gates).
    • General-Purpose Languages: Typically deal with sequential logic and do not provide built-in constructs for describing hardware components.
  • Synthesis:
    • Verilog: Code can be synthesized into a netlist, which represents the hardware structure of a design and can be implemented in FPGAs or ASICs.
    • General-Purpose Languages: Not designed for hardware synthesis.
  • Event-Driven Simulation:
    • Verilog: Utilizes an event-driven simulation model to simulate digital circuit behavior based on changes in inputs and internal events.
    • General-Purpose Languages: Follow a control-flow model where program execution depends on predefined control structures.
  • Bit-Level vs. Symbolic Level:
    • Verilog: Works at the bit level, directly manipulating individual bits and signals.
    • General-Purpose Languages: Typically operate at a higher symbolic level, working with abstract data types and variables.
  • Domains of Use:
    • Verilog: Primarily used in digital design, electronics, FPGA programming, and ASIC design.
    • General-Purpose Languages: Applied in a wide variety of domains, including software development, web development, data analysis, and more.

    Example of a Verilog Code:

    Copy Code
    module and_gate ( 
    ‎    input wire a, 
    ‎    input wire b, 
    ‎    output wire y 
    ‎); 
    ‎ 
    assign y = a & b; 
    ‎ 
    endmodule

    In this Verilog code:

    • module and_gate defines a module named "and_gate."
    • input wire a and input wire b declare two input wires named "a" and "b."
    • output wire y declares an output wire named "y."

    Inside the module:

    • assign y = a & b; assigns the logical AND operation of inputs "a" and "b" to the output "y." This line represents the behavior of a 2-input AND gate.

    You can use this Verilog code as a module to create a larger digital circuit or simulation. When you provide input values for "a" and "b," the code will simulate the AND gate's behavior and produce the corresponding output on wire "y.

    Note: This is a simple example for educational purposes. In practical applications, Verilog code can become much more complex when designing larger digital systems and incorporating hierarchical structures, timing constraints, and other features.

    You can see how to see your Design in RTL Here

    In the Next Blog you will learn about:

    • What is an RTL (Register Transfer Logic)?
    • What is Hardware Description language?
    • Basics of Designing using Verilog Coding (Sections)
    • Difference between Designing and Verification
    Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.