Model 105 Tunnel Oven Operating Manual Datasheet
 connectivity
 
connectivity
 - -TE APPLICAYION
- room/s
mmrlvlry
- -TE APPLICAYION
- room/s
mmrlvlry
 
 -.'TE
mun/wry
APPLICATION
TOOL/N6
 
 
a\
-.'TE
mun/wry
APPLICATION
TOOL/N6
 
 
a\
 -.'TE
mun/wry
APPLICATION
TOOL/N6
 
 
a\
-.'TE
mun/wry
APPLICATION
TOOL/N6
 
 
a\
 - .' TE
mmrlvlry
- .' TE
mmrlvlry
 
 
 - -TE Appu:,4mw
- rum/mo
mmI/Wry
A
C
A
A
m
 
 
a\
- -TE Appu:,4mw
- rum/mo
mmI/Wry
A
C
A
A
m
 
 
a\
 um ‘ "
um ‘ "
 
 
 
 - -TE APPLICATION
- TOOL/NC
mm”
 
 
Do not use the Emerqencv Stop Button for normal shut down as it will defeat the cool down
circuit.
 
 
al
- -TE APPLICATION
- TOOL/NC
mm”
 
 
Do not use the Emerqencv Stop Button for normal shut down as it will defeat the cool down
circuit.
 
 
al
 €15
APPLICAYIGN
TOOL/NE
 
Do not use the Circuit Breaker for normal shut down as it deieats the cool down circuit.
 
mu muuwwv
 
 
 
a\
€15
APPLICAYIGN
TOOL/NE
 
Do not use the Circuit Breaker for normal shut down as it deieats the cool down circuit.
 
mu muuwwv
 
 
 
a\
 mum:
 
 
Always use the Top Lock Pin to secure the hinqed conveyor top when i1 is not in the
horizontal position. Failure to do so can result in serious personal injury and/or damage to the
unit.
 
 
 
al
 
mum:
 
 
Always use the Top Lock Pin to secure the hinqed conveyor top when i1 is not in the
horizontal position. Failure to do so can result in serious personal injury and/or damage to the
unit.
 
 
 
al
 - .' TE
WWII-y
- .' TE
WWII-y
 
 
 
 - - TE APPLICAYIGN
- TOOL/N5
mm
 
 
 
Drive chain may cause personal iniurv or uroduct damaoe if finqers clothinq or product
enters into drive chain/sprocket area. Never operate machine without chain quard and left rear
belt guard in place.
 
 
ai
- - TE APPLICAYIGN
- TOOL/N5
mm
 
 
 
Drive chain may cause personal iniurv or uroduct damaoe if finqers clothinq or product
enters into drive chain/sprocket area. Never operate machine without chain quard and left rear
belt guard in place.
 
 
ai
 - -TE APPLICAT/ON
- TOOL/N6
mm
 
httg://www.wirebelt.com
Conveyor belt may cause personal injury or product damage if fingers clothing or product
gets entangled in belt slots or pinched between moving and stationary components. Exercise
caution when operating the machine. Never operate machine without all belt guards in place.
There are seven (7) belt guards on the machine. They are the front side center side and rear
side guards (both left and right sides) and the front belt guard.
 
 
 
 
 
 
 
al
- -TE APPLICAT/ON
- TOOL/N6
mm
 
httg://www.wirebelt.com
Conveyor belt may cause personal injury or product damage if fingers clothing or product
gets entangled in belt slots or pinched between moving and stationary components. Exercise
caution when operating the machine. Never operate machine without all belt guards in place.
There are seven (7) belt guards on the machine. They are the front side center side and rear
side guards (both left and right sides) and the front belt guard.
 
 
 
 
 
 
 
al
 .‘TE
mmrlv’fy
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
1CB Circuit Breaker, 2 Pole, 15A, 250VAC, 50/60 Hz, UL, CSA, VDE Approved
2PB Contact Block, 22.5mm IEC, 3 Across, NC
3PB Contact Block, 22.5mm IEC, 3 Across, NO
Button,
1NO Contact on "I" Button, 1NC Contact on "0" Button
1FLT Line Filler, 120/250 VAC, 20A, 50/60 HZ
Approved
Approved
CRM Relay Sockel, 4PDT, 10A, 220VAC, Surface or DIN Rail Mount
Approved
CRF,ZCR Relay Sockel, DPDT, 10A, 220VAC, Surface or DIN Rail Mount
Approved
1TMR Timer, Delay on Break, 20 Minute Delay Time, 1 A, 120 VAC 50/60 Hz
0.5 Sec. Cycle Time
1POT Digilal Polenliomeler, 3 Digit, 5K, 2 Watl, 0.1%
1R Resistor, Metal Oxide Film, 2 Walt, 5%,47K
Cover
1TS Terminal Slrip, 12 Position, Type G 5/12
1TS Terminal Slrip, 6 Position, Type G 5/6
SCR Electrical Subassembiy, R10 Relay Socket, 2 Pole
CRM,CRF,2,ECR Relay Mounting Track, DIN Style, 3 Fl. Extruded Aluminum Section
2XFMR Current Transformer, 600 Turns, 600 VAC Working Class, 50/60 Hz
Approved
1FU Fuse, IEC 5x20mm, Low Breaking, Time Delay, 250V, 1.6A
2FU Fuse, IEC 5x20mm, Low Breaking, Time Delay, 250V, 1A
0.250 Tabs
Tabs
1TVS Transient Voltage Surge Suppressor (MOV), 130VAC, 20mm Disk
2TVS Transient Voltage Surge Suppressor (MOV), 275VAC, 20mm Disk
 
 
 
 
ai
.‘TE
mmrlv’fy
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
1CB Circuit Breaker, 2 Pole, 15A, 250VAC, 50/60 Hz, UL, CSA, VDE Approved
2PB Contact Block, 22.5mm IEC, 3 Across, NC
3PB Contact Block, 22.5mm IEC, 3 Across, NO
Button,
1NO Contact on "I" Button, 1NC Contact on "0" Button
1FLT Line Filler, 120/250 VAC, 20A, 50/60 HZ
Approved
Approved
CRM Relay Sockel, 4PDT, 10A, 220VAC, Surface or DIN Rail Mount
Approved
CRF,ZCR Relay Sockel, DPDT, 10A, 220VAC, Surface or DIN Rail Mount
Approved
1TMR Timer, Delay on Break, 20 Minute Delay Time, 1 A, 120 VAC 50/60 Hz
0.5 Sec. Cycle Time
1POT Digilal Polenliomeler, 3 Digit, 5K, 2 Watl, 0.1%
1R Resistor, Metal Oxide Film, 2 Walt, 5%,47K
Cover
1TS Terminal Slrip, 12 Position, Type G 5/12
1TS Terminal Slrip, 6 Position, Type G 5/6
SCR Electrical Subassembiy, R10 Relay Socket, 2 Pole
CRM,CRF,2,ECR Relay Mounting Track, DIN Style, 3 Fl. Extruded Aluminum Section
2XFMR Current Transformer, 600 Turns, 600 VAC Working Class, 50/60 Hz
Approved
1FU Fuse, IEC 5x20mm, Low Breaking, Time Delay, 250V, 1.6A
2FU Fuse, IEC 5x20mm, Low Breaking, Time Delay, 250V, 1A
0.250 Tabs
Tabs
1TVS Transient Voltage Surge Suppressor (MOV), 130VAC, 20mm Disk
2TVS Transient Voltage Surge Suppressor (MOV), 275VAC, 20mm Disk
 
 
 
 
ai
 -.'TE
mmmrry
 
 
phase
 
elements
1500 Watts, 240V
 
 
 
 
 
 
 
 
 
999 pot setting)
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
114cm (45") x 135cm (53") x 64cm (25") high
 
 
 
at
-.'TE
mmmrry
 
 
phase
 
elements
1500 Watts, 240V
 
 
 
 
 
 
 
 
 
999 pot setting)
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
114cm (45") x 135cm (53") x 64cm (25") high
 
 
 
at
 .' TE
Mmrlv’fy
 
Such malfunctions are the only reasons to press the ErStop while the belts and lans
are still running. DO NOT use this as the normal shut down procedure as it will defeat the
cool down circuit.
 
 
al
.' TE
Mmrlv’fy
 
Such malfunctions are the only reasons to press the ErStop while the belts and lans
are still running. DO NOT use this as the normal shut down procedure as it will defeat the
cool down circuit.
 
 
al
 .' TE
Will/NI
 
Ii you plan to use the M105 Tunnel Oven in the 4" nominal position the below steps may
be skipped. Alwavs perform this operation with the control box power cord unpluqqed irom the
facililv's power outlet and the umbilical cord unoluqqed from the machine.
 
 
Hole
If you are iust unpacking the unit the Shipping Support is already installed.
 
 
al
.' TE
Will/NI
 
Ii you plan to use the M105 Tunnel Oven in the 4" nominal position the below steps may
be skipped. Alwavs perform this operation with the control box power cord unpluqqed irom the
facililv's power outlet and the umbilical cord unoluqqed from the machine.
 
 
Hole
If you are iust unpacking the unit the Shipping Support is already installed.
 
 
al
 £15
APPLICAYION
TOOL/NS
 
 
 
a\
£15
APPLICAYION
TOOL/NS
 
 
 
a\
 '-'J.IE
APPLICATION
TOOL/N6
 
 
 
a\
'-'J.IE
APPLICATION
TOOL/N6
 
 
 
a\
 .‘TE
mmumy
 
Usan the Emerqency Stop or circuit breaker as the normal shut down procedure
defeats the automatic cccl down circuit and will cause heat damage to the Tunnel Oven.
 
/_
¥
 
al
.‘TE
mmumy
 
Usan the Emerqency Stop or circuit breaker as the normal shut down procedure
defeats the automatic cccl down circuit and will cause heat damage to the Tunnel Oven.
 
/_
¥
 
al
 -.'TE
zonnKIMry
APPLICAYION
TOOL/NS
 
 
 
 
and
unnel
he
re
 
 
a\
-.'TE
zonnKIMry
APPLICAYION
TOOL/NS
 
 
 
 
and
unnel
he
re
 
 
a\
 
 - .' TE
mmrlvlry
- .' TE
mmrlvlry
 
 
 - - ' E APPLICAYION
- TOOL/NS
mmrlvlry
 
on
 
Do not use solvents for cleanino. Solvents are unnecessarv and may damaue some
components 01 the Tunnel Oven.
 
a\
- - ' E APPLICAYION
- TOOL/NS
mmrlvlry
 
on
 
Do not use solvents for cleanino. Solvents are unnecessarv and may damaue some
components 01 the Tunnel Oven.
 
a\
 -.'TE
mun/wry
APPLICATION
TOOL/N6
 
 
a\
-.'TE
mun/wry
APPLICATION
TOOL/N6
 
 
a\
 mum:
 
 
   
 
   
Belt Guard
":1-
 
Belt Guard
 
hng://www.wirebelt.cum
 
3‘
mum:
 
 
   
 
   
Belt Guard
":1-
 
Belt Guard
 
hng://www.wirebelt.cum
 
3‘
 .‘TE
Mmrlv’fy
 
Aiwavs secure Tunnel Oven TOD with in the uDr‘iaht Dositiun with the Top Lock Pin.
Failure to do so can resuit in serious personai ‘iniury and/or damage to the unit.
 
 
ai
.‘TE
Mmrlv’fy
 
Aiwavs secure Tunnel Oven TOD with in the uDr‘iaht Dositiun with the Top Lock Pin.
Failure to do so can resuit in serious personai ‘iniury and/or damage to the unit.
 
 
ai
 'TE
mmm’fy
 
 
Tunnel Oven's power to be
 
 
 
Main Power source not connected.
Connect power.
 
Stop.
 
Circuit breaker is off.
Turn on breaker.
 
activated.
 
Over Temperature Switch is faulty.
Replace switch.
 
Circuit breaker is defective.
Replace circuit breaker.
 
pressed.
 
("0") button.
 
Fuse 1FU or 2 FU blown.
Replace fuse.
 
Cool Down timer is defective.
Replace as necessary.
 
CRM is delective.
Replace CRM.
 
Control is transformer delective.
Replace 1XFMR.
 
Heater Elements failed.
Replace Heater Elements.
 
Element.
 
Element is faulty.
Element.
 
Solid state relay is defective.
Replace tSSR.
 
Temperature controller detective
Replace controller.
 
Master Control Relay Defective
Replace CRM.
 
programmed correctly.
 
 
Upper Heater Element.
 
programmed incorrectly.
 
 
 
Tunnel Oven.
 
 
 
al
'TE
mmm’fy
 
 
Tunnel Oven's power to be
 
 
 
Main Power source not connected.
Connect power.
 
Stop.
 
Circuit breaker is off.
Turn on breaker.
 
activated.
 
Over Temperature Switch is faulty.
Replace switch.
 
Circuit breaker is defective.
Replace circuit breaker.
 
pressed.
 
("0") button.
 
Fuse 1FU or 2 FU blown.
Replace fuse.
 
Cool Down timer is defective.
Replace as necessary.
 
CRM is delective.
Replace CRM.
 
Control is transformer delective.
Replace 1XFMR.
 
Heater Elements failed.
Replace Heater Elements.
 
Element.
 
Element is faulty.
Element.
 
Solid state relay is defective.
Replace tSSR.
 
Temperature controller detective
Replace controller.
 
Master Control Relay Defective
Replace CRM.
 
programmed correctly.
 
 
Upper Heater Element.
 
programmed incorrectly.
 
 
 
Tunnel Oven.
 
 
 
al
 'TE
mmm’fy
 
 
 
Solid state relay is defective.
Replace tSSR.
 
 
 
tCR is defective. Replace tCR.
CRM is detective. Replace CRM.
loo low. necessary.
 
programmed incorrectly.
 
Temperature controller is defective.
Replace the controller.
 
connections.
 
Solid state relay is defective.
Replace tSSR.
 
Fan is detective.
Replace the defective fan.
 
Thermocouple lead is shorted.
Repair shon.
 
Temperature controller is defective.
Replace controller.
 
Cool down timer is detective.
Replace tTMR.
 
connections.
 
A fan is defective.
Replace the defective fan.
 
 
 
connections.
laulty. connections.
Fan is detective. Replace fan.
 
Main Power source not connected.
Connect power.
 
sprockets.
tighten set screws.
 
motor. Check motor plug.
 
required.
 
Speed dial set to less than 100.
Increase speed setting.
 
Motor controller is defective.
Replace motor controller.
 
as necessary.
 
 
Motor controller is defective.
Replace controller.
 
Digital speed control is defective.
Replace as necessary.
 
 
are faulty.
 
 
required.
 
 
al
'TE
mmm’fy
 
 
 
Solid state relay is defective.
Replace tSSR.
 
 
 
tCR is defective. Replace tCR.
CRM is detective. Replace CRM.
loo low. necessary.
 
programmed incorrectly.
 
Temperature controller is defective.
Replace the controller.
 
connections.
 
Solid state relay is defective.
Replace tSSR.
 
Fan is detective.
Replace the defective fan.
 
Thermocouple lead is shorted.
Repair shon.
 
Temperature controller is defective.
Replace controller.
 
Cool down timer is detective.
Replace tTMR.
 
connections.
 
A fan is defective.
Replace the defective fan.
 
 
 
connections.
laulty. connections.
Fan is detective. Replace fan.
 
Main Power source not connected.
Connect power.
 
sprockets.
tighten set screws.
 
motor. Check motor plug.
 
required.
 
Speed dial set to less than 100.
Increase speed setting.
 
Motor controller is defective.
Replace motor controller.
 
as necessary.
 
 
Motor controller is defective.
Replace controller.
 
Digital speed control is defective.
Replace as necessary.
 
 
are faulty.
 
 
required.
 
 
al
 .' TE .;
Mmrlv’fy
 
The Upper Heater Etement and thermccuuple are a sinqle unit. It the wire or insutation
cannot be repaired the UDDer Heater Etement must be reDIaced.
 
 
at
.' TE .;
Mmrlv’fy
 
The Upper Heater Etement and thermccuuple are a sinqle unit. It the wire or insutation
cannot be repaired the UDDer Heater Etement must be reDIaced.
 
 
at
 .‘TE
Mmrlv’fy
 
The first part of this test is performed whlle the temperature controller is demandlnq full
Dower to the Heater Elements. The second part of the test is performed with the temDerature
controller is demandlnq no power to the Heater Elements.
 
 
al
.‘TE
Mmrlv’fy
 
The first part of this test is performed whlle the temperature controller is demandlnq full
Dower to the Heater Elements. The second part of the test is performed with the temDerature
controller is demandlnq no power to the Heater Elements.
 
 
al
 .' TE
Mmrlv’fy
 
When reinstalling the brushes ensure that they are seated in the same orientation as
when they were removed.
 
 
ai
.' TE
Mmrlv’fy
 
When reinstalling the brushes ensure that they are seated in the same orientation as
when they were removed.
 
 
ai
 - - I'E APPLICAYION
- TOOL/NE
mum
 
Only the MIN and MAX trimpols are used ior calibration purposes. The IR and CL trimpots
are set at the factor and should not be ad'usted.
 
 
 
Adjusting the MAX lrimpot affects the MIN setting and vise versa.
 
 
ai
- - I'E APPLICAYION
- TOOL/NE
mum
 
Only the MIN and MAX trimpols are used ior calibration purposes. The IR and CL trimpots
are set at the factor and should not be ad'usted.
 
 
 
Adjusting the MAX lrimpot affects the MIN setting and vise versa.
 
 
ai
 .' TE
Mmrlv’fy
 
If you are havinq trouble naviqatincl the below described menus and cannot Get out of one
of the many controller modes do not panic. The temperature controller will return to the Control
Mode ii there is no key entry activity for 2er minutes.
 
 
al
.' TE
Mmrlv’fy
 
If you are havinq trouble naviqatincl the below described menus and cannot Get out of one
of the many controller modes do not panic. The temperature controller will return to the Control
Mode ii there is no key entry activity for 2er minutes.
 
 
al
 - - I E APPLICATION
- TOOL/N6
tonnecllvlfy
 
 
e Selpoint
 
 
 
 
2 = Alarm 2 active, 1 = Alarm 1
active (Visible only it an alarm is
active)
 
 
O erator
Auto-Tu ni
Product Information
Con uration
Set U
 
Normal instrumenlo lion
Invoke Pre-Tune or Self-Tune
Partlow oductinlormation
Con ure device
Tailor settin
 
a\
- - I E APPLICATION
- TOOL/N6
tonnecllvlfy
 
 
e Selpoint
 
 
 
 
2 = Alarm 2 active, 1 = Alarm 1
active (Visible only it an alarm is
active)
 
 
O erator
Auto-Tu ni
Product Information
Con uration
Set U
 
Normal instrumenlo lion
Invoke Pre-Tune or Self-Tune
Partlow oductinlormation
Con ure device
Tailor settin
 
a\
 
 .‘TE:
 
 
mmmky
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
Configuration Lock
Code
 
 
 
 
0 Input Type YC inPt Type K thermocouple
0 Upper Range for Scaling (°C)
0 Lower Range for Scaling (°C)
0 Control Type SnGL 0th Single control (heat only)
0
Action
0 Alarm 1 Type dE ALA1 Alarm 1 = Deviation
0 Deviation Alarm = 30 °C
0 Alarm 1 Hysteresis = 1 °C
0 Alarm 2 Type bAnd ALA2 Alarm 2 = Band Alarm
0 Band Alarm = 20 “C
0 Alarm 2 Hysteresis = 1 °C
0 Loop Alarm diSA LAEn Loop Alarm disabled
0 Alarm Inhibit nonE Inhi No Inhibits
0 Output 1 Usage Pri USE1 Use Output 1 for primary control
0 Output 2 Usage A2_r USEZ Use Output 2 lor Alarm 2, Reverse
0 Output 3 Usage A1_d USES Use Output 3 for Alarm 1, Direct
0 Display Strategy 2 diSP Use second display strategy
0
 
 
 
al
.‘TE:
 
 
mmmky
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
Configuration Lock
Code
 
 
 
 
0 Input Type YC inPt Type K thermocouple
0 Upper Range for Scaling (°C)
0 Lower Range for Scaling (°C)
0 Control Type SnGL 0th Single control (heat only)
0
Action
0 Alarm 1 Type dE ALA1 Alarm 1 = Deviation
0 Deviation Alarm = 30 °C
0 Alarm 1 Hysteresis = 1 °C
0 Alarm 2 Type bAnd ALA2 Alarm 2 = Band Alarm
0 Band Alarm = 20 “C
0 Alarm 2 Hysteresis = 1 °C
0 Loop Alarm diSA LAEn Loop Alarm disabled
0 Alarm Inhibit nonE Inhi No Inhibits
0 Output 1 Usage Pri USE1 Use Output 1 for primary control
0 Output 2 Usage A2_r USEZ Use Output 2 lor Alarm 2, Reverse
0 Output 3 Usage A1_d USES Use Output 3 for Alarm 1, Direct
0 Display Strategy 2 diSP Use second display strategy
0
 
 
 
al
 :TE
 
tannerrlv’fy
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
O
Constant input lilter
0 Actual value determined by factory or field
calibration
0 Primary Power 7 PPW Power output (Read only)
0 Primary Proportional Proportional Band setting
Band (Actual setting may vary slightly)
0
(Actual setting may vary slightly)
0 Derivative time setting
(Actual setting may vary slightly)
0 Bias (Manual reset) 62 biAS Bias setting is 62
O Setpoint Upper Limit is 700 °C
0 Setpoint Lower Limit is 0 °C
0 Primary Output Control Output = 100%
Power Limit (Not limited)
0
0.5 seconds
0 Deviation Alarm = 30 °C
0 Alarm 1 Hysteresis Value : 1 ”C
0 Band Alarm = 20 “C
0 Alarm 2 Hysteresis Value : 1 ”C
0 Auto PrerTune diSA APt Auto PreiTune capability is disabled
0
Selection
0 Setpoint Ramping EnAb SPr Setpoint Ramping capability is disabled
0
Value
0 Setpoint 600°C (lactory setting — actual
setpoint determined by application
requirements)
0 Setup Lock Code 0 SLoc Setup Menu unlocked
 
 
 
 
 
 
 
al
:TE
 
tannerrlv’fy
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
O
Constant input lilter
0 Actual value determined by factory or field
calibration
0 Primary Power 7 PPW Power output (Read only)
0 Primary Proportional Proportional Band setting
Band (Actual setting may vary slightly)
0
(Actual setting may vary slightly)
0 Derivative time setting
(Actual setting may vary slightly)
0 Bias (Manual reset) 62 biAS Bias setting is 62
O Setpoint Upper Limit is 700 °C
0 Setpoint Lower Limit is 0 °C
0 Primary Output Control Output = 100%
Power Limit (Not limited)
0
0.5 seconds
0 Deviation Alarm = 30 °C
0 Alarm 1 Hysteresis Value : 1 ”C
0 Band Alarm = 20 “C
0 Alarm 2 Hysteresis Value : 1 ”C
0 Auto PrerTune diSA APt Auto PreiTune capability is disabled
0
Selection
0 Setpoint Ramping EnAb SPr Setpoint Ramping capability is disabled
0
Value
0 Setpoint 600°C (lactory setting — actual
setpoint determined by application
requirements)
0 Setup Lock Code 0 SLoc Setup Menu unlocked
 
 
 
 
 
 
 
al
 - -TE APPLICATION
- TOOL/NC
tonmrfvify
 
Lower
Upper
 
 
 
 
 
 
 
Display Display
0 PrerTune OFF Ptun PrerTune capability is disabled
0 SelfiTune OFF Stun SelfrTune capability is disabled
0 Tune Lock 0 tLoc Automatic Tuning Menu unlocked
 
 
 
 
 
 
 
 
Input Type Uni In 1 Input 1 is a universal type input
Option 1 Module Output 1 module = + 10 to 12 VDC for
Type driving a solid state relay
Type
Option 3 Module
Type
Type
Firmware Type 7 FW Value displayed is firmware type
 
 
 
 
 
 
O
O
O
O
O
O
O
O
O
O
O
O
 
 
 
 
Firmware Issue 7 I88 Value displayed is firmware issue
Product Revision
Level
Date of Manufacture 7 dOM Manufacturing date code (mmyy)
Serial Number 1 7 8m First four digits of serial number
Serial Number 2 7 Sn2 Middle four digits of serial number
Serial Number 2 7 Sn2 Last four digits of serial number
 
 
 
al
- -TE APPLICATION
- TOOL/NC
tonmrfvify
 
Lower
Upper
 
 
 
 
 
 
 
Display Display
0 PrerTune OFF Ptun PrerTune capability is disabled
0 SelfiTune OFF Stun SelfrTune capability is disabled
0 Tune Lock 0 tLoc Automatic Tuning Menu unlocked
 
 
 
 
 
 
 
 
Input Type Uni In 1 Input 1 is a universal type input
Option 1 Module Output 1 module = + 10 to 12 VDC for
Type driving a solid state relay
Type
Option 3 Module
Type
Type
Firmware Type 7 FW Value displayed is firmware type
 
 
 
 
 
 
O
O
O
O
O
O
O
O
O
O
O
O
 
 
 
 
Firmware Issue 7 I88 Value displayed is firmware issue
Product Revision
Level
Date of Manufacture 7 dOM Manufacturing date code (mmyy)
Serial Number 1 7 8m First four digits of serial number
Serial Number 2 7 Sn2 Middle four digits of serial number
Serial Number 2 7 Sn2 Last four digits of serial number
 
 
 
al
 -.'TE:-
:Mnerllv’fy
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
5090827000 Replacement Wirebelt
D330097000 Three Position Splice Clip Set
SCR Motor Controller Assy, 120V, Model KBMM w/ 0.25 Ohm Resistor,
Assembled
T/C
0283807000 Lower Heater Element, IR, 15.25"x 8.0", 1500 W, 240 VAC
8460027000 1TEMPCON Dynapar Temperature Controller, Programmed
8746067000 Replacement Motor Brush Set . Model 105 Tunnel Oven
Approved
Relay, DPST, 25A, 220VAC Contacts, 110 VAC 50/60Hz Coil, VDE
Approved
4986667000 30R Relay, Super Sensitive, SPDT, 2A, 115VAC Contacts, 5 VDC Coil
Relay, DPDT, 10A, 220VAC Contacts, 120 VAC 50/60HZ Coil, VDE
Approved
0506847000 4FAN Fan, Ball Bearing, 88/106 CFM, 120VAC 50/60 HZ, 4.69 X 4.69 X 1.5"
2437227000 173FAN Fan, Ball Bearing, 31 CFM, 120VAC, 3.62 X 3.62 X 0.98", with 12" leads
2419007000 Gearmotor, 1/12 HP, 130VDC, 0.7A
2111857000 4,6,7,10LT Ind. Light, 125 VAC Neon, Red, 0.5" Rnd Snap In Panel Mnt, 0.250 Tabs
Tabs
Ind. Light, 125 VAC Neon, Clear, 0.5" Rnd Snap In Panel Mnt, 0.250
Tabs
Approved
Switch, Temperature, NC, Open @ 225° F +/. 5°, Close @ 205° F +/7 5°,
Horizontal Tabs
8585157000 2FU Fuse, IEC 5x20mm, Low Breaking, Time Delay, 250V, 1A
Contact TE 1FU Fuse, IEC 5X20mm, Low Breaking, Time Delay, 250V, 1.6A
5143577000 1POT Digital Potentiometer, 3 Digit, 5K, 2 Watt, 0.1%
8127857000 1TMR Timer, Delay on Break, 20 Minute Delay Time, 1 A, 120 VAC 50/60 Hz
 
 
 
 
Cover
 
 
al
-.'TE:-
:Mnerllv’fy
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
5090827000 Replacement Wirebelt
D330097000 Three Position Splice Clip Set
SCR Motor Controller Assy, 120V, Model KBMM w/ 0.25 Ohm Resistor,
Assembled
T/C
0283807000 Lower Heater Element, IR, 15.25"x 8.0", 1500 W, 240 VAC
8460027000 1TEMPCON Dynapar Temperature Controller, Programmed
8746067000 Replacement Motor Brush Set . Model 105 Tunnel Oven
Approved
Relay, DPST, 25A, 220VAC Contacts, 110 VAC 50/60Hz Coil, VDE
Approved
4986667000 30R Relay, Super Sensitive, SPDT, 2A, 115VAC Contacts, 5 VDC Coil
Relay, DPDT, 10A, 220VAC Contacts, 120 VAC 50/60HZ Coil, VDE
Approved
0506847000 4FAN Fan, Ball Bearing, 88/106 CFM, 120VAC 50/60 HZ, 4.69 X 4.69 X 1.5"
2437227000 173FAN Fan, Ball Bearing, 31 CFM, 120VAC, 3.62 X 3.62 X 0.98", with 12" leads
2419007000 Gearmotor, 1/12 HP, 130VDC, 0.7A
2111857000 4,6,7,10LT Ind. Light, 125 VAC Neon, Red, 0.5" Rnd Snap In Panel Mnt, 0.250 Tabs
Tabs
Ind. Light, 125 VAC Neon, Clear, 0.5" Rnd Snap In Panel Mnt, 0.250
Tabs
Approved
Switch, Temperature, NC, Open @ 225° F +/. 5°, Close @ 205° F +/7 5°,
Horizontal Tabs
8585157000 2FU Fuse, IEC 5x20mm, Low Breaking, Time Delay, 250V, 1A
Contact TE 1FU Fuse, IEC 5X20mm, Low Breaking, Time Delay, 250V, 1.6A
5143577000 1POT Digital Potentiometer, 3 Digit, 5K, 2 Watt, 0.1%
8127857000 1TMR Timer, Delay on Break, 20 Minute Delay Time, 1 A, 120 VAC 50/60 Hz
 
 
 
 
Cover
 
 
al
 - - TE AWL/01mm
- TOOL/N6
mm
m zumwwsn/sn n
r—Afi
 
 
 
Wit *
 
 
 
 
 
 
 
 
 
 
 
 
 
H”
 
      
   
at 2
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
   
 
 
\L 552'
 
   
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
Nun:
:wwnuw: m n M w
was uwmxs: mm:
2 w: w LMUUDR mum
mm “3:: n; M cunnutmk:
:nwmm mmunn m
Emmy m m uncun my:
PIN wa Awawim:
 
1 ALL umuwm :Ecuwnnv
EnNm/cruks m is m u:
u: mm m m m can»:
muss mums: Nmtn
4 m amt/MED :En‘mmiv
:nmmrmw: (z [Wm/[n m
m m uk mm mu
VNJYE m mm was
uwzwvlii NM}:
3 ALL szcnvz [mm
(mm/ml) mecmRS m:
u M 5w W m smug
uv mm: mm: uwtwvlsz
NnYED
5 arm mu m mum:
3pm
smz, ma, am, saw
mm 04thva 57W '
a mum mun wow u;
- - TE AWL/01mm
- TOOL/N6
mm
m zumwwsn/sn n
r—Afi
 
 
 
Wit *
 
 
 
 
 
 
 
 
 
 
 
 
 
H”
 
      
   
at 2
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
   
 
 
\L 552'
 
   
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
Nun:
:wwnuw: m n M w
was uwmxs: mm:
2 w: w LMUUDR mum
mm “3:: n; M cunnutmk:
:nwmm mmunn m
Emmy m m uncun my:
PIN wa Awawim:
 
1 ALL umuwm :Ecuwnnv
EnNm/cruks m is m u:
u: mm m m m can»:
muss mums: Nmtn
4 m amt/MED :En‘mmiv
:nmmrmw: (z [Wm/[n m
m m uk mm mu
VNJYE m mm was
uwzwvlii NM}:
3 ALL szcnvz [mm
(mm/ml) mecmRS m:
u M 5w W m smug
uv mm: mm: uwtwvlsz
NnYED
5 arm mu m mum:
3pm
smz, ma, am, saw
mm 04thva 57W '
a mum mun wow u;
 
 Mmrlv’fy
 
 
 
 
  
—‘ Elk
E"E\\ E‘ :leP
E‘JULDNWE
 
 
 
 
 
(whtw)
 
 
 
 
 
   
'c
ma - .
, \ ?
pm
(m m» /
A \ / A
\ \ ‘ /_y\ ,
/ / /\ /\
:;LT
 
 
 
 
  
THE LAT
_ ,
Mmrlv’fy
 
 
 
 
  
—‘ Elk
E"E\\ E‘ :leP
E‘JULDNWE
 
 
 
 
 
(whtw)
 
 
 
 
 
   
'c
ma - .
, \ ?
pm
(m m» /
A \ / A
\ \ ‘ /_y\ ,
/ / /\ /\
:;LT
 
 
 
 
  
THE LAT
_ , Mmrlv’fy
 
 
Fie‘dSeNiceEMEA@1e.com
hug://tuu|ing.te.com/euroge
www.te.cum/suggortrcemer
 
a\
Mmrlv’fy
 
 
Fie‘dSeNiceEMEA@1e.com
hug://tuu|ing.te.com/euroge
www.te.cum/suggortrcemer
 
a\

 
                 
                 
                 
 
 
 
 Settings
        Settings
     Fast Delivery
                                    Fast Delivery
                                 Free Shipping
                                    Free Shipping
                                 Incoterms
                                    Incoterms
                                 Payment Types
                                    Payment Types
                                





 Marketplace Product
                                    Marketplace Product
                                 
                     
                                 
                                 
                                 
                         
                                 
                                 
                                 
                                 
                                 
                                 
                                 Switzerland
Switzerland