BitSim NOW
About
Since 1985, we’ve been specializing in the development of advanced vision systems, embedded systems, and camera electronics as a design house.
We help you to develop your camera, camera interfaces, network interface or other types of interfaces. The camera sensor might need a custom interface, or MIPI-CSI2, Camera link or just an SPI interface. Video is buffered on chip internal RAM or using external DDRx memory . To access the cloud or host computer, high speed internet access is needed. BitSim NOW can feed Video streams via the RTP protocol on top of our IP/UDP Ethernet FPGA IP-Block in 1G or 10G speeds, all accelerated in HW.
Imaging systems used to be based on PCs. Expensive cameras connected with cables into an expensive frame grabber in a big computer box running Windows.
A new way has evolved in recent years: low cost embedded systems based on Linux, handling both the camera sensors and the image processing as well as the host/cloud communication, all this in small packages.
For Machine Vision applications, BitSim NOW develops systems for quality control in production lines. We design complete systems, usually consisting of lighting, camera, mechanics, electronics, AI, and software.
At BitSim NOW we are doers. That means we handle the implementation part and get it to work: developing the hardware, translating an imaging design idea into algorithms, circuit boards, C/C++/Python code and accelerating functions in hardware based on powerful processing platforms including AI inference.
Additional E-mail Address: info@bitsimnow.com
Additional Office Location: Sandv 2, SE-352 45, Växjö, Sweden