Datenblatt für EVAL-AD7902SDZ Guide von Analog Devices Inc.

ANALOG DEVICES Evaluating the AD7902 Dual Pseudo Differential, 16-Bit, 1 MSPS PulSAR ADC
EVAL-AD7902SDZ User Guide
UG-608
One Technology Way P. O. Box 9106 Norwood, MA 02062-9106, U.S.A. Tel: 781.329.4700 Fax: 781.461.3113 www.analog.com
Evaluating the AD7902 Dual Pseudo Differential, 16-Bit, 1 MSPS PulSAR ADC
PLEASE SEE THE LAST PAGE FOR AN IMPORTANT
WARNING AND LEGAL TERMS AND CONDITIONS. Rev. 0 | Page 1 of 32
FEATURES
Full featured evaluation board for the AD7902
Versatile analog signal conditioning circuitry
On-board reference, reference buffers, and ADC drivers
System demonstration board compatible (EVAL-SDP-CB1Z)
PC software for control and data analysis of time and
frequency domain
EVALUATION KIT CONTENTS
EVAL-AD7902SDZ evaluation board
Wall power supply 9 V dc adapter
Daughter card power connector
ADDITIONAL EQUIPMENT/SOFTWARE NEEDED
System demonstration platform (EVAL-SDP-CB1Z)
Precision analog signal source
Power supply, +7 V/2.5 V (optional)
USB cable
SMA cable
PC running Windows XP SP2, Windows Vista, Windows 7, or
higher with USB 2.0 port
Evaluation software for the AD7902 (download from
AD7902 product page)
ONLINE RESOURCES
Documents Needed
AD7902 data sheet
EVAL-AD7902SDZ user guide
Required Software
EVAL-AD7902SDZ evaluation software
FAQs and Troubleshooting
TYPICAL SETUP
Figure 1. Typical Setup for the EVAL-AD7902SDZ
(EVAL-AD7902SDZ on Left and EVAL-SDP-CB1Z on Right)
SIGNAL SOURCE
SMA
CONNECTOR
PC
11798-001
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 2 of 32
TABLE OF CONTENTS
Features .............................................................................................. 1
Evaluation Kit Contents ................................................................... 1
Additional Equipment/Software Needed ...................................... 1
Online Resources .............................................................................. 1
Typical Setup ..................................................................................... 1
Revision History ............................................................................... 2
General Description ......................................................................... 3
Getting Started .................................................................................. 4
Software Installation Procedures ................................................ 4
Evaluation Board Setup Procedures ........................................... 7
Evaluation Board Hardware ............................................................ 8
Device Description ....................................................................... 8
Power Supplies .............................................................................. 8
Link Configuration Options ......................................................... 10
Evaluation Board Circuitry ........................................................... 11
Analog Inputs .............................................................................. 11
Reference ..................................................................................... 11
Serial Interface ............................................................................ 11
Modes of Operation ....................................................................... 12
SDP Controlled Mode ............................................................... 12
Standalone Mode ........................................................................ 12
How to Use the Software ............................................................... 13
Setting Up the System for Data Capture:
Board Operation/Connection Sequence ................................. 13
Starting the Software .................................................................. 13
Overview of the Main Window ................................................ 15
Generating a Waveform Analysis Report ................................ 16
Generating a Histogram of the ADC Code Distribution ..... 17
Generating a Fast Fourier Transform of AC Characteristics ...... 18
Generating a Summary of the Waveform, Histogram, and
Fast Fourier Transform .............................................................. 19
Evaluation Board Schematics and Artwork ................................ 20
E VA L-AD7902SDZ Schematics ............................................... 20
E VA L-AD7902SDZ Layout ....................................................... 26
Bill of Materials ............................................................................... 29
Related Links ................................................................................... 31
REVISION HISTORY
2/14Revision 0: Initial Version
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 3 of 32
GENERAL DESCRIPTION
The E VA L -AD7902SDZ is an evaluation board designed to
demonstrate the low power AD7902 performance and to
provide an easy to understand interface for a variety of system
applications. The AD7902 is a dual pseudo differential 16-bit,
1 MSPS PulSAR® ADC. A full description of the AD7902 is
available in the AD7902 data sheet and should be consulted
when using this evaluation board.
The evaluation board is ideal for use with the Analog Devices, Inc.,
system demonstration platform (SDP) board, EVAL-SDP-CB1Z.
The evaluation board interfaces to the SDP board via a 120-pin
connector. SMA Connectors J6, J10, J14, and J15 are provided
to connect a low noise analog signal source.
The user PC software executable controls the evaluation board
over the USB through the SDP board, EVAL-SDP-CB1Z.
On-board components include the following:
ADR435: high precision, buffered band gap 5.0 V reference
AD8031: reference buffer
ADA4841-1: signal conditioning circuit with op amps
ADP7104 and ADP2301: regulators to derive necessary voltage
levels on board
own. w'mamjvw m... nmmmmm —El NAmNAL NS’1RUMENTS SOFTWARE LIcENsE AGREEMENT D mmum mm. ma mommy stroke You ammo ms mm m com-m m: mmmN mum. unsruwt READ msmsebemmv nownmwms mE swim-«Emma mama ms mum aurmnm unuPLElEmE mmumm PRmiEEJaucuNaEmm ms Imus or m nsznzmmnvoummm a: worm mm mass-«m s mu on vanst Kcofli mama MszEEMEmMu as news) 3mm; lrs mum conwoue. cuckw: anagrams nmomo West. we Imwmu mom no not warm. at? usms sumamnaswmms somsmnmm {107 mm of mm ar ms sormniwmmwmrmnmwkmn MrEiMA o wry-mas»? comuznsm m: was vw ammo menu. mums mus wwficrm «mum cum": Réwm mm ruMumhummh—yfln-‘nmfimsm B25031“ m cmmmum W “El
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 4 of 32
GETTING STARTED
SOFTWARE INSTALLATION PROCEDURES
Download the evaluation board software from the AD7902
product page on the Analog Devices website, at
www.analog.com.
There are two parts to the installation:
AD7902 evaluation board software installation
EVAL-SDP-CB1Z system demonstration platform board
drivers installation
Warning
Install the evaluation board software and drivers before
connecting the evaluation board and EVAL-SDP-CB1Z board to
the USB port of the PC to ensure that the evaluation system is
correctly recognized when it is connected to the PC.
Installing the AD7902 Evaluation Board Software
To install the AD7902 evaluation board software,
1. Start the Windows operating system and download the
software from the AD7902 product page on the Analog
Devices website, at www.analog.com.
2. Unzip the downloaded file.
3. Double-click the setup.exe file to begin the evaluation
board software installation (see Figure 2).
Figure 2. AD7902 Evaluation Board Software Installation: Installation Begins
4. Select the location to install the software, and then click
Next. (The default location is C:\Program Files (x86)\
Analog Devices\AD7902_03 Evaluation Software\.
This location also contains the executable software and
example files.)
Figure 3. AD7902 Evaluation Board Software Installation:
Selecting the Location for Software Installation
(the Default Location Is Shown)
5. A license agreement appears. Read the agreement, and then
select I accept the License Agreement and click Next.
Figure 4. AD7902 Evaluation Board Software Installation:
Accepting the License Agreement
11798-003
11798-004
11798-005
.mummm. mamw—u W 1n, vm-bwnsumumx mkNum‘mwb—mnflm mmlnwmmmmuw :me ———| (—9 Please wait wl’l: setup lslnadmn. ' mfvm mum: on Welcome 00 Inc ADI SDP Drivers 2.] 960.2 Setup Wllard ummmmmxmmmamu anvsm anMymmur-wmy mmmme-umamwm. varvnsyslmflwsmhmmwvebmyw mm cickummmme
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 5 of 32
6. A summary of the installation is displayed. Click Next to
continue.
Figure 5. AD7902 Evaluation Board Software Installation:
Reviewing a Summary of the Installation
7. A dialog box shows the installation progress.
Figure 6. AD7902 Evaluation Board Software Installation:
Displaying Installation Progress
8. The dialog box informs you when the installation is
complete. Click Next.
Figure 7. AD7902 Evaluation Board Software Installation:
Indicating When the Installation Is Complete
9. The setup for the installation of the EVAL-SDP-CB1Z
system demonstration platform board drivers auto-
matically begins to load.
Figure 8. Loading the Setup for SDP Drivers Installation
Installing the EVAL-SDP-CB1Z System Demonstration
Platform Board Drivers
After the installation of the evaluation board software is complete,
a welcome window is displayed for the installation of the EVAL-
SDP-CB1Z system demonstration platform board drivers.
1. Make sure that all other applications are closed, and then
click Next.
Figure 9. EVAL-SDP-CB1Z Drivers Setup:
Beginning the Drivers Installation
11798-008
11798-009
mxelmmm‘m mmmnmxnmamvmmmz oompmmg the ADI sup Drivers WWII“ wwimsz‘uswnwrmwrm‘ lomdnlflw 2"‘960’2 SGIIJD Wllald lm,mmmwxmm.a¢kmimmmm. wvsovvrwulewzmunmmmm mm, (Kimmzmzmmri 59qu 2mm sou-mu. moan Mm mmmsmmmmflmm mm ”ammo:- umvmmmfi vale EquTQv‘QMW a vwmumxw-Wm m Wewmm HWMWM Ilyoumeannmhumemw,mmmecumnyw “MM“ Wilmwmm“ mnaum|m,mmmmswm.mwdm M51 yaw-um m; m hawk 3.5 s». we, men H (”mm (:\mmwm-wwm\ma\rw xmaI-wvc» 9 mm: w-wmwm , mu. EXKW‘ C:\LMfllWMfl-\lul\fw\mlfl_xss.m In wwd you Gk: m inns“ xhis dew: software’ NIMuAn-‘uq own, In, ADIDmhpmntTuo . mm“ mm Dmux a v. a mmmsmuuw-mmmu. . umpubfihknyoulmn Huwun g; 4:
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 6 of 32
2. Select the location to install the drivers, and then click Install.
Figure 10. EVAL-SDP-CB1Z Drivers Setup:
Selecting the Location for Drivers Installation
3. Installation of the SDP drivers begins.
Figure 11. EVAL-SDP-CB1Z Drivers Setup:
Beginning the Installation
4. A dialog box appears asking whether you would like to
install this device software. Click Install to confirm that
you would like to install the drivers.
Figure 12. EVAL-SDP-CB1Z Drivers Setup:
Granting Permission to Install Drivers
5. To complete the drivers installation, click Finish, which
closes the installation wizard.
Figure 13. EVAL-SDP-CB1Z Drivers Setup:
Completing the Drivers Setup Wizard
6. Before using the evaluation board, you must restart your
computer. A dialog box opens, giving you the following
options: Restart, Shut Down, Restart Later. Click the
appropriate button.
Figure 14. EVAL-SDP-CB1Z Drivers Setup:
Restarting the Computer
11798-012
11798-013
11798-014
11798-015
[tan-«1mm vdllfifilfl m— ”mm...“ .mommkwmmmm Jam“ V gm”, V Arm/cmwams .aw‘MMN . a nun/Ann Wm “mm ,« ”magma“ , ms , «mmmmmm .rmmm . WWW ,um ,. MMmem, . mm“
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 7 of 32
EVALUATION BOARD SETUP PROCEDURES
The AD7902 evaluation board connects to the (E VA L -SDP-CB1Z)
system demonstration board. The EVA L -SDP-CB1Z board is
the controller board, which is the communication link between
the PC and the main evaluation board.
Figure 1 shows a photograph of the connections made between
the E VA L -AD7902SDZ daughter board and the E VA L -SDP-CB1Z
motherboard.
Connecting the Evaluation and SDP Boards to a PC
1. Install the AD7902 software. Ensure that the EVA L -SDP-
CB1Z board is disconnected from the USB port of the PC
while installing the software. The PC must be restarted
after the installation is complete.
2. Before connecting power, connect the 120-pin connector, J5,
of the E VA L -AD7902SDZ board to Connector J4 on the
E VA L-SDP-CB1Z board. Nylon screws are included in the
E VA L-AD7902SDZ evaluation kit and can be used to
ensure that the E VA L-AD7902SDZ and E VA L-SDP-CB1Z
boards are connected firmly together.
3. Connect the 9 V power supply adapter included in the kit
to the E VA L -SDP-CB1Z.
4. Connect the E VA L -SDP-CB1Z board to the PC via the
USB cable. (If you are using Windows® XP, you may need to
search for the E VA L -SDP-CB1Z drivers. Choose to auto-
matically search for the drivers for the E VA L -SDP-CB1Z
board if prompted by the operating system.)
Verifying the Board Connection
1. Allow the Found New Hardware Wizard to run after the
E VA L-SDP-CB1Z board is plugged into your PC. (If you
are using Windows XP, you may need to search for the
E VA L-SDP-CB1Z drivers. Choose to automatically search
for the drivers for the E VA L -SDP-CB1Z board if prompted
by the operating system.)
2. Check that the board is connected to the PC correctly
using the Device Manager of the PC.
a. Access the Device Manager as follows:
i. Right-click My Computer and then click Manage.
ii. A dialog box appears asking for permission to
allow the program to make changes to your
computer. Click Ye s .
iii. The Computer Management box appears. From
the list of System To ols, click Device Manager.
b. Under ADI Development Tools, Analog Devices
System Development Platform SDP-B should appear
(see Figure 15), indicating that the E VA L -SDP-CB1Z
driver software is installed and that the board is
connected to the PC correctly.
Figure 15. Device Manager:
Checking that the Board Is Connected to the PC Correctly
11798-016
Table L Power Supplies Provided on the Board
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 8 of 32
EVALUATION BOARD HARDWARE
DEVICE DESCRIPTION
The AD7902 is a 16-bit, 1 MSPS, precision, power efficient, dual
pseudo differential PulSAR ADC that uses SAR-based
architecture and does not exhibit any pipeline delay or latency.
The AD7902 is specified for use with a single supply of 2.5 V
(VDD1, VDD2). The interface from the digital host to the
AD7902 uses 1.8 V/2.5 V/3.3 V/5.5 V logic. The AD7902 is
compatible with the SPI/QSPI/MICROWIRE/DSP serial
interface to transfer data conversions. Complete AD7902
specifications are provided in the AD7902 data sheet and
should be consulted in conjunction with this user guide when
using the evaluation board. Full details on the EVA L -SDP-
CB1Z are available on the Analog Devices website, at
www.analog.com.
Figure 26 to Figure 31 show the evaluation board schematics.
The board consists of an AD7902 ADC (U1) with a reference
(U6ADR435), and two ADC drivers (U12 and U17
ADA4841-1YRZ). The evaluation board is a flexible design that
enables you to adjust compensation components and operate
the evaluation board from an adjustable bench top power supply.
POWER SUPPLIES
The evaluation board can be powered from a wall adapter or
from a bench top power supply. By default, the board is set up
to operate from a 9 V wall adapter using the on-board power
supplies described in Table 1.
Table 1. Power Supplies Provided on the Board
Power Supply (V) Function Components Used
+5 SDP power ADP2301
+7.5 Positive rail ADP7104
2.5 Negative rail ADP2301
+2.5 ADC VDD rail ADP7104
+3.3 VDRIVE (digital power) ADP7104
Each on-board power supply is decoupled where it enters the
board as well as where it connects to each device. A single ground
plane is used on this board to minimize the effect of high frequency
noise interference.
Alternatively, the board can be powered from a bench top power
supply by using the J2 and J3 screw terminals and changing the
SL1 to SL4 and LK3 to LK5 solder link settings to Position B (see
Table 2). When bench top power is used, use of the wall adapter
and the on-board power supplies are no longer required.
Table 2. Solder LinksSettings for Bench Top Power Supply1
Link Setting Function
SL1
B
+V
S
SL2 B −VS
SL3 B −VS
SL4 B +VS
LK3 B V_SDP
LK4 B VREF
LK5 B VDD for ADC
1 All other solder link settings are as described in Table 3.
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 9 of 32
Figure 16. Simplified Evaluation Board Functional Block Diagram
11798-002
SDP BOARDAD7902/AD7903 PulSAR EVALUATION BOARD
VIN1+
VIN1–
IN1+
IN1–
ADC1
+V
S
–V
S
GND
+5V
ADSP-BF527
DSP
SPORT
SCK1
SDO1
CNV1
VIO1
SDI1
REF1
+7.5V
VDD1
ADA4841-1
ADA4841-1
A B
–2.5V
–2.5V
+7.5V
GND
VCM
AD8031
POWER SUPPLY CIRCUITRY
ADP7104, ADP2301
V
IN
= 9V
WALL ADAPTER
VDD
VSDP
GND
(OPTIONAL)
(OPTIONAL)
+7.5V/–2.5V 2.5V +7.5V 3.3V +5V
ADR435
GLUE
LOGIC
IN2+
IN2–
ADC2 SCK2
SDO2
CNV2
VIO2
SDI2
REF2
+7.5V VDD2
ADA4841-1
ADA4841-1
A B
–2.5V
–2.5V
+7.5V
GND
GLUE
LOGIC
2.5V
VIN2–
VIN2+
5V
5V
Table 3‘ Solder LinksiFactory Default Settings
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 10 of 32
LINK CONFIGURATION OPTIONS
Care should be taken before applying power and signals to the
evaluation board to ensure that all link positions are as required
by the operating mode. There are two modes in which to operate
the evaluation board. The evaluation board can be operated in
SDP controlled mode to be used with the SDP board, or the
evaluation board can be used in standalone mode.
When operating in SDP controlled mode, ensure that VIO is
3.3 V. Operating with a VIO greater than 3.3 V in SDP controlled
mode may damage the SDP board.
The Setting column of Table 3 shows the default positions in which
the links are set when the evaluation board is packaged. When
the board is shipped, it is assumed that you are going to operate
the evaluation board with the SDP board (SDP controlled mode).
Table 3. Solder LinksFactory Default Settings
Link Setting Function Comment
SL1 A +VS Change to B if using bench supplies.
SL2
A
−V
S
Change to B if using bench supplies.
SL3 A −VS Change to B if using bench supplies.
SL4 A +VS Change to B if using bench supplies.
SL5 B Analog input Do not alter.
SL6 B Analog input Do not alter.
LK1 A +VS Change to B if using bench supplies.
LK2 A −VS Change to B if using bench supplies.
LK3 A V_SDP Change to B if using bench supplies.
LK4 A VREF Change to B if using bench supplies.
LK5 A VDD for ADC Change to B if using bench supplies.
LK6 Not applicable Not applicable Do not place
LK7 Not applicable Not applicable Do not place
LK8 A ADC2 input Do not alter.
LK9 A ADC2 input Change to B if using ADC1 input.
LK10 A U17 input Change to B if U17 needs to be bypassed.
LK11 A U17 input Change to B if U17 needs to be bypassed.
LK12 A ADC2 input Do not alter.
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 11 of 32
EVALUATION BOARD CIRCUITRY
ANALOG INPUTS
The analog inputs to the evaluation board are SMA Connectors J6
and J14. These inputs are buffered with dedicated amplifier
circuitry (U12 and U17), as shown in Figure 26 and Figure 27.
The circuit not only allows different configurations, input range
scaling, and filtering but also allows adding a dc component and
using different op amps and supplies. The analog input amplifiers
are set as unity-gain buffers by factory default. The amplifier
positive rail is driven from 7.5 V (from U13ADP7104). The
negative amplifier rail is driven from –VS (generated by U3
ADP2301).
The default configuration sets all op amps (U12 and U17) at
midscale, generated from a buffered reference voltage divider
(VCM).
The evaluation board is configured by factory default for providing
a pseudo differential analog input path to ADC1 and ADC2 (see
Figure 16).
For dynamic performance, an FFT test can be done by applying
a very low distortion ac source.
For low frequency testing, the audio precision source can be
used directly because its outputs are isolated. Set the outputs as
balanced with a floating ground. The J10 and J15 connectors are
provided for balanced termination of a signal source. Different
sources can be used; however, most are single-ended sources
that use a fixed output resistance.
By default, the evaluation board uses the amplifiers as unity-gain
buffers. The noninverting input has a common-mode adjustment
that involves a 100 kshunt resistor. This resistor creates a
voltage divider with the source, which must be accounted for
when using the board.
REFERENCE
An external 5 V reference (U6ADR435) is used to supply the
ADCs directly.
SERIAL INTERFACE
The evaluation board uses the SPORT interface from the
ADSP-BF527 D S P.
Multiple AND gates (U9, U10, and U11) are used to clock and
gate the SPORT transfer to the ADC device.
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 12 of 32
MODES OF OPERATION
SDP CONTROLLED MODE
The AD7902 uses a high speed serial interface that allows sampling
rates of up to 1 MSPS. For more information about the operation of
the serial interface, refer to the AD7902 data sheet.
The AD7902 uses the serial interface to transfer data to the
E VA L-SDP-CB1Z.
The E VA L -AD7902SDZ communicates with the E VA L -SDP-
CB1Z board using level shifters. The E VA L -SDP-CB1Z operates
at a 3.3 V logic level, which allows logic voltages that exceed
3.3 V to be used without damaging the SDP interface.
STANDALONE MODE
The E VA L -AD7902SDZ can also be used without the E VA L -SDP-
CB1Z controller board. In this case, the E VA L -AD7902SDZ is
connected to the serial interface using the J5 connector or the
test points. For more information about the operation of the
serial interface, refer to the AD7902 data sheet.
> Hardware Seiect System Develnpmenl Plallnrm Wail b Hdrdwarsl §olart MSDPsystanwasfufl,Mhedadlbboudwssmt demmd.mmdammdsamdndma wmmwmmawwmc IfmsDPisrmflymcmdmmbehhmof boofixg‘witmscumdm, Sdecfiucamflwlahwsoflwaremmmhsm ninth Rescan Select AnSDPsvshanwasm.Mfl1edanhherbwdwasr\ot dammidcedxmeda‘mmboardisahadndma mamsmmmkescanwcmmabm. IfmsDPisrecmflvmrmdetmaybenfiepmmsof Immigwitnmardllsm. mwflahwsoflwxemmmhsm madl- No Hardware Connected. Sofiware VII oped! In shod-alone mode.
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 13 of 32
HOW TO USE THE SOFTWARE
SETTING UP THE SYSTEM FOR DATA CAPTURE:
BOARD OPERATION/CONNECTION SEQUENCE
With the evaluation software installed, the following board
operation/connection sequence can be used:
1. Connect the SDP controller board to the evaluation board
via the J5 connector (screw into place as required). The
software is configured to find the evaluation board on either
the J4 or J5 connector of the SDP board.
2. Power the board with the appropriate supply, as described
in the Power Supplies section.
3. Connect the E VA L -SDP-CB1Z board to a PC using the
USB cable.
4. Start the evaluation software. Click Start > All Programs >
AD7902_03_Evaluation > AD7902_03_Evaluation_
Software.
5. Apply a signal source and capture data.
STARTING THE SOFTWARE
When the software starts running, it searches for hardware
connected to the PC. The software automatically detects the
generic attached to the PC, or you can choose to run the software
in standalone mode without any hardware connected.
With Hardware Connected
To run the program with hardware connected,
1. Click Start > All Programs > AD7902_03_Evaluation >
AD7902_03_Evaluation_Software. (To uninstall the
program, click Start > Control Panel > Add or Remove
Programs > AD7902_03_Evaluation.)
2. If the SDP board is not connected to the USB port when
the software is launched, a connectivity error displays (see
Figure 17). If a connectivity error is displayed, connect the
evaluation board to the USB port of the PC, wait a few
seconds, click Rescan, and follow the instructions.
Figure 17. SDP Board Not Connected to the USB Port Pop-Up Window Error
3. After finding the evaluation board, the software connects
to the board and displays the dialog box shown in Figure 18.
Figure 18. Software Connects to SDP Board
4. After the board is correctly detected, the main window of
the software appears (see Figure 21), showing that the
E VA L-AD7902SDZ board is connected.
Without Hardware Connected
The software can run in standalone mode when no evaluation
board hardware is connected to the USB port.
1. Click Start > All Programs > AD7902_03_Evaluation >
AD7902_03_Evaluation_Software.
2. The software automatically seeks to find the hardware
connected; therefore, when no hardware is connected, a
connectivity error is displayed (see Figure 19). If you wish to
continue without hardware in standalone mode, click Cancel.
Figure 19. No Hardware Connected Pop-Up Window Error
3. The software alerts the user that no hardware is connected
and that the software is going to continue in standalone mode.
Figure 20. Software Indicates Operating in Standalone Mode
11798-017
11798-018
11798-019
11798-020
m. m w AD7902/AD7903 Evaluation Software ”WNM“ [cmmymm [W [m mm,“ m g o “W mam mm mm,” .mmmw. mm m. In) mm, mm 4cm.” wmmw mm; mms, ~ mm.” . [E mm
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 14 of 32
4. You can then load example files or previously saved files and
analyze data. The main window of the software appears (see
Figure 21), showing the evaluation board connected as the
part number from the saved data file.
5. If you decide to connect hardware at this point, you must
close the software and relaunch it to allow it to search for
the board again.
Figure 21. Main Window
11798-021
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 15 of 32
OVERVIEW OF THE MAIN WINDOW
The main window of the software is shown in Figure 21 and has
the features described in this section.
File Menu
The File menu offers the choice to
Load data: load previously captured data.
Save Data as .tsv: save captured data in .tsv format for
future analysis.
Save Picture: save the current screen capture.
Print: print the main window to the default printer.
Exit: close the application.
Eval Board Connected Box
The Eval Board Connected box displays the evaluation board con-
nected to the USB port—either E VA L -AD7902 or E VA L -AD7903.
When an evaluation board is not connected to the USB port, the
software can be operated in standalone mode for data analysis,
and the part information notes the part number from the saved
data file.
ADC Settings Area
The ADC Settings area allows changing the sampling frequency
and the reference voltage value, as well as selecting Channel 1 or
Channel 2.
Reference Voltage (V) Box
By default, the external reference voltage is 5 V (ADR435 on-board
reference). The minimum/maximum voltage calculations are based
on this reference voltage. If you change the reference voltage, you
must change this input accordingly.
Sampling Freq (Hz) Box
The default sampling frequency (10000000 Hz) in the Sampling
Freq (Hz) box matches the maximum sample rate of the ADC
connected to the board. Although you can adjust the sampling
frequency, there are limitations in terms of the sample frequencies
that can be entered related to the SCLK frequency applied. The
sample frequency must be an integer divider of the SCLK
frequency. If an unusable sample frequency is input, the software
automatically adjusts the sample frequency accordingly. Units
can be entered as, for example, 10k for 10,000 Hz. The software
automatically adjusts the sample frequency according to the ability
of the ADC connected to the board. For example, if you enter a
value that is beyond the ability of the device, the software indicates
this and reverts to the maximum sample frequency.
Select Channels Checkboxes
Select either Channel 1 or Channel 2 or both to read the data
from a single ADC or both ADCs simultaneously.
Tabs Area
There are five tabs available in the tabs area of the main window:
Configure, Waveform, Histogram, FFT, and Summary. These
tabs display the data in different formats. Navigation tools are
provided within each tab to allow you to control the cursor,
zooming, and panning (see Figure 22) within the graphs displayed.
Each tab is described in more detail in the Generating a
Waveform Analysis Report; Generating a Histogram of the
ADC Code Distribution; Generating a Fast Fourier Transform
of AC Characteristics; and Generating a Summary of the
Waveform, Histogram, and Fast Fourier Transform sections.
Single Capture Button
Clicking Single Capture performs a single capture from the ADC.
Continuous Capture Button
Clicking Continuous Capture performs a continuous capture
from the ADC.
Num Samples Box
The Num Samples box allows you to select the number of
samples to analyze.
Exit Button
Clicking the Exit button (in the upper right corner of the
window) closes the software. Alternatively, you can select Exit
from the File menu.
AD7902/AD7903 Evaluation Software ‘Ewfimmnmwim m WW W m 55am swan mm mm Mama Am , m f man 1 mp- Em xww a 0 mm mm noon mu 2mm way-lam Wm “Wm; Lnuuusa nan-m immuyfl ”Hawaiian. vrzuga mumm4isf MT}: 5. num-xymns w mmwmmue mm 1.11m my
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 16 of 32
GENERATING A WAVEFORM ANALYSIS REPORT
Figure 22 illustrates the Wav e for m tab for a 10 kHz sine wave
input signal when the on-board 5 V external reference is used.
The Waveform Analysis area (located toward the bottom of the
window) reports the amplitudes recorded from the captured signal
and the frequency of the signal tone. Select the Channel 1 tab
or Channel 2 tab in the Waveform Analysis area to view the
corresponding waveform.
Figure 22. Waveform Tab
11798-022
CONTROL
CURSOR CONTROL
PANNING
CONTROL
ZOOMING
AbiéOZ/AD7903 Evaluatlon Software m... 'wmfumn £15.... mg; ”ming Q "mmm [5... e... um». osmo- Mm mm MM..- ’ mu “mm :mm «1" am sq Rum mm v an us- M mam V I3"). w nmmwa. om- m ‘mmx-m m 1.1m: MV 0
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 17 of 32
GENERATING A HISTOGRAM OF THE ADC CODE
DISTRIBUTION
The Histogram tab can be used to perform ac testing or, more
commonly, dc testing. This tab shows the ADC code distribution of
the input and computes the mean and standard deviation, which are
displayed as DC Offset/Mean and Transition Noise, respectively,
in the Histogram Analysis area (located toward the bottom of
the window).
Figure 23 shows the histogram with ac input for a 1 kHz sine
wave applied to the ADC input and the resulting calculations.
AC Input
To perform a histogram test of ac input,
1. Apply a sinusoidal signal with low distortion (better than
100 dB) to the evaluation board at the J6 or J14 input SMA
connector pair.
2. Click the Histogram tab from the main window.
3. Click Single Capture or Continuous Capture.
Raw data is then captured and passed to the PC for statistical
computations, and various measured values are displayed in the
Histogram Analysis area.
DC Input
A histogram test of dc input can be performed with or without
an external source because the evaluation board has a buffered
VREF/2 source at the ADC input.
To perform a histogram test of dc input,
1. If an external source is being used, apply a sinusoidal signal
with low distortion (better than 100 dB) to the evaluation
board at the J6 or J14 input SMA connector pair. It may be
required to filter the signal to ensure that the dc source is
noise-compatible with the ADC.
2. Click the Histogram tab from the main window.
3. Click Single Capture or Continuous Capture.
Raw data is then captured and passed to the PC for statistical
computations, and various measured values are displayed in the
Histogram Analysis area.
Figure 23. Histogram Tab
11798-023
AD7902/AD7903 Evaluation Software 15...". me\ -1’m «5...; sum-- wan-a“:- wwlmmmzmmm-mtmam u-mm.) .. m mm um mum mm pm W aim 5c ”emu um u. rm Inn-m nan n. v: mm ,. unma- m. m u: ‘Lst name: an Man'u a mum- un- u. mmnw- mx an we om - um u. m 54m|y u...» mu a
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 18 of 32
GENERATING A FAST FOURIER TRANSFORM
OF AC CHARACTERISTICS
Figure 24 shows the FFT tab. This feature tests the traditional
ac characteristics of the converter and displays a fast Fourier
transform (FFT) of the results.
To perform an ac FFT test,
1. Apply a sinusoidal signal with low distortion (better than
100 dB) to the evaluation board at the J6 or J14 input SMA
connector pair. To attain the requisite low distortion,
which is necessary to allow true evaluation of the part, one
option is to
a. Filter the input signal from the ac source. A band-pass
filter can be used; its center frequency must match the
test frequency of interest.
b. If a low frequency band-pass filter is used when the full-
scale input range is more than a few volts peak-to-peak,
use the on-board amplifiers to amplify the signal, thus
preventing the filter from distorting the input signal.
2. Click the FFT tab from the main window.
3. Click Sample.
As in the histogram test, raw data is then captured and passed
to the PC, which performs the FFT and displays the resulting
SNR, SINAD, THD, and SFDR.
The FFT Analysis area displays the results of the captured data.
The area labeled 1 in Figure 24 shows the spectrum
information.
The area labeled 2 in Figure 24 displays the fundamental
frequency and amplitude. You can also click Show
Harmonic Content to view information about the second
to fifth harmonics.
The area labeled 3 in Figure 24 displays the performance data,
including the SNR, THD, SINAD, and noise performance.
Figure 24. FFT Tab
11798-024
1 2 3
M .. .. w. AD7902/AD7903 Evaluatlon Software aw W W m a“... mu m 0 m wm-w n4... m,“ v w. m nmw g. Kan-elm mm: y 2mm ‘5-
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 19 of 32
GENERATING A SUMMARY OF THE WAVEFORM,
HISTOGRAM, AND FAST FOURIER TRANSFORM
Figure 25 shows the Summary tab. The Summary tab captures
all the display information and provides it in one panel with a
synopsis of the information, including key performance parameters,
such as SNR and THD.
Figure 25. Summary Tab
11798-025
ADC 1 DRWERS AAAAAA
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 20 of 32
EVALUATION BOARD SCHEMATICS AND ARTWORK
EVAL-AD7902SDZ SCHEMATICS
Figure 26. Schematic, Page 1
11798-026
LT
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 21 of 32
Figure 27. Schematic, Page 2
11798-027
Sex 3773 ”773737me zOCumzzou WED/$7.7 127707770 9135.: _U is; m éU|A n“ 7 7 . u 7 7 . n 7 2 a i 7 7 EsmHui 7 g . . n a a» 7 5% 1 7 . A 7 ,Eflnmfluvl : 7 m... 7 f 3 7 2: W7
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 22 of 32
Figure 28. Schematic, Page 3
11798-028
m m -. mm .1 K , , , , , , , , , in: n|l z , , , , , , M :Ly m E if u5o> . 5+ u z; AW :4, 22.“ 3% m > 1 0E; w Em fi E .iA WIN“): \\\\\\\\\\\\\\\ L >m.w\ ijo> . >m+ H 27> é “m ”A 39:35 E 3&3 35$ :3 :51 3
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 23 of 32
Figure 29. Schematic, Page 4
11798-029
SE 76 2 3.7577 2 3 mum: 559%? Euflfl 565%? 257 new 2378: .7 213 NW E. wx :5: n S «x 5555 E35: :7 E :7 x: a : >m+ u 2 7 a g NEEEE : 7 7 7 7 7 7 7 7 7 2 7 7 7 7 7 7 7 U702 mam 707 >733 7370.7 7 7 $77.; 7 54 m ‘ 939: < 03="">3 om< 707="" banjm="" $7,707="" 7="" 7="" 7="" 7="" 7="" 7="" 7="" 7="" 7="" 7="" 7="" 7="" 7="" 7="" w="" e="" 55;:="" 7="" 7="" 7="" :2="" a:="" hum="" 7="" w="" 7="" 7am|m|m="" a="" 7="" g="" :4="" 7="" 7="" 7="" :2="" 5:="" h.717="" 7="" 7="" (="" 7="" 7="" 7="" 7="" 7="" 7="" 7="" 7="" 7="" 7="">
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 24 of 32
Figure 30. Schematic, Page 5
11798-030
SUP CONNH} \ OR $3; \NTERFACE GLUE LOG‘C slaqu m A ... m w.“ Us: sup
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 25 of 32
Figure 31. Schematic, Page 6
11798-031
‘ v uANAE "' '3 E5935" un$\\” 20 Lead Dual PuISAR 2 ifiiffif‘j “:mfififgu 5 “‘. DD H D" 4 D? ‘EELLJDU" vmu a: ‘ a n r“ W. E." Eganmfiggfi u: 1 n, g“ m Ed] E3“ mam Haj; ; IEZIEij] m“ 7 :D' Dry—v: may“; 5:: f D #5? DEE D“ u. ”an“ Es {flags Wu P “WHD um Eh VIII” mm “mm Erufiflfl mfi'm 3333:3155 rims“ Wm». RH HH‘ mm: m KI]
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 26 of 32
EVAL-AD7902SDZ LAYOUT
Layout Considerations
When laying out the printed circuit board (PCB) for the AD7902,
follow the recommended guidelines described in this section to
obtain the maximum performance from the converter. Figure 33
through Figure 36 show the recommended layout for the AD7902
evaluation board.
Decouple all the power supply pins (VDD1, VDD2, and
VIO) and the REF pin with low ESR and low ESL ceramic
capacitors, typically 10 µF and 100 nF, placed close to the
DUT (U1) and connected using short, wide traces to provide
low impedance paths and to reduce the effect of glitches on
the power supply lines.
Separate analog and digital sections and keep power supply
circuitry away from the AD7902.
Avoid running digital lines under the device and crossover
of digital and analog signals because these couple noise into
the AD7902.
Figure 32. EVAL-AD7902SDZ Evaluation Board SilkscreenTop Assembly
11798-032
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 27 of 32
Figure 33. EVAL-AD7902SDZ Evaluation BoardTop Layer
Figure 34. EVAL-AD7902SDZ Evaluation Board Layer 2Ground
11798-033
11798-034
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 28 of 32
Figure 35. EVAL-AD7902SDZ Evaluation Board Layer 3Power
Figure 36. EVAL-AD7902SDZ Evaluation Board Bottom Layer
11798-035
11798-036
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 29 of 32
BILL OF MATERIALS
Table 4. EVAL-AD7902SDZ Bill of Materials
Reference Designator Part Description Manufacturer Part Number Stock Code
U1 Dual pseudo differential 16-bit, 1 MSPS
PulSAR ADC
Analog Devices AD7902 AD7902
U2 1.2 A, 20 V, 1.4 MHz nonsynchronous step-
down switching regulator
Analog Devices ADP2301AUJZ ADP2301AUJZ-R7
U3 1.2 A, 20 V, 1.4 MHz nonsynchronous step-
down switching regulator
Analog Devices ADP2301AUJZ ADP2301AUJZ-R7
U4 Linear regulator, 3.3 V, 20 V, 500 mA,
ultralow noise, CMOS
Analog Devices ADP7104ARDZ-3.3 ADP7104ARDZ-3.3-R7
U5 2.7 V, 800 µA, 80 MHz rail-to-rail I/O single
amplifier SOT23-5
Analog Devices AD8031ARTZ AD8031ARTZ-R2
U6 Ultralow noise XFET voltage references Analog Devices ADR435BRZ ADR435BRZ
U7 Linear regulator, 2.5 V, 20 V, 500 mA, ultralow
noise, CMOS
Analog Devices ADP7104ARDZ-2.5 ADP7104ARDZ-2.5-R7
U8 Single INV Fairchild NC7SZ04M5 Farnell 1013809
U9
Single AND gate
Fairchild
NC7SZ085M5
Farnell 1013807
U10
Single AND gate
Fairchild
NC7SZ085M5
Farnell 1013807
U11 Single AND gate Fairchild NC7SZ085M5 Farnell 1013807
U12
Low noise, high speed amplifier for 16-bit
systems
Analog Devices
ADA4841-1YRZ
ADA4841-1YRZ-R7
U13 20 V, 500 mA, low noise, CMOS adjustable LDO Analog Devices ADP7104ARDZ ADP7104ARDZ-R7
U14 Not applicable Not applicable Not applicable Do not place
U15 32k I2C serial EEPROM, 8-lead MSOP Microchip 24LC32A-I/MS Farnell 1331330
U16 Not applicable Not applicable Not applicable Do not place
U17 Low noise, high speed amplifier for 16-bit
systems
Analog Devices ADA4841-1YRZ ADA4841-1YRZ-R7
C1, C2, C5, C9, C11,
C13, C19
Capacitor tantalum, 20 V AVX TAJB106K020RNJ Farnell 197427
C3, C4, C6, C7 Capacitor ceramic, 4.7 µF, 16 V, X7R, 0805 Taiyo Yuden EMK212B7475KG-T Farnell 1853520
C8, C20, C23, C25, C27,
C28, C30, C31, C34,
C37, C41, C42, C44,
C53, C54, C56, C57,
C59, C77, C78
Capacitor ceramic, 50 V, X7R Murata GRM188R71H104KA93D Farnell 8820023
C9 Capacitor ceramic, 50 V, X7R, 0805 Murata C0805C104K5RACTU Farnell 1414664
C12, C40, C79 Capacitor ceramic, 22 µF, 10 V, X7R, 1206 AVX LMK316AB7226ML-TR Farnell 1894515
C14 Capacitor ceramic, 4.7 µF, 16 V, X5R, 1206 Taiyo Yuden EMK316BJ475KL-T Farnell 6578937
C15, C16, C17, C21,
C22, C26
Capacitor, 0805, 1 µF, 50 V, X7R Murata GRM21BR71H105KA12L Farnell 1735541
C18 Capacitor ceramic, 50 V, X7R Murata GRM188R71H103KA01D Farnell 1118178
C33, C58 Capacitor ceramic ,10 pF, 100 V, C0G, 0603 AVX 06031A100JAT2A Farnell 1273324
C35, C74 Capacitor ceramic, 2700 pF, 50 V, C0G/NP0,
0603
TDK C1608C0G1H272J Farnell 1844178
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 30 of 32
Reference Designator Part Description Manufacturer Part Number Stock Code
C24, C29, C32, C36,
C38, C39, C43, C45,
C46, C47, C48, C49,
C50, C51, C52, C55,
C60, C61, C62, C63,
C65, C66, C67, C68,
C69, C70, C71, C72,
C73, C75, C76, C80,
C81
Not applicable Not applicable Not applicable Do not place
R1 Resistor, thick film, 2.4 , 0603, 100 mW, 1% Yageo RC0603FR-072K4L Farnell 1799329
R2 SMD resistor Multicomp MC 0.1W 0805 1% 62K Farnell 9333436
R3 Resistor, 0603, 35.7 Multicomp MC 0.063W 0603 1%
35K7
Farnell 1170942
R4 SMD resistor Multicomp MC 0.0625W 0402 1%
53K6
Farnell 1803723
R5 SMD resistor Multicomp MC 0.0625W 0402 1%
10K2
Farnell 1803137
R6 Resistor, 0603, 16.9 Multicomp MC 0.063W 0603 1%
16K9
Farnell 1170908
R7 Resistor, 0805, 12.1 , 1% Vishay Draloric CRCW080512K1FKEA Farnell 1469866
R10 Resistor, 0603, 82 , 0.063 W, 1% Multicomp MC 0.063W 0603 1%
82K
Farnell 9331573
R11, R13, R42, R44 SMD resistor Multicomp MC 0.063W 0603 1%
100K
Farnell 9330402
R12, R15
Resistor, 20 , 0.063 W, 1%, 0603
Multicomp
MC 0063W 0603 1 20K
Farnell 9330771
R14, R20, R21, R23,
R25, R26, R36, R45,
R48, R53, R63, R69,
R70, R71, R72
SMD resistor
Multicomp
MC 0.063W 0603 0R
Farnell 9331662
R17, R22, R46, R47 Resistor, 0805, 49.9 Ω, 0.1%, 0.125 W Panasonic ERA6AEB49R9V Farnell 1810805
R28, R35, R50, R74 Resistor, 2 , 0.1 W, 1%, 0805 Multicomp MC 01W 0805 1 2K Farnell 9332766
R27, R34, R49, R73 Resistor, 100 , 0.1 W, 1%, 0805 Multicomp MC 01W 0805 1 100K Farnell 9332405
R24, R67 Resistor, 22 Ω, 1% 0805 Vishay Draloric CRCW080522ROFKEAHP Farnell 1738936
R8, R9, R16, R18, R19,
R29, R30, R31, R32, R33,
R37, R38, R39, R40,
R41, R44, R54, R55,
R56, R59, R60, R61,
R62, R64, R65, R66,
R68
Not applicable Not applicable Not applicable Do not place
EVAL-AD7902SDZ User Guide UG-608
Rev. 0 | Page 31 of 32
RELATED LINKS
Resource
Description
AD7902 Product Page: Dual Pseudo Differential 16-Bit, 1 MSPS PulSAR ADC
ADA4841-1 Product Page: Unity Gain Stable, Low Noise and Distortion, Rail-to-Rail Output Amplifier
AD8031 Product Page: 2.7 V, 800 μA, 80 MHz Rail-to-Rail I/O Amplifiers
ADP7104 Product Page : 20 V, 300 mA/500 mA, Low Noise, CMOS LDO
ADP2301 Product Page: 1.2 A, 20 V, 1.4 MHz, Nonsynchronous Step-Down Regulator
ADR435 Product Page: Ultralow Noise, High Accuracy Voltage References
ANALOG DEVICES www.analuu.com
UG-608 EVAL-AD7902SDZ User Guide
Rev. 0 | Page 32 of 32
NOTES
ESD Caution
ESD (electrostatic discharge) sensitive device. Charged devices and circuit boards can discharge without detection. Although this product features patented or proprietary protection
circuitry, damage may occur on devices subjected to high energy ESD. Therefore, proper ESD precautions should be taken to avoid performance degradation or loss of functionality.
Legal Terms and Conditions
By using the evaluation board discussed herein (together with any tools, components documentation or support materials, the “Evaluation Board”), you are agreeing to be bound by the terms and conditions
set forth below (“Agreement”) unless you have purchased the Evaluation Board, in which case the Analog Devices Standard Terms and Conditions of Sale shall govern. Do not use the Evaluation Board until you
have read and agreed to the Agreement. Your use of the Evaluation Board shall signify your acceptance of the Agreement. This Agreement is made by and between you (“Customer”) and Analog Devices, Inc.
(“ADI”), with its principal place of business at One Technology Way, Norwood, MA 02062, USA. Subject to the terms and conditions of the Agreement, ADI hereby grants to Customer a free, limited, personal,
temporary, non-exclusive, non-sublicensable, non-transferable license to use the Evaluation Board FOR EVALUATION PURPOSES ONLY. Customer understands and agrees that the Evaluation Board is provided
for the sole and exclusive purpose referenced above, and agrees not to use the Evaluation Board for any other purpose. Furthermore, the lice
nse granted is expressly made subject to the following additional
limitations: Customer shall not (i) rent, lease, display, sell, transfer, assign, sublicense, or distribute the Evaluation Board; and (ii) permit any Third Party to access the Evaluation Board. As used herein, the term
“Third Party includes any entity other than ADI, Customer, their employees, affiliates and in-house consultants. The Evaluation Board is NOT sold to Customer; all rights not expressly granted herein, including
ownership of the Evaluation Board, are reserved by ADI. CONFIDENTIALITY. This Agreement and the Evaluation Board shall all be considered the confidential and proprietary information of ADI. Customer may
not disclose or transfer any portion of the Evaluation Board to any other party for any reason. Upon discontinuation of use of the Evaluation Board or termination of this Agreement, Customer agrees to
promptly return the Evaluation Board to ADI. ADDITIONAL RESTRICTIONS. Customer may not disassemble, decompile or reverse engi
neer chips on the Evaluation Board. Customer shall inform ADI of any
occurred damages or any modifications or alterations it makes to the Evaluation Board, including but not limited to soldering or any other activity that affects the material content of the Evaluation Board.
Modifications to the Evaluation Board must comply with applicable law, including but not limited to the RoHS D
irective. TERMINATION. ADI may terminate this Agreement at any time upon giving written notice
to Customer. Customer agrees to return to ADI the Evaluation Board at that time. LIMITATION OF LIABILITY. THE EVALUATION BOARD PROVIDED HEREUNDER IS PROVIDED AS IS” AND ADI MAKES NO
WARRANTIES OR REPRESENTATIONS OF ANY KIND WITH RESPECT TO IT. ADI SPECIFICALLY DISCLAIMS ANY REPRESENTATIONS, ENDORSEMENTS, GUARANTEES, OR WARRANTIES, EXPRESS OR IMPLIED, RELATED
TO THE EVALUATION BOARD INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTY OF MERCHANTABILITY, TITLE, FITNESS FOR A PARTICULAR PURPOSE OR NONINFRINGEMENT OF INTELLECTUAL
PROPERTY RIGHTS. IN NO EVENT WILL ADI AND ITS LICENSORS BE LIABLE FOR ANY INCIDENTAL, SPECIAL, INDIRECT, OR CONSEQUENTIAL DAMAGES RESULTING FROM CUSTOMER’S POSSESSION OR USE OF
THE EVALUATION BOARD, INCLUDING BUT NOT LIMITED TO LOST PROFITS, DELAY COSTS, LABOR COSTS OR LOSS OF GOODWILL. ADI’S TOTAL LIABILITY FROM ANY AND ALL CAUSES SHALL BE LIMITED TO THE
AMOUNT OF ONE HUNDRED US DOLLARS ($100.00). EXPORT. Customer agrees that it will not directly or indirectly export the Evaluation Board to another country, and that it will comply with all applicable
United States federal laws and regulations relating to exports. GOVERNING LAW. This Agreement shall be governed by and construed in accordance with the substantive laws of the Commonwealth of
Massachusetts (excluding conflict of law rules). Any legal action regarding this Agreement will be heard in the state or federal courts having jurisdiction in Suffolk County, Massachusetts, and Customer hereby
submits to the personal jurisdiction and venue of such courts. The United Nations Convention on Contracts for the International Sale of Goods shall not apply to this Agreement and is expressly disclaimed.
©2014 Analog Devices, Inc. All rights reserved. Trademarks and
registered trademarks are the property of their respective owners.
UG11798-0-2/14(0)