www.hancomm org
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
 
www.hancomm org
 
IB IL AI 2-HART (-PAC)
6758_en_01 PHOENIX CONTACT 16
The HART Telegram Structure
Key:
Structure of the AD Address for Long Addresses:
Long address (5 bytes)
Further information on the HART topic can be downloaded 
from the homepage of the HCF user organization (HART 
COMMUNICATION FOUNDATION) at www.hartcomm.org
The HART protocol can be implemented by any 
manufacturer and it can be freely used by any user. This 
open communication protocol between operating and field 
device is supported by the HART Communication 
Foundation (HCF). The HCF also provides technical 
support for the user. Among other things, the HCF monitors 
the openness of the protocol and manages device 
descriptions of all devices approved for operation.
.
HART and HCF logo
14.3 HART Operating Mode (Polling/Burst) for Point-
to-Point Connections and Multidrop Networks
Point-to-Point Connection (PTP)
For a point-to-point connection, connect a HART field 
device (slave) to the HART operating device (master). The 
master communicates with precisely one HART device via 
one pair of wires. For this reason, the device address "0" 
must be set for the HART field device (cf. Figure 5 and 
Figure 6 on page 10).
Multidrop Network
In a multidrop network, the HART operating device 
communicates with up to 5 HART field devices being 
connected in parallel to the master via an individual wire pair 
each (cf. Figure 7). The device address of each slave 
determines which slave is addressed by the master. This 
device address is to be preset according to the range from 
1 to 15. Please make sure
– NOT to set the device address "0" for slaves
– NOT to assign device addresses twice.
Burst Mode Operation
Burst mode operation is only possible for point-to-point 
connections. Here the slave is requested by the master to 
send a standard HART response telegram (burst telegram). 
This burst telegram is sent continuously by the HART slave 
until the master cancels the request. 
The command number of the response is variable and is 
transmitted via the CONTROL object. This command 
number is sent to the HART slave via command 108. After 
this, burst mode operation is enabled via command 109. 
The current response can be read via the POLL/
BURST_RESPONSE_CHANNEL_x_SLAVE_1 object.
In this operating mode a timeout is maintained:
If no response telegram is received within 800 ms, the 
object length is set to 0.
When sending the burst command number or the burst 
enter command, the first status byte of the response is 
checked. If the HART device responds negatively to 
commands 108 or 109, the response is made available in 
Preamble SC AD HC BC ST DA CS
x1 
byte
5 
bytes
1 
byte
1 
byte
2 
bytes xx xxx
Preamble: The preamble is used to synchronize the 
HART devices.
SC: Start byte
The start byte indicates the sender (master, 
slave, slave in burst mode) and whether a long 
or a short address is used.
AD: Address
Length: 5 bytes = long address
1 byte = short address
Via this address the two masters are 
distinguished, burst telegrams and field 
devices are identified.
HC: HART command
The HART command encodes the master's 
commands.
BC: Byte count = ST + DA
This byte indicates the number of transmitted 
status and data bytes.
ST: Status
The response message of a HART slave 
contains two status bytes. It indicates whether 
the data was received without errors (= 0) and 
the current field device status. 
DA: Data
The maximum data length is 26 bytes, 
depending on the HART command.
CS: Checksum of the entire telegram.
Master Burst Bit 31, 30, 29, ...0