Datenblatt für ADP165Z/166Z-REDYKIT Guide von Analog Devices Inc.

ANALOG DEVICES ANALOG. . DtVLLts: ' . AWN/4774mm W M voy HMO a, Ow: C1‘(2 W. _ ,, “.;.: (.mVD. O E” O ANALOG ’ . DEVICES '2 . ADPLES/Er—VEVALZ VIN 2m vow ’ © MEEEQEZQ HE EM - EN-GND-A .
ADP165Z-REDYKIT/ADP166Z-REDYKIT User Guide
UG-717
One Technology Way P. O. Box 9106 Norwood, MA 02062-9106, U.S.A. Tel: 781.329.4700 Fax: 781.461.3113 www.analog.com
Setting Up the Evaluation Boards for the ADP165/ADP166
PLEASE SEE THE LAST PAGE FOR AN IMPORTANT
WARNING AND LEGAL TERMS AND CONDITIONS. Rev. A | Page 1 of 9
FEATURES
Input voltage range: 2.2 V to 5.5 V
Output current range: 0 mA to 150 mA
Output voltage accuracy: ±1%
Operating temperature range: −40°C to +125°C
GENERAL DESCRIPTION
The ADP165/ADP166 evaluation boards are used to demonstrate
the functionality of the ADP165/ADP166 series of linear
regulators.
Simple device measurements such as line and load regulation,
dropout voltage, and ground current can be demonstrated with
only a single voltage supply, a voltmeter, an ammeter, and load
resistors.
Complete specifications for the ADP165/ADP166 linear regulators
are available in the ADP165/ADP166 data sheet available from
Analog Devices, Inc., and should be consulted in conjunction
with this user guide when using the evaluation boards.
ADP165/ADP166 EVALUATION BOARDS
Figure 1. TSOT Printed Circuit Board (PCB) Layout
Figure 2. WLCSP PCB Layout
Figure 3. LFCSP PCB Layout
12433-001
12433-002
12433-003
UG-717 ADP165Z-REDYKIT/ADP166Z-REDYKIT User Guide
TABLE OF CONTENTS
Features .............................................................................................. 1
General Description ......................................................................... 1
ADP165/ADP166 Evaluation Boards ............................................ 1
Revision History ............................................................................... 2
Evaluation Board Hardware ............................................................ 3
Evaluation Board Configurations .............................................. 3
Output Voltage Measurements ................................................... 4
Line Regulation Measurements .................................................. 5
Load Regulation Measurements ................................................. 5
Dropout Voltage Measurements..................................................5
Ground Current Measurements ..................................................6
Ground Current Consumption ...................................................7
Ordering Information .......................................................................8
Bill of Materials ..............................................................................8
ADP165Z-REDYKIT Contents ...................................................8
ADP166Z-REDYKIT Contents ...................................................9
REVISION HISTORY
2/15Rev. 0 to Rev. A
Changes to General Description Section ...................................... 1
Changes to Figure 8 .......................................................................... 4
Added ADP165Z-REDYKIT Contents Section and Table 3;
Renumbered Sequentially ................................................................ 8
Added ADP166Z-REDYKIT Contents Section and Table 4 ...... 9
9/14Revision 0: Initial Version
Rev. A | Page 2 of 9
ADP165Z-REDYKIT/ADP166Z-REDYKIT User Guide UG-717
Rev. A | Page 3 of 9
EVALUATION BOARD HARDWARE
EVALUATION BOARD CONFIGURATIONS
The ADP165/ADP166 evaluation boards come supplied with
different components, depending on the version ordered.
Components common to all versions are C1, C2, and J1.
Resistors R1 and R2 and Jumper J2 are used for the adjustable
output ADP165/ADP166, the 6-lead LFCSP and 5-lead TSOT
options. Figure 4, Figure 5, and Figure 6 show the schematics of
these evaluation board configurations. Table 1 describes the
components.
The adjustable ADP165/ADP166 has an output voltage range of
1.2 V to 4.2 V. The output voltage is set by the ratio of two external
resistors, as shown in Figure 4 and Figure 6. The device servos the
output to maintain the voltage at the ADJ pin at 1.0 V referenced
to ground. The current in R1 is then equal to 1.0 V/R2, and the
current in R1 is the current in R2 plus the ADJ pin bias current.
The ADJ pin bias current, 10 nA at 25°C, flows through R1 into
the ADJ pin.
Calculate the output voltage using the following equation:
VOUT = 1.0 V(1 + R1/R2) + (ADJI-BIAS)(R1)
The value of R1 must be less than 200 kΩ to minimize errors in
the output voltage caused by the ADJ pin bias current. For example,
when R1 and R2 each equal 200 kΩ, the output voltage is 2.0 V.
The output voltage error introduced by the ADJ pin bias current
is 1 mV or 0.05%.
To minimize quiescent current in the ADP165/ADP166, use
high values of resistance for R1 and R2. Using a value of 1 MΩ
for R2 keeps the total, no load quiescent current below 2 μA.
However, high values of resistance introduce a small output
voltage error. For example, assuming that R1 and R2 are 1,
the output voltage is 2 V. Taking into account the nominal
ADJ pin bias current of 10 nA, the output voltage error is 0.25%.
Note that when the device is in shutdown, the output turns off,
and the divider current is zero.
5
4
1
2
3
VIN
GND
EN
VOUT
NC/
ADJ
J2
J1 C2
C1
R1
R2
VOUT
U1
12433-004
Figure 4. Evaluation Board Schematic, TSOT
C2
J1
C1
VOUT
U1
VOUTVIN
GNDEN
VIN
12433-005
Figure 5. Evaluation Board Schematic, WLCSP
VIN
NC
EN
6
5
4
1
2
3
GND
VOUT
NC/
ADJ J2
J1
V
IN
C2
C
1
R1
R2
V
OUT
U1
12433-006
Figure 6. Evaluation Board Schematic, LFCSP
Table 1. Evaluation Board Hardware Components
Component Description
U1 ADP165/ADP166 low dropout linear regulator
C11 Input bypass capacitor, 1 μF, 0603 size
C21 Output capacitor, 1 μF, 0603 size
J1 Jumper (connects EN to VIN for automatic startup)
J2 Jumper (connects VOUT to the resistor divider
for the adjustable ADP165/ADP166)
R1, R2 Resistor divider to set ADP165/ADP166 output
voltage
1 The ADP165/ADP166 evaluation boards require only one input bypass
capacitor and one output capacitor for stable operation.
! \ r VUT /\ \g/ x ALOG: . ICES. AN DEV ,6, ADP165/ J Lg
UG-717 ADP165Z-REDYKIT/ADP166Z-REDYKIT User Guide
Rev. A | Page 4 of 9
OUTPUT VOLTAGE MEASUREMENTS
Figure 7. Output Voltage Measurement Setup, TSOT
Figure 8. Output Voltage Measurement Setup, WLCSP
Figure 7 and Figure 8 show how the evaluation board can be
connected to a voltage source and a voltmeter for basic output
voltage accuracy measurements. Note that the LFCSP
measurement setup is the same as the TSOT setup.
A resistor can be used as the load for the regulator. Ensure that
the resistor has a power rating that is adequate to handle the power
expected to dissipate across it. An electronic load can also be
used as an alternative. Ensure that the voltage source can supply
enough current for the expected load levels.
Follow these steps to connect the evaluation board to a voltage
source and voltmeter:
1. Connect the negative terminal (−) of the voltage source to
one of the GND pads on the evaluation board.
2. Connect the positive terminal (+) of the voltage source to
the VIN pad on the evaluation board.
3. Connect a load between the VOUT pad and one of the
GND pads on the evaluation board.
4. Connect the negative terminal (−) of the voltmeter to one
of the GND pads on the evaluation board.
5. Connect the positive terminal (+) of the voltmeter to the
VOUT pad on the evaluation board.
When these steps are completed, the voltage source can be turned
on. If J1 is inserted (connecting EN to VIN for automatic startup),
the regulator powers up.
If the load current is large, the user must connect the voltmeter
as close as possible to the output capacitor to reduce the effects
of IR drops.
+–
VOLTAGE
SOURCE
3.29999
+–
VOLTMETER
LOAD
12433-007
VOLTAGE
SOURCE
3.29999
+–
VOLTMETER
+–
LOAD
12433-008
ADP165Z-REDYKIT/ADP166Z-REDYKIT User Guide UG-717
LINE REGULATION MEASUREMENTS
For line regulation measurements, the output of the regulator
is monitored while its input is varied. For good line regulation,
the output must change as little as possible with varying input
levels. To ensure that the device is not in dropout mode during line
regulation measurement, VIN must be varied between VOUTNOM +
0.4 V (or 2.2 V, whichever is greater) and VINMAX. For example,
for an ADP165 with a fixed 3.3 V output, VIN must be varied
between 2.7 V and 5.5 V. This measurement can be repeated under
different load conditions. Figure 9 shows the typical line regulation
performance of an ADP165 with a fixed 3.3 V output.
Figure 9. Output Voltage (VOUT) vs. Input Voltage (VIN) at
VOUT = 3.3 V, TA = 25°C
LOAD REGULATION MEASUREMENTS
For load regulation measurements, the output of the regulator is
monitored while the load is varied. For good load regulation, the
output must change as little as possible with varying load. The input
voltage must be held constant during load regulation measurement.
The load current can be varied from 0 mA to 150 mA. Figure 10
shows the typical load regulation performance of an ADP165
with a fixed 3.3 V output for an input voltage of 3.8 V.
Figure 10. Output Voltage (VOUT) vs. Load Current (IOUT) at
VIN = 3.8 V, VOUT = 3.3 V, TA = 25°C
DROPOUT VOLTAGE MEASUREMENTS
The dropout voltage can be measured using the configurations
shown in Figure 7 and Figure 8. Dropout voltage is defined as
the input to output voltage differential when the input voltage is
set to the nominal output voltage. The ADP165/ADP166 only
enter dropout mode for output voltages higher than 2.2 V; for
lower voltage outputs, the ADP165/ADP166 shut down. The
dropout voltage increases with larger loads.
For accurate measurements, use a second voltmeter to monitor
the input voltage across the input capacitor. The input supply
voltage may need adjusting to account for IR drops, especially
when using large load currents. Figure 11 shows the typical curve
of dropout voltage measurements with different load currents.
Figure 11. Dropout Voltage vs. Load Currents (ILOAD),
VOUT = 2.0 V and 3.3 V, TA = 25°C
3.33
3.23
3.24
3.25
3.26
3.27
3.28
3.29
3.30
3.31
3.32
3.7 3.9 4.1 4.3 4.5 4.7 4.9 5.1 5.55.3
V
OUT
(V)
VIN (V)
1µA
100µA
1mA
10mA
100mA
150mA
12433-009
3.35
3.25
3.26
3.27
3.28
3.29
3.30
3.31
3.32
3.33
3.34
0.001 0.01 10001001010.1
V
OUT
(V)
ILOAD (mA)
12433-010
0.27
0.24
0.21
0.18
0.15
0.12
0.09
0.06
0.03
0
0.001 10.10.01
DRO
POUT VOLTAGE (V)
I
L
OAD
(A)
V
OUT
= 2.0V
V
OUT
= 3.3V
12433-011
Rev. A | Page 5 of 9
VEVALZ ANALOG DEVICES= ° ADPlfiE/ér 33)) VOOOA (CC:
UG-717 ADP165Z-REDYKIT/ADP166Z-REDYKIT User Guide
Rev. A | Page 6 of 9
GROUND CURRENT MEASUREMENTS
Figure 12. Ground Current Measurement Setup, TSOT
Figure 13. Ground Current Measurement Setup, WLCSP
Figure 12 and Figure 13 show how the evaluation board can be
connected to a voltage source and an ammeter for ground
current measurements. Note that the LFCSP measurement
setup is the same as the TSOT setup
A resistor can be used as the load for the regulator. Ensure that
the resistor has a power rating that is adequate to handle the
power expected to be dissipated across it. An electronic load
can be used as an alternative. Ensure that the voltage source can
supply enough current for the expected load levels.
Follow these steps to connect the evaluation board to a voltage
source and ammeter:
1. Connect the positive terminal (+) of the voltage source to
the VIN pad on the evaluation board.
2. Connect the positive terminal (+) of the ammeter to one of
the GND pads on the evaluation board.
3. Connect the negative terminal (−) of the ammeter to the
negative terminal (−) of the voltage source.
4. Connect a load between the VOUT pad on the evaluation
board and the negative terminal (−) of the voltage source.
When these connection steps are completed, the voltage source
can be turned on. If J1 is inserted (connecting EN to VIN for
automatic startup), the regulator powers up.
+
VOLTAGE
SOURCE
0.00112
+
AMMETER
LOAD
12433-012
+
VOLTAGE
SOURCE
0.00112
+
AMMETER
LOAD
12433-013
ADP165Z-REDYKIT/ADP166Z-REDYKIT User Guide UG-717
GROUND CURRENT CONSUMPTION
Ground current measurements can determine how much
current the internal circuits of the regulator consume while the
circuits perform the regulation function. To be efficient, the
regulator must consume as little current as possible. Typically,
the regulator uses the maximum current when supplying its
largest load level (150 mA). Figure 14 shows the typical ground
current consumption for various load levels at VOUT = 3.3 V and
TA = 25°C.
When the device is disabled (EN = GND), the ground current
drops to less than 50 nA.
Figure 14. Ground Current vs. Input Voltage (VIN),
VOUT = 3.3 V, TA = 25°C
100
0.1
1
10
–50–250255075100125150
GROUND CURRENT (µA)
JUNCTION TEMPERATURE(°C)
NO LOAD
1µA
100µA
1mA
10mA
100mA
150mA
12433-014
Rev. A | Page 7 of 9
Table 3‘
UG-717 ADP165Z-REDYKIT/ADP166Z-REDYKIT User Guide
ORDERING INFORMATION
BILL OF MATERIALS
Table 2.
Reference Designator Description Manufacturer Part No.
C1, C2 Capacitor, MLCC, 1 µF, 16 V, 0603, X5R Murata (or equivalent) GRM188R61C105KA93
J1, J2 Header, single, STR, two pins Sullins Connector Solutions PEC02SAAN
U1 IC, low dropout (LDO) regulator Analog Devices, Inc. ADP165/ADP166
R1, R2 Resistor, 0402, 1% tolerance Any manufacturer Depends on manufacturer
ADP165Z-REDYKIT CONTENTS
Table 3.
Quantity Model Output Voltage (V) Maximum Current (mA) Description
1 ADP165CB-EVALZ 1.8 150 Evaluation board
1
ADP165CP-EVALZ
2.3
Evaluation board
1 ADP165UJ-EVALZ 3.3 150 Evaluation board
1 ADP165ACPZN-R7 Adjustable 150 6-lead LFCSP
1 ADP165ACPZN-1.2-R7 1.2 150 6-lead LFCSP
1 ADP165ACPZN-1.8-R7 1.8 150 6-lead LFCSP
1 ADP165ACPZN-3.0-R7 3.0 150 6-lead LFCSP
1 ADP165ACPZN-3.3-R7 3.3 150 6-lead LFCSP
1 ADP165AUJZ-R7 Adjustable 150 5-lead TSOT
1 ADP165AUJZ-1.2-R7 1.2 150 5-lead TSOT
1 ADP165AUJZ-1.8-R7 1.8 150 5-lead TSOT
1 ADP165AUJZ-2.3-R7 2.3 150 5-lead TSOT
1 ADP165AUJZ-3.0-R7 3.0 150 5-lead TSOT
Rev. A | Page 8 of 9
ANALOG DEVICES www.analug.com
ADP165Z-REDYKIT/ADP166Z-REDYKIT User Guide UG-717
ADP166Z-REDYKIT CONTENTS
Table 4.
Quantity Model Output Voltage (V) Maximum Current (mA) Description
1
ADP166CB-EVALZ
1.8
150
Evaluation board
1 ADP166CP-EVALZ 2.3 150 Evaluation board
1 ADP166UJ-EVALZ 3.3 150 Evaluation board
1 ADP166ACPZN-R7 Adjustable 150 6-lead LFCSP
1 ADP166ACPZN-1.2-R7 1.2 150 6-lead LFCSP
1 ADP166ACPZN-1.8-R7 1.8 150 6-lead LFCSP
1 ADP166ACPZN-3.0-R7 3.0 150 6-lead LFCSP
1 ADP166ACPZN-3.3-R7 3.3 150 6-lead LFCSP
1 ADP166AUJZ-R7 Adjustable 150 5-lead TSOT
1 ADP166AUJZ-1.2-R7 1.2 150 5-lead TSOT
1 ADP166AUJZ-1.8-R7 1.8 150 5-lead TSOT
1 ADP166AUJZ-2.3-R7 2.3 150 5-lead TSOT
1 ADP166AUJZ-3.0-R7 3.0 150 5-lead TSOT
ESD Caution
ESD (electrostatic discharge) sensitive device. Charged devices and circuit boards can discharge without detection. Although this product features patented or proprietary protection circuitry,
damage may occur on devices subjected to high energy ESD. Therefore, proper ESD precautions should be taken to avoid performance degradation or loss of functionality.
Legal Terms and Conditions
By using the evaluation board discussed herein (together with any tools, components documentation or support materials, the “Evaluation Board”), you are agreeing to be bound by the terms and conditions
set forth below (“Agreement”) unless you have purchased the Evaluation Board, in which case the Analog Devices Standard Terms and Conditions of Sale shall govern. Do not use the Evaluation Board until you
have read and agreed to the Agreement. Your use of the Evaluation Board shall signify your acceptance of the Agreement. This Agreement is made by and between you (“Customer”) and Analog Devices, Inc.
(“ADI”), with its principal place of business at One Technology Way, Norwood, MA 02062, USA. Subject to the terms and conditi
ons of the Agreement, ADI hereby grants to Customer a free, limited, personal,
temporary, non-exclusive, non-sublicensable, non-transferable license to use the Evaluation Board FOR EVALUATION PURPOSES ONLY. Customer understands and agrees that the Evaluation Board is provided
for the sole and exclusive purpose referenced above, and agrees not to use the E
valuation Board for any other purpose. Furthermore, the license granted is expressly made subject to the following additional
limitations: Customer shall not (i) rent, lease, display, sell, transfer, assign, sublicense, or distribute the Evaluation Board; and (ii) permit any Third Party to access the Evaluation Board. As used herein, the term
“Third Party” includes any entity other than ADI, Customer, their employees, affiliates and in-house consultants. The Evaluation Board is NOT sold to Customer; all rights not expressly granted herein, including
ownership of the Evaluation Board, are reserved by ADI. CONFIDENTIALITY. This Agreement and the Evaluation Board shall all be considered the confidential and proprietary information of ADI. Customer may
not disclose or transfer any portion of the Evaluation Board to any other party for any reason. Upon discontinuation of use of the Evaluation Board or termination of this Agreement, Customer agrees to
promptly return the Evaluation Board to ADI. ADDITIONAL RESTRICTIONS. Customer may not disassemble, decompile or reverse engineer chips on the Evaluation Board. Customer shall inform ADI of any
occurred damages or any modifications or alterations it makes to the Evaluation Board, including but not limited to soldering or any other activity that affects the material content of the Evaluation Board.
Modifications to the Evaluation Board must comply with applicable law, including but not limited to the RoHS Directive. TERMINATION. ADI may terminate this Agreement at any time upon giving written notice
to Customer. Customer agrees to return to ADI the Evaluation Board at that time. LIMITATION OF LIABILITY. THE EVALUATION BOARD PROVIDED HEREUNDER IS PROVIDED AS IS” AND ADI MAKES NO
WARRANTIES OR REPRESENTATIONS OF ANY KIND WITH RESPECT TO IT. ADI SPECIFICALLY DISCLAIMS ANY REPRESENTATIONS, ENDORSEMENTS, GUARANTEES, OR WARRANTIES, EXPRESS OR IMPLIED, RELATED
TO THE EVALUATION BOARD INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTY OF MERCHANTABILITY, TITLE, FITNESS FOR A PARTICULAR PURPOSE OR NONINFRINGEMENT OF INTELLECTUAL
PROPERTY RIGHTS. IN NO EVENT WILL ADI AND ITS LICENSORS BE LIABLE FOR ANY INCIDENTAL, SPECIAL, INDIRECT, OR CONSEQUENTIAL DAMAGES RESULTING FROM CUSTOMER’S POSSESSION OR USE OF
THE EVALUATION BOARD, INCLUDING BUT NOT LIMITED TO LOST PROFITS, DELAY COSTS, LABOR COSTS OR LOSS OF GOODWILL. ADI’S TOTAL LIABILITY FROM ANY AND ALL CAUSES SHALL BE LIMITED TO THE
AMOUNT OF ONE HUNDRED US DOLLARS ($100.00). EXPORT. Customer agrees that it will not directly or indirectly export the Evaluation Board to another country, and that it will comply with all applicable
United States federal laws and regulations relating to exports. GOVERNING LAW. This Agreement shall be governed by and construed in accordance with the substantive laws of the Commonwealth of
Massachusetts (excluding conflict of law rules). Any legal action regarding this Agreement will be heard in the state or federal courts having jurisdiction in Suffolk County, Massachusetts, and Customer hereby
submits to the personal jurisdiction and venue of such courts. The United Nations Convention on Contracts for the International Sale of Goods shall not apply to this Agreement and is expressly disclaimed.
©20142015 Analog Devices, Inc. All rights reserved. Trademarks and
registered trademarks are the property of their respective owners.
UG12433-0-2/15(A)
Rev. A | Page 9 of 9