Datenblatt für GEN4-IB von 4D Systems Pty Ltd

4 D SYSTE MS
Uncontrolled Copy when printed or downloaded.
Please refer to the 4D Systems website for the latest Revision of this document
www.4dsystems.com.au
DATASHEET
gen4 Interface Board
For all gen4 sizes (Picaso and Diablo16), and pixxiLCD
gen4-IB
Document Date: 14th December 2020
Document Revision: 1.2
gen4—IB gen4 Interface Board mincum I Emom NumtuhE UCNQ
gen4 Interface Board gen4-IB
© 2020 4D SYSTEMS Page 2 of 8 www.4dsystems.com.au
Contents
Description ...................................................................................................................3
Example Hardware Connections ....................................................................................4
Schematic Diagram .......................................................................................................6
Mechanical Drawing .....................................................................................................7
Legal Notice ..................................................................................................................8
Contact Information .....................................................................................................8
gen4 Interface Bnard genll—IE www unsgstems com au ‘Sv m llfllll EII EEJEZI ll :n E u m D =r I: m Dy )7 m :l g “I. C GI 01 I 'D h [D O a: GI U [U "c E E i m on www.4dsysiems.com.au The Slandard FFC cable supplied has the following specificalions:
gen4 Interface Board gen4-IB
© 2020 4D SYSTEMS Page 3 of 8 www.4dsystems.com.au
Description
This datasheet covers the gen4-IB (Interface board) which is compatible with all of the gen4 range of
Intelligent Display modules which feature Picaso or Diablo16 graphics processors, along with the pixxiLCD
range of display modules too. It is included with every display module, and is a quick and easy way to
interface to the gen4 range, without having to break out the signals from the 30-way FFC cable.
The gen4-IB is a simple interface that converts the 30-way FFC cable coming from your gen4 display module,
into the common 5 signals used for programming and interfacing to 4D Systems products. The remaining
signals from the display module are not accessible through this interface board. Please refer to the gen4-
PA (Programming Adaptor) or UPA (Universal Programming Adaptor) which are USB programmers for the
display modules, and also breaks out all of the signals from the display.
If you have existing 4D Products and have a uUSB-PA5 or uUSB-PA5-II, or even a 4D Programming Cable,
then you can use these programming devices via the gen4-IB to program the display modules directly,
without the need of a gen4-PA board.
The gen4-IB can be used to interface with 4D Programming devices, as mentioned above, for interfacing to
a breadboard for prototyping, interfacing to Arduino and Raspberry Pi interfaces (see gen4 -AR and -PI kits),
or for interfacing to virtually any host.
The gen4-IB has no processor, requires no drivers or any software. It is a simple interface only, converting
the signals from the 30-way FFC cable from the display module, and breaking out the 5 important signals
required for programming and basic interfacing.
More information can be found inside the datasheet for the specific display module being used. Please
refer to the 4D Systems website and the product page of your chosen product, for more information.
www.4dsystems.com.au
The Standard FFC cable supplied has the following specifications:
30 Pin Flexible Flat Cable, 150mm Long, 0.5mm (0.02") pitch
Cable Type: AWM 20624 80C 60V VW-1
Heat Resistance 80 Degrees Celsius
Connections on the opposite side at each end (Type B)
gen4 Interface Bnard genll—IE g “I. C GI 01 I 'D h [D O a: GI U [U "c E E i m on
gen4 Interface Board gen4-IB
© 2020 4D SYSTEMS Page 4 of 8 www.4dsystems.com.au
Example Hardware Connections
The following pictures illustrate how to connect the parts of a gen4 display module together, specifically
utilising the gen4-IB. Note, the display module illustrated below is the gen4-uLCD-32DT.
Figure 1. Typical components that come with a gen4 display.
Figure 2. gen4 display connected to a breadboard via a gen4-IB and 5-way cable
Figure 3. Components in the AR Kit connected together. The gen4-IB interfaces to the gen4 display module, and
to the Arduino Adaptor Shield via our 5-way cable.
gen44E gen4 Interface Bnard m=u_ucum I Emom NumtuhE
gen4 Interface Board gen4-IB
© 2020 4D SYSTEMS Page 5 of 8 www.4dsystems.com.au
Figure 4. gen4 display, connected to the gen4-IB, with the uUSB-PA5 programming adaptor connected directly.
Figure 5. PixxiLCD connection, please refer to the pixxiLCD Getting Started Manual for more information
gen4 Interface Board genll—IE g “I. C GI 01 I 'D h [D O a: GI U [U "c E E i m on www.4dsystems.com.au [suggon salesQadsystemsLomau www.4dsyslems.com.au
gen4 Interface Board gen4-IB
© 2020 4D SYSTEMS Page 8 of 8 www.4dsystems.com.au
Legal Notice
Proprietary Information
The information contained in this document is the property of 4D Systems Pty. Ltd. and may be the subject of patents
pending or granted, and must not be copied or disclosed without prior written permission.
4D Systems endeavours to ensure that the information in this document is correct and fairly stated but does not
accept liability for any error or omission. The development of 4D Systems products and services is continuous and
published information may not be up to date. It is important to check the current position with 4D Systems. 4D
Systems reserves the right to modify, update or makes changes to Specifications or written material without prior
notice at any time.
All trademarks belong to their respective owners and are recognised and acknowledged.
Disclaimer of Warranties & Limitation of Liability
4D Systems makes no warranty, either expressed or implied with respect to any product, and specifically disclaims all
other warranties, including, without limitation, warranties for merchantability, non-infringement and fitness for any
particular purpose.
Information contained in this publication regarding device applications and the like is provided only for your
convenience and may be superseded by updates. It is your responsibility to ensure that your application meets with
your specifications.
Images and graphics used throughout this document are for illustrative purposes only. All images and graphics used
are possible to be displayed on the 4D Systems range of products, however the quality may vary.
In no event shall 4D Systems be liable to the buyer or to any third party for any indirect, incidental, special,
consequential, punitive or exemplary damages (including without limitation lost profits, lost savings, or loss of
business opportunity) arising out of or relating to any product or service provided or to be provided by 4D Systems,
or the use or inability to use the same, even if 4D Systems has been advised of the possibility of such damages.
4D Systems products are not fault tolerant nor designed, manufactured or intended for use or resale as on line control
equipment in hazardous environments requiring fail safe performance, such as in the operation of nuclear facilities,
aircraft navigation or communication systems, air traffic control, direct life support machines or weapons systems in
which the failure of the product could lead directly to death, personal injury or severe physical or environmental
damage (‘High Risk Activities’). 4D Systems and its suppliers specifically disclaim any expressed or implied warranty
of fitness for High Risk Activities.
Use of 4D Systems’ products and devices in 'High Risk Activities' and in any other application is entirely at the buyer’s
risk, and the buyer agrees to defend, indemnify and hold harmless 4D Systems from any and all damages, claims, suits,
or expenses resulting from such use. No licenses are conveyed, implicitly or otherwise, under any 4D Systems
intellectual property rights.
Contact Information
For Technical Support: www.4dsystems.com.au/support
For Sales Support: sales@4dsystems.com.au
Website: www.4dsystems.com.au
Copyright 4D Systems Pty. Ltd. 2000-2020.