Set LF In RUN mode, when DS2-4 is ON, sets the frequency of the supplemental low pass filter between
0.1 Hz and 10 Hz.
Ver In RUN mode, returns the version number of the unit's firmware to determine whether certain
commands will work.
Z In CAL mode, sets the module's zero output point at the minimum position of the LVDT's core; function
is the same as pressing the ZERO pushbutton. Occasionally it may require setting a second time after
using the FS command.
Endpoint Recalibration Process
In certain circumstances, it may be desirable to perform a "hot" recalibration on a module. Typically this
need arises from the effects of thermal expansion and/or contraction on a mechanical system when the
initial calibration was done at room temperature, but the workpiece and its LVDTs are now operating at
elevated temperature and the normal calibration process cannot be repeated under these new conditions.
Anticipating this problem, a recalibration feature has been incorporated into any S1A module with firmware
version 2.0 or higher. A pair of RS-485 commands, Recal FS and Recal Z, permit trimming of either end
point's analog output in a system that has already been calibrated, provided that the actual output values
from the module are within ±5% of the full span of the output chosen by the setting of DS-1. Recalibration
can be used to trim either end point's analog output independent of the other and is done while the module
is operational. As a result, these commands have immediate effect upon the system's analog output.
Before attempting a recalibration on a module, establish RS-485 communications with the module from a
terminal as noted on page 12. Then invoke the Ver command to find out if the module is running firmware
version 2.0 or higher. If it is not, the recalibration feature is not available.
If Ver shows the recalibration feature is available, before proceeding to perform a recalibration, verify that
the difference between the actual output of the end point to be trimmed is within ±5% of the span of the
analog output for which the module was set, where the span is the difference between the maximum and
minimum values of the selected analog output. Thus, the trimmable range of actual output at the system's
Zero point is -5 to 5% of the span, and at the Full Scale point, it is 95 to 105% of the span. If the actual
analog output of an end point is not within the limits noted, the attempt at recalibration will not be effective.
Either of the Recal commands may need to be repeated one time to get the most precise recalibration.
Hot Swapping Modules
Under the right conditions, an S1A module connected in a multi-module array can be "hot swapped" with
another module having the same internal DIP switch settings and loaded with values in certain EEPROM
locations that match those in the original module. This process will take the selected module off-line, but if
done carefully, will allow the remaining modules in the array to continue operating normally.
To prepare the replacement module for a hot swap, the configuration data of the original module, which
should have been obtained previously and saved for a possible hot swap, is needed. If this data is not
available, connect to the RS-485 port of the original module with a PC and terminal program, and use the
Config command to get it. Using that data, set the internal DIP switches and jumpers of the new module
to match, then power it up and use its RS-485 port as noted above to load the values of ADC HI, ADC Lo,
In Pot, Gain, and, if needed, FOP, FD, and LF using the Set command for each value.
To do the hot swap, the first remove the positive power line for the original module connected to J4-4, the
red plug. This may be done by loosening the screw terminal of J4-4 and carefully removing the wire, or by
pulling the power fuse, or by tripping a circuit breaker, or switching it off the power switch for that module.
Do not remove the red plug with any power present. Once the unit has been depowered, the plugs may be
disconnected from the original module in order of J4 (red), J3 (green), J2 (blue), then J1 (black). The
sequence for plugging back into the replacement module is J1 (black), J2 (blue), J3 (green), and last, J4,
the red plug with no power positive connected. Finally, reconnect positive power to J4-4.