Datenblatt für BGM111 Bluetooth Radio Brd User Guide von Silicon Labs

SILICEIN LABS
UG122: BGM111 Bluetooth Module Radio
Board User's Guide
A Silicon Labs Wireless Starter Kit for the BGM111 Blue Gecko
Bluetooth® Module is an excellent starting point to get familiar with
the device, and it provides all necessary tools for developing a Sili-
con Labs wireless application.
The Wireless Starter Kit Mainboard contains sensors and peripherals enabling easy
demonstration of some of the BGM111's many capabilities. An on-board J-Link debugger
allows debugging of the attached radio board as well as providing a debug connection
for external hardware.
A plug-in Radio Board contains the reference design for the BGM111 itself, including the
RF section and device-specific hardware.
WSTK MAINBOARD FEATURES
Ethernet and USB connectivity
SEGGER J-Link on-board debugger
Supports debugging the attached radio
board or an external device
Silicon Labs' Si7021 Relative Humidity and
Temperature sensor
Ultra low power 128x128 pixel Memory
LCD
User LEDs / Pushbuttons
20-pin 2.54 mm header for expansion
boards
Breakout pads for direct access to radio
board I/O pins
Power sources include USB and CR2032
coin cell.
BRD4300A RADIO BOARD FEATURES
BGM111 Blue Gecko Bluetooth Module
with 256 kB Flash and 32 kB RAM, with
integrated chip antenna, RF matching
network, crystals and decoupling.
EXTENSION BOARD FEATURES
• Accelerometer
Buttons and LEDs
• Joystick
EXPANSION BOARD FEATURES
• Accelerometer
Buttons and LEDs
• Joystick
SOFTWARE SUPPORT
Blue Gecko Bluetooth Software
Blue Gecko Bluetooth SDK
Simplicity Studio
iOS and Android applications
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00
1. Introduction
The BGM111 Blue Gecko Bluetooth Module itself is featured on a Radio Board that forms a complete reference design, inluding the RF
section and other components.
The BGM111 Radio Board plugs directly into a Wireless Starter Kit Mainboard. The WSTK Mainboard features several tools for easy
evaluation and development of wireless applications. An on-board J-Link debugger enables programming and debugging on the target
device over USB or Ethernet. The Advanced Energy Monitor (AEM) offers real-time current and voltage monitoring. A virtual COM port
interface (VCOM) provides an easy-to-use serial port connection over USB or Ethernet. The Packet Trace Interface (PTI) offers invalua-
ble debug information about transmitted and received packets in wireless links.
All debug functionality, including AEM, VCOM and PTI, can also be used towards external target hardware instead of the attached radio
board.
To further enhance its usability, the WSTK Mainboard contains sensors and peripherals demonstrating some of the BGM111's many
capabilities.
The Wireless Starter Kit for BGM111 includes an add-on board (BRD8006A) that can be connected to the WSTK Mainboard expansion
header. The expansion board contains additional peripherals such as an accelerometer, buttons, LEDs, joystick and a footprint for an
I2C authentication device.
1.1 Radio Boards
A Wireless Starter Kit consists of one or more mainboards and radio boards that plug into the mainboard. Different radio boards are
available. Each featuring different Silicon Labs devices with different operating frequency bands.
Since the mainboard is designed to work with all different radio boards, the actual pin mapping from a device pin to a mainboard feature
is done on the radio board. This means that each radio board has its own pin mapping to the Wireless Starter Kit features such as
buttons, LEDs, the display, the EXP header and the breakout pads. Because this pin mapping is different for every radio board, it is
important that the correct document be consulted which shows the kit features in context of the radio board plugged in.
This document explains how to use the Wireless Starter Kit (Wireless STK) when the BGM111 Bluetooth Module Radio Board
(BRD4300A) is combined with a Wireless STK Mainboard. The combination of these two boards is hereby referred to as a Wireless
Starter Kit (Wireless STK).
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Introduction
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 1
1.2 Ordering Information
BRD4300A can be obtained as part of SLWSTK6101C Blue Gecko Module Wireless Starter Kit or as a separate radio board,
SLWRB4300A.
Table 1.1. Ordering Information
Part Number Description Contents Notes
SLWSTK6101A Blue Gecko Module Wireless Start-
er Kit
1x BRD4001A Wireless Starter Kit Mainboard
1x BRD4300A BGM111 Bluetooth Module Radio Board
1x BRD8006A Blue Gecko Module Kit Add-on Board
1x CR2032 Lithium battery
1x USB Type A <-> USB Mini-B cable
Obsoleted
SLWSTK6101B Blue Gecko Module Wireless Start-
er Kit
1x BRD4001A Wireless Starter Kit Mainboard
1x BRD4300A BGM111 Bluetooth Module Radio Board
1x BRD4300B BGM113 Bluetooth Module Radio Board
1x BRD8006A Blue Gecko Module Kit Add-on Board
1x CR2032 Lithium battery
1x USB Type A <-> USB Mini-B cable
Obsoleted
SLWSTK6101C Blue Gecko Module Wireless Start-
er Kit
1x BRD4001A Wireless Starter Kit Mainboard
1x BRD4300A BGM111 Bluetooth Module Radio Board
1x BRD4302A BGM121 Bluetooth System-in-Package Radio Board
1x BRD8006A Blue Gecko Module Kit Add-on Board
1x CR2032 Lithium battery
1x USB Type A <-> USB Mini-B cable
SLWRB4300A BGM111 Bluetooth Module Radio
Board
1x BRD4300A BGM111 Bluetooth Module Radio Board
1.3 Getting Started
Detailed instructions for how to get started can be found on the Silicon Labs web pages:
http://www.silabs.com/bluetooth-getstarted
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Introduction
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 2
Advanced Energy Mannming \ . . . muesczku __ N g. t n sILItuu LABS u mplicity Connector
2. Kit Hardware Overview
The layout of the BGM111 Bluetooth Module Wireless Starter Kit is shown in the figure below.
BGM111
Module
Radio Board
Breakout pads
Breakout pads
1.28" Memory-LCD Display
Ultra-low power
128 x 128 pixel resolution
SPI interface
Ethernet RJ-45
J-Link Debugger
Virtual COM port
Packet Trace
Advanced Energy Monitoring
USB mini-B
J-Link Debugger
Virtual COM port
Packet Trace
Advanced Energy Monitoring
Coin Cell Holder
CR2032 Battery
Power Select Switch
BAT / USB / AEM
2x User Push Buttons 2x User LEDs
Simplicity Connector
External targets:
Virtual COM port
Packet Trace
Advanced Energy Monitoring
Debug Connector
ARM Coresight 19-pin
OUT: External targets
IN: External debug probes
Reset Button
Si7021
Relative Temperature &
Humidity Sensor
EXP Header
Expansion board connector
Expansion Board
3-axis Accelerometer
2x Push Buttons
2x LEDs
Analog Joystick
I2C device footprint
Figure 2.1. Kit Hardware Overview
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Kit Hardware Overview
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 3
w TKM nbua mm '3: at race lEliiTiI EH [EC] User BLmons Ben/I111 Bluetooth Module & LED:
3. Kit Block Diagram
An overview of the BGM111 Bluetooth Module Wireless Starter Kit is shown in the figure below.
WSTK Mainboard
USB Mini-B
Connector
RJ-45 Ethernet
Connector
Debug
UART
Packet Trace
AEM
Debug
UART
ETM Trace
Packet Trace
AEM
Debug
UART
Packet Trace
AEM
Simplicity
Connector
Debug
Connector
Board
Controller
Multiplexer
OUT
IN
MCU
BGM111
Bluetooth Module
128 x 128 pixel
Memory LCD
I2C
Si7021
Temperature
& Humidity
Sensor
GPIO
EXP
Header
User Buttons
& LEDs
GPIO
Expansion Board Peripherals
Footprint for
I2C Expansion
BGM111
I2C
Accelerometer
BMA280
SPI
Buttons
&
LEDs
GPIO
Analog
Joystick
ADC input
Figure 3.1. Kit Block Diagram
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Kit Block Diagram
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 4
“BM/ coco.“ _ o o D D ' ' ' lnlOul Debut SlmP'm'W Header A " Connector :.\ a an on as 00 on on no 00 no no on on be 00 no so on on an on an no
4. Connectors
This chapter gives you an overview of the Wireless STK Mainboard connectivity. The placement of the connectors can be seen in the
figure below.
Simplicity
Connector
In/Out Debug
Header
GND
GND
5V
5V
P25
P24
P27
P26
P29
P28
P31
P30
P33
P32
P35
P34
P37
P36
P39
P38
P41
P40
P43
P42
P45
P44
GND
GND
NC
NC
Radio Board
Connectors
Expansion
Header
GND
GND
VMCU
VMCU
P1
P0
P3
P2
P5
P4
P7
P6
P9
P8
P11
P10
P13
P12
P15
P14
P17
P16
P19
P18
P21
P20
GND
GND
P23
P22
VRF
VRF
3V3
3V3
Figure 4.1. Mainboard Connector Layout
4.1 Breakout Pads
Most of the BGM111's pins are routed from the radio board to breakout pads at the top and bottom edges of the Wireless STK Main-
board. A 2.54 mm pitch pin header can be soldered on for easy access to the pins. The figure below shows you how the pins of the
BGM111 maps to the pin numbers printed on the breakout pads. To see the available functions on each, please refer to the BGM111
Data Sheet.
GND
VMCU
P23 / PD15 / DISP_ENABLE
P21 / PD14 / DISP_SCS
P19 / PD13 / DISP_EXTCOMIN
P17 / NC
GND
P15 / NC
P13 / PC10 / I2C_SDA
P11 / PA1 / VCOM_RX
P9 / PA0 / VCOM_TX
P7 / PC9
P5 / PC8 / DISP_SCLK
P3 / PC7
P1 / PC6 / DISP_SI
GNDGND
5V5V
NCNC
P45 / NCNC / P44
P43 / NCNC / P42
P41 / NCNC / P40
3V33V3
P39 / NCNC / P38
P37 / tied high / SENSOR_ENABLENC / P36
P35 / NCNC / P34
P33 / PF7 / BTN1_LED1NC / P32
P31 / PF6 / BTN0_LED0NC / P30
P29 / PF2 / DBG_TDO_SWONC / P28
P27 / PF1 / DBG_TMS_SWDIONC / P26
P25 / PF0 / DBG_TCK_SWCLKNC / P24
GNDGND
VRF
GND
VMCU
PTI_FRAME / PB13 / P22
VCOM_ENABLE / PA5 / P20
PTI_DATA / PA4 / P18
NC / P16
GND
NC / P14
I2C_SCL / PC11 / P12
DBG_TDI / PF3 / P10
PTI_CLK / PB11 / P8
PF5 / P6
PF4 / P4
VCOM_RTS / PA3 / P2
VCOM_CTS / PA2 / P0
VRF
J101 J102
Figure 4.2. Radio Board Pin Mapping on Breakout Pads
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Connectors
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 5
I I Power I Ground I 20 19 18 : : 17 16 _ _ 15 14 13 12 ' ' 11 74. 14 =1? . . 6 5 A ' ' a 2 ' ' 1 . .
4.2 Expansion Header
On the right hand side of the board an angled 20-pin expansion header is provided to allow connection of peripherals or plugin boards.
The connector contains a number of I/O pins that can be used with most of the BGM111 Blue Gecko's features. Additionally, the VMCU,
3V3 and 5V power rails are also exported.
The connector follows a standard which ensures that commonly used peripherals such as an SPI, a UART and an I2C bus are available
on fixed locations in the connector. The rest of the pins are used for general purpose IO. This allows the definition of expansion boards
that can plug into a number of different Silicon Labs starter kits.
The figure below shows the pin assignment of the expansion header for the BGM111 Wireless Starter Kit. Because of limitations in the
number of available GPIO pins, some of the expansion header pins are shared with kit features.
12
4
8
6
10
3
5
9
7
12
13
14
11
1516
17
18
20 19
VMCU
SPI_MOSI / PC6
SPI_MISO / PC7
SPI_SCK / PC8
SPI_CS / PC9
UART_TX / PA0
UART_RX / PA1
I2C_SDA / PC10
5V
3V3
GND
PA2 / UART_CTS
PA3 / UART_RTS
PF4 / GPIO
PF5 / GPIO
PB11 / GPIO (PTI_CLK)
PF3 / GPIO (DBG_TDI)
PC11 / I2C_SCL
Board ID SDA
Board ID SCL
Reserved (Board Identification)
BGM111 I/O Pin
Figure 4.3. Expansion Header
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Connectors
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 6
4.2.1 Expansion Header Pin-out
The pin-routing on the BGM111 is very flexible, so most peripherals can be routed to any pin. However, many pins are shared between
the Expansion Header and other functions on the Wireless STK Mainboard. Table 4.1 Expansion Header Pinout on page 7 includes
an overview of the mainboard features that share pins with the Expansion Header.
Table 4.1. Expansion Header Pinout
Pin Connection EXP Header function Shared feature Peripheral mapping
20 3V3 Board controller supply
18 5V Board USB voltage
16 PC10 I2C_SDA SENSOR_I2C_SDA I2C0_SDA #15
14 PA1 UART_RX VCOM_RX USART0_RX #0
12 PA0 UART_TX VCOM_TX USART0_TX #0
10 PC9 SPI_CS USART1_CS #11
8 PC8 SPI_SCLK DISP_SCLK USART1_CLK #11
6 PC7 SPI_MISO USART1_RX #11
4 PC6 SPI_MOSI DISP_MOSI USART1_TX #11
2 VMCU BGM111 voltage domain, included in AEM measurements.
19 BOARD_ID_SDA Connected to Board Controller for identification of add-on boards.
17 BOARD_ID_SCL Connected to Board Controller for identification of add-on boards.
15 PC11 I2C_SCL SENSOR_I2C_SCL I2C0_SCL #15
13 PF3 GPIO DBG_TDI
11 PB11 GPIO PTI_CLK
9 PF5 GPIO
7 PF4 GPIO
5 PA3 UART_RTS VCOM_RTS USART0_CS #0
3 PA2 UART_CTS VCOM_CTS USART0_CLK #0
1 GND Ground
Note: Pin PF3 is used for DBG_TDI in JTAG mode only. When Serial Wire Debugging is used, PF3 can be used for other purposes.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Connectors
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 7
\“H‘ m. TTT ‘mw—nnou N H“ J.“ TIT
4.3 Debug Connector
The Debug Connector serves multiple purposes based on the "debug mode" setting which can be configured in Simplicity Studio. When
the debug mode is set to "Debug IN", the debug connector can be used to connect an external debugger to the BGM111 on the radio
board. When set to "Debug OUT", this connector allows the kit to be used as a debugger towards an external target. When set to "De-
bug MCU" (default), the connector is isolated from both the on-board debugger and the radio board target device.
Because this connector is electronically switched between the different operating modes, it can only be used when the Board Controller
is powered (i.e. J-Link USB cable connected). If debug access to the target device is required when the Board Controller is unpowered,
connect directly to the appropriate breakout pins.
The pinout of the connector follows that of the standard ARM Cortex Debug+ETM 19-pin connector. The pinout is described in detail
below. Even though the connector has support for both JTAG and ETM Trace, it does not necessarily mean that the kit or the on-board
target device supports this.
1 2
4
8
6
10
3
5
9
12
13 14
11
15 16
17 18
2019
TMS / SWDIO / C2D
TCK / SWCLK / C2CK
TDO / SWO
TDI / C2Dps
TRACECLK
TRACED0
TRACED1
TRACED2
TRACED3
RESET / C2CKps
GND
NC
NC
GND
GND
GND
7
GND
VTARGET
Cable Detect
NC
Figure 4.4. Debug Connector
Note: The pinout matches the pinout of an ARM Cortex Debug+ETM connector, but these are not fully compatible as pin 7 is physically
removed from the Cortex Debug+ETM connector. Some cables have a small plug that prevent them from being used when this pin is
present. If this is the case, remove the plug, or use a standard 2x10 1.27 mm straight cable instead.
Table 4.2. Debug Connector Pin Descriptions
Pin number(s) Function Description
1 VTARGET Target voltage on the debugged application.
2 TMS / SDWIO / C2D JTAG test mode select, Serial Wire data or C2 data
4 TCK / SWCLK / C2CK JTAG test clock, Serial Wire clock or C2 clock
6 TDO/SWO JTAG test data out or Serial Wire Output
8 TDI / C2Dps JTAG test data in, or C2D "pin sharing" function
10 RESET / C2CKps Target device reset, or C2CK "pin sharing" function
12 TRACECLK
14 TRACED0
16 TRACED1
18 TRACED2
20 TRACED3
9 Cable detect Connect to ground
11, 13 NC Not connected
3, 5, 15, 17, 19 GND Ground
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Connectors
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 8
4.4 Simplicity Connector
The Simplicity Connector enables the advanced debugging features, such as the AEM, the Virtual COM port and the Packet Trace In-
terface, to be used towards an external target. The pinout is illustrated in the figure below.
VMCU 1
33V3
5
5V
15
GND
13
GND
11
GND
9
GND
7
GND
17
Board ID SCL
19
Board ID SDA
2Virtual COM TX / MOSI
4Virtual COM RX / MISO
6Virtual COM CTS / SCLK
8Virtual COM RTS / CS
10 Packet Trace 0 Sync
12 Packet Trace 0 Data
14 Packet Trace 0 Clock
16 Packet Trace 1 Sync
18 Packet Trace 1 Data
20 Packet Trace 1 Clock
Figure 4.5. Simplicity Connector
Note: Current drawn from the VMCU voltage pin is included in the AEM measurements, while the 3V3 and 5V voltage pins are not. To
monitor the current consumption of an external target with the AEM, unplug the Radio Board from the Wireless STK Mainboard to avoid
that the Radio Board current consumption is added to the measurements.
Table 4.3. Simplicity Connector Pin Descriptions
Pin number(s) Function Description
1 VMCU 3.3 V power rail, monitored by the AEM
3 3V3 3.3 V power rail
5 5V 5 V power rail
2 VCOM_TX_MOSI Virtual COM Tx/MOSI
4 VCOM_RX_MISO Virtual COM Rx/MISO
6 VCOM_CTS_SCLK Virtual COM CTS/SCLK
8 VCOM_RTS_CS Virtual COM RTS/CS
10 PTI0_SYNC Packet Trace 0 Sync
12 PTI0_DATA Packet Trace 0 Data
14 PTI0_CLK Packet Trace 0 Clock
16 PTI1_SYNC Packet Trace 1 Sync
18 PTI1_DATA Packet Trace 1 Data
20 PTI1_CLK Packet Trace 1 Clock
17 EXT_ID_SCL Board ID SCL
19 EXT_ID_SDA Board ID SDA
7, 9, 11, 13, 15 GND Ground
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Connectors
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 9
an be selected wi
5. Power Supply and Reset
5.1 Radio Board Power Selection
The BGM111 on a Wireless Starter Kit can be powered by one of these sources:
the debug USB cable;
a 3 V coin cell battery; or
a USB regulator on the Radio Board (for devices with USB support only).
The power source for the radio board is selected with the slide switch in the lower left corner of the Wireless STK Mainboard. Figure
5.1 Power Switch on page 10 shows how the different power sources can be selected with the slide switch.
VMCU
AEM
USB
BAT
USB Mini-B
Connector
Advanced
Energy
Monitor
3 V Lithium Battery
(CR2032)
BAT
USB
AEM
LDO
BGM111
5 V 3.3 V
Figure 5.1. Power Switch
With the switch in the AEM position, a low noise 3.3 V LDO on the WSTK Mainboard is used to power the Radio Board. This LDO is
again powered from the debug USB cable. The Advanced Energy Monitor is now also connected in series, allowing accurate high
speed current measurements and energy debugging/profiling.
With the switch in the USB position, radio boards with USB-support can be powered by a regulator on the radio board itself. BRD4300A
does not contain an USB regulator, and setting the switch in the USB postition will cause the BGM111 to be unpowered.
Finally, with the switch in the BAT position, a 20 mm coin cell battery in the CR2032 socket can be used to power the device. With the
switch in this position no current measurements are active. This is the recommended switch position when powering the radio board
with an external power source.
Note: The current sourcing capabilities of a coin cell battery might be too low to supply certain wireless applications.
Note: The Advanced Energy Monitor can only measure the current consumption of the BGM111 when the power selection switch is in
the AEM position.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Power Supply and Reset
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 10
5.2 Board Controller Power
The board controller is responsible for important features such as the debugger and the Advanced Energy Monitor, and is powered
exclusively through the USB port in the top left corner of the board. This part of the kit resides on a separate power domain, so a differ-
ent power source can be selected for the target device while retaining debugging functionality. This power domain is also isolated to
prevent current leakage from the target power domain when power to the Board Controller is removed.
The board controller power domain is not influenced by the position of the power switch.
The kit has been carefully designed to keep the board controller and the target power domains isolated from each other as one of them
powers down. This ensures that the target BGM111 device will continue to operate in the USB and BAT modes.
5.3 BGM111 Reset
The BGM111 Bluetooth Module can be reset by a few different sources:
A user pressing the RESET button.
The on-board debugger pulling the #RESET pin low.
An external debugger pulling the #RESET pin low.
In addition to the reset sources mentioned above, a reset to the BGM111 will also be issued during Board Controller boot-up. This
means that removing power to the Board Controller (plugging out the J-Link USB cable) will not generate a reset, but plugging the cable
back in will, as the Board Controller boots up.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Power Supply and Reset
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 11
6. Peripherals
The starter kit has a set of peripherals that showcase some of the features of the BGM111.
Be aware that most BGM111 I/O routed to peripherals are also routed to the breakout pads. This must be taken into consideration when
using the breakout pads for your application.
6.1 Push Buttons and LEDs
The kit has two user push buttons marked PB0 and PB1. They are connected directly to the BGM111, and are debounced by RC filters
with a time constant of 1 ms. The buttons are connected to pins PF6 and PF7.
The kit also features two yellow LEDs marked LED0 and LED1, that are controlled by GPIO pins on the BGM111. The LEDs are con-
nected to pins PF6 and PF7 in an active-high configuration.
User Buttons
& LEDs
UIF_BUTTON0_LED0
UIF_BUTTON1_LED1
PF6 (GPIO)
PF7 (GPIO)
BGM111
Figure 6.1. Buttons and LEDs
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Peripherals
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 12
4 Board Conuoner +> msESCLK Dwspjl msP,scs D‘SPiEXTCOMIN D‘SPiENABLE % 77 SI % 65'? 4, SILIEIJN LABS EXTCOM‘N % 128x128 pixel Memory LCD
6.2 Memory LCD-TFT Display
A 1.28-inch SHARP Memory LCD-TFT is available on the kit to enable interactive applications to be developed. The display has a high
resolution of 128 by 128 pixels, and consumes very little power. It is a reflective monochrome display, so each pixel can only be light or
dark, and no backlight is needed in normal daylight conditions. Data sent to the display is stored in the pixels on the glass, which means
no continous refreshing is required to maintain a static image.
The display interface consists of an SPI-compatible serial interface and some extra control signals. Pixels are not individually addressa-
ble, instead data is sent to the display one line (128 bits) at a time.
The Memory LCD-TFT display is shared with the kit Board Controller, allowing the Board Controller application to display useful infor-
mation when the user application is not using the display. The user application always controls ownership of the display with the
DISP_ENABLE signal:
DISP_ENABLE = LOW: The Board Controller has control of the display
DISP_ENABLE = HIGH: The user application (BGM111) has control of the display
Power to the display is sourced from the target application power domain when the BGM111 controls the display, and from the Board
Controller's power domain when the DISP_ENABLE line is low. Data is clocked in on DISP_SI when DISP_CS is high, and the clock is
sent on DISP_SCLK. The maximum supported clock speed is 1.1 MHz.
DISP_COM is the "COM Inversion" line. It must be pulsed periodically to prevent static build-up in the display itself. Please refer to the
display application information for details on driving the display:
http://www.sharpmemorylcd.com/1-28-inch-memory-lcd.html
Figure 6.2. 128x128 Pixel Memory LCD
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Peripherals
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 13
6.3 Si7021 Relative Humidity and Temperature Sensor
The Si7021 I2C relative humidity and temperature sensor is a monolithic CMOS IC integrating humidity and temperature sensor ele-
ments, an analog-to-digital converter, signal processing, calibration data, and an I2C Interface. The patented use of industry-standard,
low-K polymeric dielectrics for sensing humidity enables the construction of low-power, monolithic CMOS Sensor ICs with low drift and
hysteresis, and excellent long term stability.
The humidity and temperature sensors are factory-calibrated and the calibration data is stored in the on-chip non-volatile memory. This
ensures that the sensors are fully interchangeable, with no recalibration or software changes required.
The Si7021 is available in a 3x3 mm DFN package and is reflow solderable. It can be used as a hardware- and software-compatible
drop-in upgrade for existing RH/ temperature sensors in 3x3 mm DFN-6 packages, featuring precision sensing over a wider range and
lower power consumption. The optional factory-installed cover offers a low profile, convenient means of protecting the sensor during
assembly (e.g., reflow soldering) and throughout the life of the product, excluding liquids (hydrophobic/oleophobic) and particulates.
The Si7021 offers an accurate, low-power, factory-calibrated digital solution ideal for measuring humidity, dew-point, and temperature,
in applications ranging from HVAC/R and asset tracking to industrial and consumer platforms.
The I2C bus used for the Si7021 is shared with the Expansion Header. The temperature sensor is normally isolated from the I2C line. To
use the sensor, SENSOR_ENABLE (tied high) must be set high. When enabled, the sensor's current consumption is included in the
AEM measurements.
SENSOR_ENABLE
0: I2C lines are isolated, sensor is not powered
1: Sensor is powered and connected
PC11 (I2C0_SCL)
PC10 (I2C0_SDA)
NC (tied high)
SENSOR_I2C_SDA
SENSOR_I2C_SCL
VMCU
VDD
SCL
SDA Temperature
& Humidity
Sensor
BGM111
Si7021
Figure 6.3. Si7021 Relative Humidity and Temperature Sensor
Please refer to the Silicon Labs web pages for more information: http://www.silabs.com/humidity-sensors
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Peripherals
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 14
6.4 Virtual COM Port
An asynchronous serial connection to the board controller is provided for application data transfer between a host PC and the target
BGM111. This eliminates the need for an external serial port adapter.
VCOM_ENABLE
PA0 (US0_TX#0)
PA1 (US0_RX#0)
PA5 (GPIO)
VCOM_RX
VCOM_TX
Board
Controller
BGM111
USB Host
PC
Isolation & Level Shift
PA2 (US0_CTS#30)
PA3 (US0_RTS#30)
VCOM_CTS
VCOM_RTS
ETH
or
Figure 6.4. Virtual COM Port Interface
The Virtual COM port consists of a physical UART between the target device and the board controller, and a logical function in the
board controller that makes the serial port available to the host PC over USB or Ethernet. The UART interface consists of four pins and
an enable signal.
Table 6.1. Virtual COM Port Interface Pins
Signal Description
VCOM_TX Transmit data from the BGM111 to the board controller
VCOM_RX Receive data from the board controller to the BGM111
VCOM_CTS Clear to Send hardware flow control input, asserted by the board controller when it is ready to receive more data
VCOM_RTS Request to Send hardware flow control output, asserted by the BGM111 when it is ready to receive more data
VCOM_ENABLE Enables the VCOM interface, allowing data to pass through to the board controller.
The parameters of the serial port, such as baud rate or flow control, can be configured using the admin console. The default settings
depends on which radio board is used with the Wireless STK Mainboard. Please see 11. Device Connectivity for more details.
Note: The VCOM port is only available when the board controller is powered, which requires the J-Link USB cable to be inserted.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Peripherals
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 15
7. Board Controller
The Wireless STK Mainboard contains a microcontroller separate from the BGM111 Blue Gecko that is responsible for some of the
advanced kit features provided. This microcontroller is referred to as the "Board Controller", and is not programmable by the user. The
board controller acts as an interface between the host PC and the target device on the radio board, as well as handling some house-
keeping functions on the board.
Some of the kit features actively managed by the board controller are:
The On-board Debugger, which can flash and debug both on-board and external targets.
The Advanced Energy Monitor, which provides real-time energy profiling of the user application.
The Packet Trace Interface , which is used in conjunction with PC software to provide detailed insight into an active radio network.
The Virtual COM Port and Virtual UART interfaces, which provide ways to transfer application data between the host PC and the
target processor.
The Admin Console, which provides configuration of the various board features.
Silicon Labs publishes updates to the board controller firmware in form of firmware upgrade packages. These updates may enable new
features or fix issues. See 12.2 Firmware Upgrades for details on firmware upgrade.
7.1 Admin Console
The admin console is a command line interface to the board controller on the kit. It provides functionality for configuring the kit behavior
and retreiving configuration and operational parameters.
Connecting
The Wireless STK Mainboard must be connected to Ethernet using the Ethernet connector in the top left corner of the mainboard for
the admin console to be available. See ● Ethernet Interface for details on the Ethernet connectivity.
Connect to the Admin Console by opening a telnet connection to the kit's IP address, port number 4902.
When successfully connected, a WSTK> prompt is displayed.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Board Controller
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 16
Built-in Help
The admin console has a built in help system which is accessed by the help command. The help command will print a list of all top
level commands:
WSTK> help
*************** Root commands ****************
aem AEM commands [ calibrate, current, dump, ... ]
boardid Commands for board ID probe. [ list, probe ]
dbg Debug interface status and control [ info, mode,]
dch Datachannel control and info commands [ info ]
discovery Discovery service commands.
net Network commands. [ dnslookup, geoprobe, ip ]
pti Packet trace interface status and control [ config, disable, dump, ... ]
quit Exit from shell
sys System commands [ nickname, reset, scratch, ... ]
target Target commands. [ button, flashwrite, go, ... ]
time Time Service commands [ client, server ]
user User management functions [ login,]
The help command can be used in conjunction with any top level command to get a list of sub-commands with description. For exam-
ple, pti help will print a list of all available sub-commands of pti:
WSTK> pti help
*************** pti commands ****************
config Configure packet trace
disable Disable packet trace
dump Dump PTI packets to the console as they come
enable Enable packet trace
info Packet trace state information
This means that running pti enable will enable packet trace.
Command Examples
PTI Configuration
pti config 0 efruart 1600000
Configures PTI to use the "EFRUART" mode at 1.6 Mb/s.
Serial Port Configuration
serial config vcom handshake enable
Enables hardware handshake on the VCOM UART connection.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Board Controller
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 17
8. Expansion Board
The User Interface Expansion Board included with the BGM111 Wireless STK includes the following features:
1x 3-axis accelerometer (Bosch Sensortech BMA280)
1x Joystick with 9 measurable positions
2x Push buttons and 2x LEDs
The connections between the Expansion Board and the BGM111 are shown in the figure below:
PA1 (GPIO)
BUTTON_LED2 (EXP7)
PF4 (GPIO)
BGM111
BUTTON_LED3 (EXP14) Buttons
& LEDs
Accelerometer
BMA280
Analog
Joystick
JOYSTICK (EXP12)
ACC_MOSI (EXP4)
ACC_MISO (EXP6)
ACC_SCK (EXP8)
ACC_CS (EXP10)
ACC_INT (EXP9)
PA0 (ADC)
PC6 (USART1_TX)
PC7 (USART1_RX)
PC8 (USART1_CLK)
PC9 (USART1_CS)
PF5 (GPIO)
Figure 8.1. User Interface Expansion Board
The following sections contain more detailed information about each feature.
8.1 Accelerometer
Bosch Sensortec BMA280 is a triaxial, low-power, low-g accelerometer sensor with SPI interface. It features 14-bit digital resolution and
allows very low-noise measurement of acceleration in 3 perpendicular axes and can therefore sense tilt, motion, shock and vibration.
Please refer to Bosch Sensortec's product page for a detailed datasheet of this sensor: http://www.bosch-sensortec.com/bst/products/
all_products/bma280
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Expansion Board
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 18
chU A u \FJOYST‘CK Joystick SW S SE 15k GUAk
8.2 Push Buttons and LEDs
The Expansion Board contains two push buttons (marked BTN2 and BTN3 on the PCB) and two LEDs (LED2 and LED3, not marked
but placed correspondingly above the push button markings). One push button and one LED share the same I/O pin on the BGM111.
The push button is connected to the LED through a transistor, allowing the I/O to be used either as an input (for reading the push button
state) or as an output (to control the LED state on or off).
When configured as an input, "0" indicates that the button is being pressed and "1" that the push button is not being pressed. Likewise,
when configured as an output, "0" will turn the LED on and "1" will turn it off.
Pressing a push button will also light up the corresponding LED because the LED is controlled by the same line (state) regardless of
whether it is the BGM111 or the push button that pulls the line low.
The each button is debounced by an RC filter with a time constant of about 1 ms. Pressing the push button while having the pin config-
ured as an output in high state ("1") will not cause damage, but will cause extra current to flow.
8.3 Joystick
The analog joystick offers 9 measureable positions. This joystick is connected to the BGM111 pin PD4. Each of the joystick output pins
are connected to a different resistor value to create a unique voltage that is measured by the internal ADC on the BGM111. The joystick
output is connected to AD Channel 0 (ADC0). The figure below shows the connection between the joystíck and the BGM111.
PA0 (ADC)
BGM111
PA0 (ADC)_miso
MX25R8035F
8 Mbit
Figure 8.2. User Interface Expansion Board Joystick
The table below lists the expected output voltage from each joystick position.
Table 8.1. Joystick Output Voltage
Position Resistor combinations [kohm] Joystick output voltage [V]1
Center press 0.1 / (0.1 + 10) 0.03 V
Up (N) 60.4 / (60.4 + 10) 2.83 V
Up-Right (NE) {(N // E) / {(N // E) + 10 } = 21.34 / (21.34
+ 10)
2.25 V
Right (E) 33 / (33 + 10) 2.53 V
Down-Right (SE) (S // E) / {(S // E) + 10)} = 7.67 / (7.67 + 10) 1.43 V
Down (S) 10 / (10 + 10) 1.65 V
Down-Left (SW) (S // W) / {(S // W) + 10)} = 6 / (6 + 10) 1.24 V
Left (W) 15 / (15 + 10) 1.98 V
Up-Left (NW) (N // W) / {(N // W) + 10)} = 12.01 / (12.01
+ 10)
1.80 V
Note: 1) Output Voltage is calculated with VMCU of 3.3 V .
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Expansion Board
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 19
3.3V Power Se‘ect Switch VMCU 2.35 0 Sense Resistor i/ l Current Sense Amp‘ifier Multip‘e Gain Stages ii
9. Advanced Energy Monitor
9.1 Introduction
Any embedded developer seeking to make his embedded code spend as little energy as the underlying architecture supports, needs
tools to easily and quickly discover inefficiencies in the running application.
This is what the Simplicity Energy Profiler is designed to do. It will in real-time graph and log current as a function of time while correlat-
ing this to the actual target application code running on the BGM111. There are multiple features in the profiler software that allows for
easy analysis, such as markers and statistics on selected regions of the current graph or aggregate energy usage by different parts of
the application.
9.2 Theory of Operation
The Advanced Energy Monitor (AEM) circuitry on the board is capable of measuring current signals in the range of 0.1 µA to 95 mA,
which is a dynamic range of alomst 120 dB. It can do this while maintaining approximately 10 kHz of current signal bandwidth. This is
accomplished through a combination of a highly capable current sense amplifier, multiple gain stages and signal processing within the
kit's board controller before the current sense signal is read by a host computer for display and/or storage.
The current sense amplifier measures the voltage drop over a small series resistor, and the gain stage further amplifies this voltage with
two different gain settings to obtain two current ranges. The transition between these two ranges occurs around 250 µA.
The current signal is combined with the target processor's Program Counter (PC) sampling by utilizing a feature of the ARM CoreSight
debug architecture. The ITM (Instrumentation Trace Macrocell) block can be programmed to sample the MCU's PC at periodic intervals
(50 kHz) and output these over SWO pin ARM devices. When these two data streams are fused and correlated with the running appli-
cation's memory map, an accurate statistical profile can be built, that shows the energy profile of the running application in real-time.
At kit power-up or on a power-cycle, and automatic AEM calibration is performed. This calibration compensates for any offset errors in
the current sense amplifiers.
BGM111
LDO
Peripherals
AEM
Processing
Figure 9.1. Advanced Energy Monitor
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Advanced Energy Monitor
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 20
9.3 AEM Accuracy and Performance
The AEM is capable of measuring currents in the range of 0.1 µA to 95 mA. For currents above 250 µA, the AEM is accurate within 0.1
mA. When measuring currents below 250 µA, the accuracy increases to 1 µA. Even though the absolute accuracy is 1 µA in the sub
250 µA range, the AEM is able to detect changes in the current consumption as small as 100 nA.
The AEM current sampling rate is 10 kHz.
Note: The AEM circuitry only works when the kit is powered and the power switch is in the AEM position.
9.4 Usage
The AEM data is collected by the board controller and can be displayed by the Energy Profiler, available through Simplicity Studio. By
using the Energy Profiler, current consumption and voltage can be measured and linked to the actual code running on the BGM111 in
realtime.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Advanced Energy Monitor
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 21
10. On-Board Debugger
The Wireless Starter Kit contains an integrated debugger, which can be used to download code and debug the BGM111. In addition to
programming the BGM111 on the kit, the debugger can also be used to program and debug external Silicon Labs EFM32, EFM8,
EZR32 and EFR32 devices.
The debugger supports three different debug interfaces used with Silicon Labs devices:
Serial Wire Debug, is used with all EFM32, EFR32 and EZR32 devices
JTAG, which can be used with EFR32 and some EFM32 devices
C2 Debug, which is used with EFM8 devices
In order for debugging to work properly, make sure you have the appropriate debug interface selected that works with your device. The
debug connector on the board supports all three of these modes.
10.1 Host Interfaces
The Wireless Starter Kit supports connecting to the on-board debugger using either Ethernet or USB.
Many tools support connecting to a debugger using either USB or Ethernet. When connected over USB, the kit is identified by its J-Link
serial number. When connected over Ethernet, the kit is normally identified by its IP address. Some tools also support using the serial
number when connecting over Ethernet, this typically require the computer and the kit to be on the same subnet for the discovery proto-
col (using UDP broadcast packets) to work.
USB Interface
The USB interface is available whenever the USB Mini-B connector on the left hand side of the mainboard is connected to a computer.
Ethernet Interface
The Ethernet interface is available when the mainboard Ethernet connector in the top left corner is connected to a network. Normally,
the kit will receive an IP address from a local DHCP server, and the IP address is printed on the LCD display. If your network does not
have a DHCP server, you need to connect to the kit via USB and set the IP address manually using Simplicity Studio, Simplicity
Commander or J-Link Configurator.
For the Ethernet connectivity to work, the kit must still be powered through the USB Mini-B connector. See 5.2 Board Controller Power
for details.
Serial Number Identification
All Silicon Labs kits have a unique J-Link serial number which identifies the kit to PC applications. This number is 9 digits, and is nor-
mally on the form 44xxxxxxx.
The J-Link serial number is normally printed at the bottom of the kit LCD display.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
On-Board Debugger
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 22
10.2 Debug Modes
Programming external devices is done by connecting to a target board through the provided Debug IN/OUT Connector, and by setting
the debug mode to [Out]. The same connector can also be used to connect an external debugger to the BGM111 Bluetooth Module on
the kit, by setting debug mode to [In].
Selecting the active debug mode is done with a drop-down menu in the Kit Manager tool in Simplicity Studio.
Debug MCU: In this mode the on-board debugger is connected to the BGM111 on the SLWSTK6101C.
RADIO BOARD
Board
Controller
USB
Host
Computer
DEBUG HEADER
External
Hardware
Figure 10.1. Debug MCU
Debug OUT: In this mode, the on-board debugger can be used to debug a supported Silicon Labs device mounted on a custom board.
Board
Controller
USB
Host
Computer
DEBUG HEADER
External
Hardware
RADIO BOARD
Figure 10.2. Debug OUT
Debug IN: In this mode, the on-board debugger is disconnected, and an external debugger can be connected to debug the BGM111 on
the Wireless Starter Kit.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
On-Board Debugger
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 23
Board
Controller
USB
Host
Computer
DEBUG HEADER
External Debug Probe
RADIO BOARD
Figure 10.3. Debug IN
Note: For "Debug IN" to work, the board controller on the kit must be powered throught the USB connector.
10.3 Debugging During Battery Operation
When the BGM111 is powered by battery and the J-Link USB is still connected, the on-board debug functionality is available. If the USB
power is disconnected, the Debug In mode will stop working.
If debug access is required when the target is running of another energy source, such as a battery, and the board controller is powered
down, the user should make direct connections to the GPIO used for debugging. This can be done by connecting to the appropriate
pins of the breakout pads. Some Silicon Labs kits provide a dedicated pin header for this purpose.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
On-Board Debugger
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 24
11. Device Connectivity
The Wireless STK Mainboard provides several convenient ways to communicate with a target application without soldering or using
external hardware.
11.1 Virtual COM Port
When the target device drives the VCOM_ENABLE (PA5) signal high, a communication line to the Board Controller is enabled. The
target can then communicate to the host computer via the Board Controller using USART0, Location 0 (TX pin PA0, RX pin PA1).
When enabling VCOM, the Board Controller makes communication to the host computer possible on the following interfaces:
Virtual USB serial port using a CDC driver.
TCP/IP, by connecting to the Wireless STK on port 4901 with a Telnet client.
Note: Only one of these can be used at the same time, meaning that if a socket is connected to port 4901, no data can be sent or
received on the USB COM port.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Device Connectivity
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 25
5 mm. i Adapter lnfonnntlon Tm USE Saul Mumbet 440019215 deu Slaw Ki! lnformltion Null- W32 Gil! Gl(kn Sum: Kl Bord In W lav. A03 Sui Mumhn 1W3 Flmvflle Vain“ 0199137391 um n lam flange Fm“ My mm mm— MCU lnfonnatlon Name swam mm W [00:31 [*9 um ~ 0 JD mm ID 20 m h 1524 k‘B sum in 125 “3 “w“ ID Wm
12. Kit Manager and Upgrades
The Kit Manager is a program that comes with Simplicity Studio. It can perform various kit and device specific tasks.
12.1 Kit Manager Operation
This utility gives the ability to program the BGM111, upgrade the kit, lock and unlock devices and more. Some of the features will only
work with Silicon Labs kits, while other will work with a generic J-Link debugger connected.
Figure 12.1. Kit Manager
12.2 Firmware Upgrades
Upgrading the kit firmware is done through Simplicity Studio. Simplicity Studio will automatically check for new updates on startup.
You can also use the Kit Manager for manual upgrades. Click the [Browse] button in the [Update Kit] section to select the correct file
ending in ".emz". Then, click the [Install Package] button.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Kit Manager and Upgrades
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 26
13. Radio Board Connectors
Radio Boards contain two dual-row, female socket, 0.05" pitch polarized connectors (P/N: SFC-120-T2-L-D-A-K-TR) which provide the
interface to the Wireless Starter Kit Mainboard. The Mainboard has the corresponding male header pin connectors (P/N: TFC-120-02-
F-D-LC-ND).
13.1 Radio Board Connector Pin Mapping
The figure below shows the pin mapping on the connector to the radio pins and their corresponding function on the Wireless Starter Kit
Mainboard.
GND
F9 / PA3 / VCOM_RTS
3V3
NC / P36
P200
Upper Row
NC / P38
NC / P40
NC / P42
NC / P44
DBG_TMS_SWDIO / PF1 / F0
DISP_ENABLE / PD15 / F14
BUTTON0 / PF6 / F12
LED0 / PF6 / F10
VCOM_CTS / PA2 / F8
DBG_RESET / F4
DBG_TDO_SWO / PF2 / F2
DISP_SI / PC6 / F16
VCOM_TX / PA0 / F6
PTI_DATA / PA4 / F20
DISP_EXTCOMIN / PD13 / F18
USB_VBUS
5V
Board ID SCL
GND
Board ID SDA
USB_VREG
F7 / PA1 / VCOM_RX
F5 / PA5 / VCOM_ENABLE
F3 / PF3 / DBG_TDI
F1 / PF0 / DBG_TCK_SWCLK
P45 / NC
P43 / NC
P41 / NC
P39 / NC
P37 / TIED HIGH / SENSOR_ENABLE
F11 / PF7 / LED1
F13 / PF7 / BUTTON1
F15 / PC8 / DISP_SCLK
F17 / PD14 / DISP_SCS
F19 / PB13 / PTI_FRAME
F21 / PB11 / PTI_CLK
GND VMCU_IN
EXP3 / PA2 / P0
P201
Lower Row
EXP5 / PA3 / P2
EXP7 / PF4 / P4
EXP9 / PF5 / P6
GND VRF_IN
P35 / NC
P7 / PC9 / EXP10
P5 / PC8 / EXP8
P3 / PC7 / EXP6
P1 / PC6 / EXP4
P33 / PF7
P31 / PF6
P29 / PF2
P27 / PF1
P25 / PF0
P23 / PD15
P21 / PD14
P19 / PD13
P17 / NC
P15 / NC
P13 / PC10 / EXP16
P11 / PA1 / EXP14
P9 / PA0 / EXP12
NC / P34
NC / P32
NC / P30
NC / P28
NC / P26
NC / P24
PB13 / P22
PA5 / P20
PA4 / P18
NC / P16
NC / P14
EXP15 / PC11 / P12
EXP13 / PF3 / P10
EXP11 / PB11 / P8
Figure 13.1. Radio Board Connectors
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Radio Board Connectors
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 27
40 mm 24 mm 5mm uuuuuuu uuuuuuu- uuuuuuu uuuuuuuu uuuuuuu- uuuuuuuu 15 mm
14. Mechanical Details
The mechanical layout of BRD4300A BGM111 Blue Gecko Bluetooth Module Radio Board is illustrated in the figures below.
Figure 14.1. BRD4300A Top View
Figure 14.2. BRD4300A Bottom View
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Mechanical Details
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 28
15. Schematics, Assembly Drawings and BOM
Schematics, assembly drawings and bill of materials (BOM) are available through Simplicity Studio when the kit documentation pack-
age has been installed.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Schematics, Assembly Drawings and BOM
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 29
16. Radio Board Revision History and Errata
16.1 Revision History
Radio Board revision is printed on the backside of the BRD4300A Radio Board.
Table 16.1. BRD4300A Revision History
Radio Board Revision Released Description
A03 2016-07-04 Updated BGM111 module revision from V1.1 to V2
A02 2016-03-28 Updated BGM111 module revision from V1 to V1.1.
A01 2015-07-01 Updated BGM111 module to first release version.
A00 2015-05-22 Pre-production series with early version of BGM111. This version does not have
full RF performance.
16.2 Errata
Table 16.2. BRD4300A Errata
Radio Board Revision Problem Description
A01 RF performance. Reduced RF performance.
A00 RF performance RF range reduced due to sub-optimal antenna matching on the BGM111 mod-
ule.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Radio Board Revision History and Errata
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 30
(1P) Part: (D) Date. S.nr: (Q) Qty: 1 H|||\||||||||\|\||||\IHHIIIII\Im||\H|||\||||||\|\|||||H||| H|||\|\||
17. Kit Revision History and Errata
The kit revision can be found printed on the kit packaging label, as outlined in the figure below.
SLWSTK6101C
Blue Gecko Module Wireless Starter Kit
124802042
29-09-16
A00
Figure 17.1. Kit Label
17.1 SLWSTK6101A Revision history
Kit Revision Released Description
A01 2015-07-01 Updated BRD4300A from revision A00 to revision A01.
A00 2015-06-17 Initial kit release.
17.2 SLWSTK6101B Revision History
Kit Revision Released Description
A01 2016-07-06 Updated BRD4300A to revision A03.
A00 2016-04-13 Initial kit release. Replaces SLWSTK6101A. Adds BGM113 Bluetooth Module
Radio Board to kit.
17.3 SLWSTK6101C Revision history
Kit Revision Released Description
A00 2016-09-29 Initial kit release. Replaces SLWSTK6101B. Adds BGM121 Bluetooth System-
in-Package Radio Board to kit and removes BGM113 Bluetooth Module Radio
Board.
17.4 SLWRB4300A Revision history
Kit Revision Released Description
A01 2016-08-16 Updated BRD4300A to from revision A02 to revision A03.
A00 2016-02-01 Initial release.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Kit Revision History and Errata
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 31
18. Document Revision History
Revision 3.00
2016-10-19
Added sections for ordering information, mechanical drawings and radio board connector pin-out, deprecating the BRD4300A Refer-
ence Manual.
Added kit revision A01 to revision history.
Smart removed from Bluetooth Smart for consistenty.
Simplicity Studio added to front page features.
Revision 2.00
2016-03-28
Updated document to reflect transition to SLWSTK6101B.
Added chapter on EXP board included in kit.
Revision 1.00
2015-09-30
Corrected pinout for buttons/leds and I2C bus.
Revision 0.90
2015-06-30
Initial version.
UG122: BGM111 Bluetooth Module Radio Board User's Guide
Document Revision History
silabs.com | Smart. Connected. Energy-friendly. Rev. 3.00 | 32
Table of Contents
1. Introduction ................................1
1.1 Radio Boards ..............................1
1.2 Ordering Information ...........................2
1.3 Getting Started .............................2
2. Kit Hardware Overview............................3
3. Kit Block Diagram .............................4
4. Connectors ................................5
4.1 Breakout Pads .............................5
4.2 Expansion Header ............................6
4.2.1 Expansion Header Pin-out .........................7
4.3 Debug Connector.............................8
4.4 Simplicity Connector............................9
5. Power Supply and Reset .......................... 10
5.1 Radio Board Power Selection ........................10
5.2 Board Controller Power...........................11
5.3 BGM111 Reset .............................11
6. Peripherals ............................... 12
6.1 Push Buttons and LEDs ..........................12
6.2 Memory LCD-TFT Display..........................13
6.3 Si7021 Relative Humidity and Temperature Sensor .................14
6.4 Virtual COM Port .............................15
7. Board Controller ............................. 16
7.1 Admin Console .............................16
8. Expansion Board ............................. 18
8.1 Accelerometer..............................18
8.2 Push Buttons and LEDs ..........................19
8.3 Joystick ................................19
9. Advanced Energy Monitor ......................... 20
9.1 Introduction...............................20
9.2 Theory of Operation ............................20
9.3 AEM Accuracy and Performance .......................21
9.4 Usage ................................21
10. On-Board Debugger ........................... 22
10.1 Host Interfaces .............................22
10.2 Debug Modes .............................23
Table of Contents 33
10.3 Debugging During Battery Operation ......................24
11. Device Connectivity ........................... 25
11.1 Virtual COM Port ............................25
12. Kit Manager and Upgrades ......................... 26
12.1 Kit Manager Operation ..........................26
12.2 Firmware Upgrades ...........................26
13. Radio Board Connectors ......................... 27
13.1 Radio Board Connector Pin Mapping......................27
14. Mechanical Details ............................ 28
15. Schematics, Assembly Drawings and BOM .................. 29
16. Radio Board Revision History and Errata ................... 30
16.1 Revision History.............................30
16.2 Errata ................................30
17. Kit Revision History and Errata ....................... 31
17.1 SLWSTK6101A Revision history .......................31
17.2 SLWSTK6101B Revision History .......................31
17.3 SLWSTK6101C Revision history .......................31
17.4 SLWRB4300A Revision history........................31
18. Document Revision History ........................ 32
Table of Contents .............................. 33
Table of Contents 34
Q SILICON LABS
http://www.silabs.com
Silicon Laboratories Inc.
400 West Cesar Chavez
Austin, TX 78701
USA
Simplicity Studio
One-click access to MCU and
wireless tools, documentation,
software, source code libraries &
more. Available for Windows,
Mac and Linux!
IoT Portfolio
www.silabs.com/IoT
SW/HW
www.silabs.com/simplicity
Quality
www.silabs.com/quality
Support and Community
community.silabs.com
Disclaimer
Silicon Labs intends to provide customers with the latest, accurate, and in-depth documentation of all peripherals and modules available for system and software implementers using or
intending to use the Silicon Labs products. Characterization data, available modules and peripherals, memory sizes and memory addresses refer to each specific device, and "Typical"
parameters provided can and do vary in different applications. Application examples described herein are for illustrative purposes only. Silicon Labs reserves the right to make changes
without further notice and limitation to product information, specifications, and descriptions herein, and does not give warranties as to the accuracy or completeness of the included
information. Silicon Labs shall have no liability for the consequences of use of the information supplied herein. This document does not imply or express copyright licenses granted
hereunder to design or fabricate any integrated circuits. The products are not designed or authorized to be used within any Life Support System without the specific written consent of
Silicon Labs. A "Life Support System" is any product or system intended to support or sustain life and/or health, which, if it fails, can be reasonably expected to result in significant personal
injury or death. Silicon Labs products are not designed or authorized for military applications. Silicon Labs products shall under no circumstances be used in weapons of mass
destruction including (but not limited to) nuclear, biological or chemical weapons, or missiles capable of delivering such weapons.
Trademark Information
Silicon Laboratories Inc.® , Silicon Laboratories®, Silicon Labs®, SiLabs® and the Silicon Labs logo®, Bluegiga®, Bluegiga Logo®, Clockbuilder®, CMEMS®, DSPLL®, EFM®, EFM32®,
EFR, Ember®, Energy Micro, Energy Micro logo and combinations thereof, "the world’s most energy friendly microcontrollers", Ember®, EZLink®, EZRadio®, EZRadioPRO®,
Gecko®, ISOmodem®, Precision32®, ProSLIC®, Simplicity Studio®, SiPHY®, Telegesis, the Telegesis Logo®, USBXpress® and others are trademarks or registered trademarks of Silicon
Labs. ARM, CORTEX, Cortex-M3 and THUMB are trademarks or registered trademarks of ARM Holdings. Keil is a registered trademark of ARM Limited. All other products or brand
names mentioned herein are trademarks of their respective holders.