Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Product List
anti-static-slide9

In summary, when choosing a static control product, it is necessary to consider the type material or substrate to which the product will be applied, whether it is more appropriate to eliminate the static completely, or to control and dissipate it, and if the solution is to be permanent or temporary. This means a choice between static-eliminating topical liquids and static-dissipative coatings which both play a major role in a ESD-control program.

PTM Veröffentlicht am: