Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
Image of Advantech ADAM-6300 OPC UA Remote I/O with Security Chip - Water Treatment

This is an example of a wastewater management application. The water quality is detected by analyzing parameters such as COD, PH, and particle levels. The ADAM-6317-A1 has analog input to obtain the data parameters from sensors. It directly supports the OPC UA protocol that can connect with the control center and cloud.

PTM Veröffentlicht am: