Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Gateway Function

The ADAM-6700 utilizing Node-RED allows the data to be converted into MQTT, RESTful, or Modbus protocols prior to sending to the Cloud or local SCADA system. In addition, the ADAM-6700 includes two RS-485 ports and two Ethernet ports on the module, which provide the flexibility to connect the ADAM-4000 series and ADAM-6000 series as an I/O extension or obtain data from devices like power meters.

PTM Veröffentlicht am: