Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Product List
simultaneous use

This Simultaneous Use Chart shows the variety of configurations while working with the FM-203. Shown here, if the far right side says “Yes” then those two irons can be used simultaneously because the power consumption combined does not go over 140 W. If it indicates “No”, then those two irons cannot be used together at the same time. It is useful for an operator to view this chart before beginning the work.

PTM Veröffentlicht am: