Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List Associated Content
Choosing the Right CO2 Sensor

Selecting the right CO2 sensor depends on the application. If the monitored environment experiences periodic exposure to background CO2 levels, the optimal solution will be a single-channel NDIR sensor utilizing ABC Logic™. This sensor will provide in-situ automated recalibration for the life of the sensor, improving performance and reducing the cost of ownership. If the monitored environment is continually occupied or not expected to see diurnal CO2 concentration cycles (such as hospitals, detention facilities, or indoor agricultural structures), a dual-channel NDIR is necessary. Without periodic exposure to background CO2 levels, firmware-based algorithms cannot be reliably deployed for drift compensation. While the hardware-based reference inherent in the dual-channel NDIR sensors can provide excellent drift compensation, recalibration will eventually be required for these NDIR sensors in order to retain factory-performance specifications.

PTM Veröffentlicht am: