Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
ADM3251E-Slide8

A charge pump voltage converter is used to generate the±10V supply for the RS-232 transmitter. This is done in two stages. First, the 5V input is doubled using a capacitor connected between pins C1+ and C1-. The +10V is then inverted by the capacitor connected between pins C2+ and C2- to produce the -10V supply. The receiver, on the other hand, uses an inverting level shifter to translate the higher voltage, dual polarity RS-232 signals into 5V logic levels.

PTM Veröffentlicht am: