Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Product List
Guide to PCB Layout Slide 6

You need to drive the layout process to a successful conclusion. When working with a CAD group, it is essential to spend the required time with the CAD personnel to explain the design including providing a description of the circuit, why it is essential to place certain components in the proper locations, defining the I/Os, outlining the power supply, and providing a complete board outline. After all, the CAD department is only going to do what they are told to do. It is the responsibility of the designer to communicate to them the desired layout and to maintain that communication until the desired result is obtained.

PTM Veröffentlicht am: