Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
ADF7xxx ISM Transceivers Slide 4

Using the ADF7xxx family, it is possible to achieve greater than a 3km range line of sight (LOS) without the need for external amplification. This is important for achieving range in difficult radio environments, such as communication from an underground water-pit to a meter reader. As can be seen here, the other standards support shorter ranges, and in some cases, higher data rates.

PTM Veröffentlicht am: