Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
core destroyer

It is often very difficult to securely erase all the data on an SSD. Sometimes a minor remnant of data may still be recoverable after some overwrite methods have been done on SSDs. It is the wear-leveling technology in SSDs that make it almost impossible to ensure each block is emptied out. This can be highly risky if the host of the drive often relies on SSDs for storing sensitive or even secret information. The Apacer CoreDestroyer Technology is the ultimate data-destroying, disk-execution solution. When executed, it not only wipes out data stored in user block and spare block, but also eliminates the management table in the system block and even the firmware. The disk is basically terminated and not workable. Everything in the drive is destroyed and the drive is lifeless. Users have to reload firmware into the SSD to bring it back to life.

PTM Veröffentlicht am: