Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Product List
Crypto Products Slide 31
Microchip does acknowledge that there are some overlaps in the types of applications that both CryptoMemory® and CryptoAuthentication™ can be used in. Here are some of the key differences between the two product offerings. First, CryptoMemory includes a faster 64-bit key algorithm, while CryptoAuthentication includes the standard SHA-256 algorithm. Second, CryptoMemory includes a range of EEPROM densities with very flexible security options. CryptoAuthentication has a small number of fuse bits for one-time programming. Third, CryptoMemory uses the industry standard I²C interface, and CryptoAuthentication uses a 1-wire interface. Finally, CryptoMemory is available in a variety of 8-lead plastic packages while CryptoAuthentication is available in the industry’s smallest 3-pin SOT23.
PTM Veröffentlicht am: