Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
MCU-Intro-Slide21
AVR offers a complete toolchain to aid in system design. Microchip provides complete high quality, low-cost development solutions including AVR Studio, an assembler, starter kits, and in-circuit-emulators which have all been created to maximize functionality. In-system development reduces time to market by letting the device be its own emulator ensuring identical behavior and electrical characteristics. Additionally, parts can be programmed when soldered into the board. This way, the test-program can be separated from the application to save flash space. More importantly, calibration code can be downloaded to the device. Calibration data is then stored in the flash or EEPROM while the final application is downloaded to the product. The AVR devices also support self-programming allowing the devices to upgrade their own firmware. This can be done with minimum risk, as most devices have a separate boot-block that can be individually protected.
PTM Veröffentlicht am: