Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
PowerProtector and AutoRefresh Technologies Slide 4

The unstable power conditions of systems running in extreme or harsh environments run the risk of data loss and drive corruption during a sudden power failure or a power cycling event. Power failures result in downtime of the application as embedded systems are reformatted and operating systems are reinstalled. ATP’s PowerProtector features operates continuously during a power glitch meaning it is a true protection solution, not just an auto-save at the moment of the power loss as many other power features operate. PowerProtector plus continues to operate throughout the power cycle and even during complete power loss to provide true data saving and retention.

PTM Veröffentlicht am: