Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Product List
AMS22B-Slide4
The construction of the Model AMS22B Rotary Non-Contacting Position Sensor is shown in a cutaway view on this slide. Areas to highlight are the sintered bronze bushing, the stainless steel shaft design, and the conformal coated sensor PCB assembly. Rotational cycle testing has shown that the materials selected for the bushing/shaft design perform extremely well under side loading. In addition, the sensor PCB assembly is conformal coated for optimum performance under exposure to harsh environments. The Model AMS22B Rotary Non-Contacting Position Sensor is manufactured in an ISO certified production plant utilizing state-of-the-art assembly equipment and lean manufacturing principles, along with computer automated production testers. This compact and versatile design is well-suited for applications with space constraints.
PTM Veröffentlicht am: