Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Slides9

Bourns® Switch Grade Fail-Short device is designed to be the most reliable and safe fail-short device on the market. Many other GDT manufacturers use either a burn-through or solder pellet design, both of which can have limitations in supporting significant, longer duration AC power faults at temperature extremes. In Bourns’ view, the burn-through design is unreliable due to residue which may remain as the fail-short activates which can cause higher contact resistance and thermal runaway. Bourns uses a spring clip with a standoff support in its design. The support holds the clip away from the GDT outer electrodes with a eutectic solder joint. Under extended AC fault, the GDT heats to the point that the joint releases causing a snap action release of the fail-short, diverting the current to ground. This process should eliminate concerns of high contact resistance or partial closure of the fail-short mechanism within rated limits.

PTM Veröffentlicht am: