Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
What is a Mini-Breaker?

A Mini-Breaker is a TCO device that combines overtemperature and overcurrent protection for rechargeable battery applications in a single, compact package. It is an ingenious combination of two common circuit protection technologies, a PTC and a bi-metal switch. It has two key terminals for conducting current; the arm terminal and base terminal which are connected in a normally closed position to allow current flow through the device. The contact point between both terminals is critical and a testament to the high precision of the Bourns Mini-breaker in that the contact resistance in some model families is as low as 1 milliohm (mΩ).

PTM Veröffentlicht am: