Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Product List
TCO-Slide3

There are a few terms to know when choosing a thermal cut-off. Holding temperature is considered the maximum continuous exposure temperature during operation. Functioning temperature is the temperature at which the thermal element melts and the springs move the contact away and open the circuit. Maximum overshoot temperature is the temperature at which the TCO may conduct again due to the possibility of melting the plastic insulating parts.

PTM Veröffentlicht am: