Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
ESD-Slide10

An example of the Charged Device Model shown here, is when the IC slides from the packaging tube, friction causes static charge to form within the device. The IC discharges as the terminals contact a grounded surface, for example, a metal table, or when the part is picked up with metallic tweezers.

PTM Veröffentlicht am: