Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
types of gears
The greatest advantage of the planetary gear is its high strength. Since the load is dispersed over multiple gears, the amount of wear and the chances of gear loss are reduced. The teeth of a spur gear are parallel to the axis of rotation of the shaft. Spur gears are widely used, as they are simpler in design and thus, easier to manufacture.
PTM Veröffentlicht am: