Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Digital-Slide3

The PG-100 series is suitable for monitoring pressure of various types of industrial equipment. This compact digital manometer is easy to carry around and can be operated with one hand, making it convenient for various field service calibrations. The PG-100N series is the next-generation model of PG-100 with additional functions that have been added to enhance usability such as one-touch zero point adjustment, multiple power-off modes, and selectable pressure units. The PG-100B series is the latest model which uses SUS316L stainless steel diaphragm for pressure sensing allowing the PG-100B series to measure both gas and liquid pressure.

PTM Veröffentlicht am:
PTM Updated on: 2019-08-06