Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
key adv
When compared to the primary competitors in the application space, the Wolfspeed C2M1000170D SiC MOSFET outperforms all of them. The Wolfspeed device is more robust and has better overall current-carrying capability. The lower output capacitance is linked to smaller die size of the SiC material, and is responsible for the reduced switching losses. The higher gate drive voltage is compatible with existing silicon drive circuits.
PTM Veröffentlicht am: