Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
SSR-Slide12 meh new

Crydom offers a variety of on-line tools to assist the customer in selecting the solid state relay or contactor that will suit ones application. The Selector for AC Motors (top hyper link) is intended to help the customer find the appropriate solid state relay or contactor for single-phase or three-phase motors. Users only need to enter a few of the motor’s specifications and the customer will get as a result some of the suggested part numbers that could be suitable for specific motor controlling needs. The Parametric Search Engine Tool (bottom hyper link) can also help get users started selecting a solid state relay from Crydom’s standard product catalog. This tools utilizes 7 key performance and configuration parameters beginning with mounting style to point a designer to the best solid state relay or contactor for the combination of application parameters selected.

PTM Veröffentlicht am: