Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
panel-slide14

Mechanical encoders are essentially a series of switches. The code wheel contains contacts spaced evenly along its outer edge. Another contact is stationary and mounted on the encoder chassis. As the code wheel turns, it makes, then breaks contact with the code wheel contacts, one at a time. This making and breaking of a circuit generates a voltage pulse which can be read by a microcontroller.

PTM Veröffentlicht am: