Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
PSoC 4000: Low-Cost 32-bit MCU Slide 9

The Cypress PSoC 4000 family delivers 32-bit performance with a 32-bit ARM Cortex-M0 MCU to upgrade legacy 8-bit and 16-bit MCUs. The ARM Cortex-M0 processes instructions three times faster than a 16-bit MCU and 45 times faster than an 8-bit device. Faster instruction processing enables the ARM Cortex-M0 to spend more time in sleep modes, thereby, reducing the power consumption. The graph on this slide compares the performance of an ARM Cortex-M0 device against legacy 8-bit and 16-bit MCUs using the Dhrystone Benchmark which is used to calculate the relative performance of an MCU.

PTM Veröffentlicht am: