Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Slide11

The PMC series is ready to use with Universal Input while competitors’ devices can have the selectable input switch accidentally be in the wrong position, thus causing damage to the power supply and/or the connected system. In addition, the PMC series is intelligently designed to have NO POWER DE-RATING across the entire input voltage range. This enables full load output with very low input voltage.

PTM Veröffentlicht am: