Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
PMR-Slide4

The PMR series comes with universal AC input and encased in a low profile (1U) full corrosion resistant Aluminum casing with built-in active PFC. Another feature is the built-in parallel and DC OK relay contact which are available as options. This series also has conformal coating on PCBA that can protect the product against chemical and common dust pollutants during operation.

PTM Veröffentlicht am: