Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Chat Session via XBee Slide 13

In order to chat with the other module, use the XCTU console or any serial port terminal application such as CoolTerm or TeraTerm (for Windows only). This demonstration will use the XCTU console for chatting. Note, if the user has two computers, connect a module to each computer. XCTU (or any other serial terminal) will need to be installed on both computers in order to chat. If XCTU is not already running, to chat through XCTU open it on each computer. If using only one computer, one instance of XCTU is adequate. Switch to the Consoles working mode. This working mode of XCTU allows the user to communicate with the radio modules in the devices list. XCTU loads a list of consoles in the working area—one for each module of the devices list, sorted in a tabbed format.

PTM Veröffentlicht am: