Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
Slide6

A visual comparison is shown here between the IP20 and IP68 protection level. Looking at the IP20 image, the electronics and motor windings are exposed with no additional protection. In the image of the IP68 fan, both the electronics and motor windings are completely encapsulated, this provides the high level of protection against the ingress of dust and water.

PTM Veröffentlicht am: