Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
ECS Products for Automotive

One of the fastest growing industries in the market is the smart car. Autonomous vehicles are the future, and the design and implementation of these cars is happening today. More and more electronic features are being added every year. This is a harsh environment for electronic components; it requires products that can operate at extreme temperatures and are capable of dealing with high levels of shock and vibration while still delivering high performance. They are built in factories adhering to the ISO automotive standard IATF 16949. The industry designation for these products is AEC-Q200. These products are also ideal for use in municipality products, such as gas and water meters. Their reliability offers a great solution for industrial and medical applications as well. The next few slides will showcase products developed to meet the stresses of these applications.

PTM Veröffentlicht am: