Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List Associated Content
Summary

In summary, the Efinix Trion™ family offers many advantages to enable the customers design. Efinix is bringing the unique disruptive Quantum FPGA fabric with the combination of lower power, smaller package and optimized for use in volume designs for edge, compute, bridge, and processing applications. Efinix has included some very key hard blocks for DDR memory controllers and MIPI/CSI controllers for use in interfacing to the latest camera sensors or any other type of inline buffered bridging functions needed. These hard blocks further the advantage on power, price and package when compared to implementing these functions in the logic elements like traditional FPGAs. Using FPGA logic resources for these functions would not be as efficient as dedicated functions and the customer would need larger and more power-hungry devices to implement these same high performance functions in other FPGA families.

PTM Veröffentlicht am: