Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
EM Microelectronics Bluetooth® Beacons - EMBP01

The latest ruggedized beacon is the EMBP01 shown here. It is potted, has an IP rating of IP66 or 67 depending on the situation, and 50 meters or more of range outdoors. It also supports up to 10-year battery life if appropriately configured, and has FCC, IC, and CE certification. It is impact, crush, and vibration resistant, and submersible.

PTM Veröffentlicht am: