Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
eGaN-Basics-Slide10

EPC eGaN FETs perform very well at high frequency. These are results of varying input voltages stepped down to 1.2V output at frequencies ranging from 300kHz up to 800kHz. With EPC eGaN FETs designers can demonstrate significant system size reductions without loss of efficiency, as well as extreme space savings by driving frequency from the traditional 300kHz all the way up to 800kHz.

PTM Veröffentlicht am: